Hi we are using the RZN1D to run ECAT slave using ETH4 and ETH5 ports,
We saw on the "RZ_N1_EB_Board_Setup_Notes.VE10.pdf" document section 8 the following remark :
Limitations: The default assembly of PHY addresses is not compliant with the EtherCAT standard. Solution: Change assembly of PHY address setting (refer chapter 5.1.3)
Can you explain how the Phy address is impacting the compliance to the ETHERCAT standard?