I was trying to setup for network booting; But it is throwing Bad Linux ARM64 Image magic!
I want to go back to SD card Booting as I need to check some algorithm;
Please suggest me steps to follow I tried to set default environment.
Thank you
You need to show some kind of log or something.
Or, if you are new to Linux, just start all over again if you are not sure what you broke.
type "print" to show your boot command (bootmcd)
Start all over again means can we reset ?
I was working with SD card only, booting and executable file transfer all..
This is a Renesas RZ/V2L board?
Yessss
I think what is on your SD card does not match your boot command. Also, make sure you have your SD card plugged into the carrier board, not the SOM board