Hii MicBis,
I am bulid yocto linux using BSP-3.0.5 and 3.0.4 both But docker is getting segmentation fault.
but in prebuild image it working.
Hii iam facing issue in doker in RZFIVE I am using BSP-3.0.5root@smarc-rzfive:~# dockerd[ 1885.906390] dockerd[283]: unhandled signal 11 code 0x2 at 0x000000000003c298 in dockerd[10000+2fe0000][ 1885.918618] CPU: 0 PID: 283 Comm: dockerd Not tainted 5.10.175-cip29-yocto-standard #1[ 1885.927684] Hardware name: Renesas SMARC EVK based on r9a07g043f01 (DT)[ 1885.935369] epc: 000000000003c298 ra : 000000000001eec0 sp : 0000003fffd0b9e0[ 1885.943456] gp : 00000000030b5a60 tp : 0000003fed747370 t0 : 0000000000400000[ 1885.951621] t1 : 0000000000000018 t2 : 00000000030d1480 s0 : 0000000000000001[ 1885.959764] s1 : 0000000000008000 a0 : 000000000302f4e0 a1 : 00000000000003f8[ 1885.967919] a2 : 0000000000000003 a3 : 0000000000000081 a4 : 000000000302e360[ 1885.976080] a5 : 0000000000000044 a6 : 0000000000000001 a7 : 0000000000000002[ 1885.984319] s2 : 000000000302f4e0 s3 : 0000000000000000 s4 : 0000003fffd0b9cc[ 1885.992504] s5 : 0000000000000090 s6 : 0000000000000090 s7 : 0000000000000000[ 1886.000675] s8 : 0000003fc50eb810 s9 : 0000000000000000 s10: 0000002b147a6a30[ 1886.008818] s11: 000000000309ff00 t3 : 0000003fed7d780e t4 : 0000003fed93d048[ 1886.016937] t5 : 0000000000000008 t6 : 000000000003beb8[ 1886.023198] status: 0000000200004020 badaddr: 000000000003c298 cause: 0000000000000001[ 1886.032198] audit: type=1701 audit(1699327864.680:8): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=283 comm="dockerd" exe="/usr/bin/dockerd" sig=11 res=1Segmentation faultplease help me
Hi umesh,We tried to reproduce your issue, but we didn't face any error like that. If you follow the instructions carefully described on document SMARC EVK of RZ/Five Linux Start-up Guide Rev.1.00 (2…
Hi Renesas Team,
umesh@ubuntu:~/rzfive_vlp_3.0.5/build$ MACHINE=smarc-rzfive bitbake core-image-minimalWARNING: Layer qt5-layer should set LAYERSERIES_COMPAT_qt5-layer in its conf/layer.conf file to list…
Hi umesh,We tried to reproduce your issue, but we didn't face any error like that. If you follow the instructions carefully described on document SMARC EVK of RZ/Five Linux Start-up Guide Rev.1.00 (2.Build Instructions), you should be able to get it work.Kind Regards.
umesh@ubuntu:~/rzfive_vlp_3.0.5/build$ MACHINE=smarc-rzfive bitbake core-image-minimalWARNING: Layer qt5-layer should set LAYERSERIES_COMPAT_qt5-layer in its conf/layer.conf file to list the core layer names it is compatible with.WARNING: Layer qt5-layer should set LAYERSERIES_COMPAT_qt5-layer in its conf/layer.conf file to list the core layer names it is compatible with.Loading cache: 100% |############################################################################################| Time: 0:00:00Loaded 3656 entries from dependency cache.Removing 21 recipes from the riscv64 sysroot: 100% |#############################################################| Time: 0:00:00NOTE: Resolving any missing task queue dependenciesERROR: Nothing RPROVIDES 'gcc' (but /home/umesh/rzfive_vlp_3.0.5/build/../poky/meta/recipes-core/images/core-image-minimal.bb RDEPENDS on or otherwise requires it)gcc was skipped: it has incompatible license(s): GPL-3.0gcc was skipped: it has incompatible license(s): GPL-3.0NOTE: Runtime target 'gcc' is unbuildable, removing...Missing or unbuildable dependency chain was: ['gcc']ERROR: Required build target 'core-image-minimal' has no buildable providers.Missing or unbuildable dependency chain was: ['core-image-minimal', 'gcc']
Summary: There were 2 WARNING messages shown.Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
i try to install GCC and nano but it giving error How to resolve this
> gcc was skipped: it has incompatible license(s): GPL-3.0
GPL-3.0 packages are disabled in Renesas default build config.If you want to install gcc, you have to remove it (INCOMPATIBLE_LICENSE in local.conf).Note that remove it will change many software in the system.
i am geetig segmentation fault in gcc
root@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service#coot@smarc-rzfive:~/gateway/sink_service# riscv64-poky-linux-gcc -o hello hello.cSegmentation faultroot@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service#root@smarc-rzfive:~/gateway/sink_service# riscv64-poky-linux-gcc --versionSegmentation faultroot@smarc-rzfive:~/gateway/sink_service#
Hi umesh,Do you want to compile your application on target ( rzfive )? It doesn't sound like a good idea.Could you please describe what you want to do to assist you further?If you want just to speed up the compile/run process you can use scp(Linux) or WinSCP(Windows).Let me know if you need any help.Kind Regards.
Hi Renesas team,
I need install wirepass i need compile on target board,
root@smarc-rzfive:~/wirepas/gateway/python_transport# ./generate_package.shTraceback (most recent call last): File "/usr/bin/py3clean", line 8, in <module> sys.exit(py3clean()) File "/usr/lib/python3.8/site-packages/pyclean/cli.py", line 183, in py3clean main('CPython3') File "/usr/lib/python3.8/site-packages/pyclean/cli.py", line 161, in main impl = compat.get_implementation(override=override) File "/usr/lib/python3.8/site-packages/pyclean/compat.py", line 28, in get_implementation return import_module(module_name) File "/usr/lib/python3.8/importlib/__init__.py", line 127, in import_module return _bootstrap._gcd_import(name[level:], package, level) File "<frozen importlib._bootstrap>", line 1014, in _gcd_import File "<frozen importlib._bootstrap>", line 991, in _find_and_load File "<frozen importlib._bootstrap>", line 975, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 671, in _load_unlocked File "<frozen importlib._bootstrap_external>", line 843, in exec_module File "<frozen importlib._bootstrap>", line 219, in _call_with_frames_removed File "/usr/lib/python3.8/site-packages/pyclean/py3clean.py", line 32, in <module> from debpython import files as dpfModuleNotFoundError: No module named 'debpython'running cleanremoving 'build/temp.linux-riscv64-3.8' (and everything under it)removing 'build/lib.linux-riscv64-3.8' (and everything under it)'build/bdist.linux-riscv64' does not exist -- can't clean it'build/scripts-3.8' does not exist -- can't clean itremoving 'build'running sdistrunning egg_infowriting wirepas_gateway.egg-info/PKG-INFOwriting dependency_links to wirepas_gateway.egg-info/dependency_links.txtwriting entry points to wirepas_gateway.egg-info/entry_points.txtwriting requirements to wirepas_gateway.egg-info/requires.txtwriting top-level names to wirepas_gateway.egg-info/top_level.txtreading manifest file 'wirepas_gateway.egg-info/SOURCES.txt'writing manifest file 'wirepas_gateway.egg-info/SOURCES.txt'running checkcreating wirepas_gateway-1.4.3rc5creating wirepas_gateway-1.4.3rc5/wirepas_gatewaycreating wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocreating wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscreating wirepas_gateway-1.4.3rc5/wirepas_gateway/dbus/c-extensioncreating wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcreating wirepas_gateway-1.4.3rc5/wirepas_gateway/utilscopying files to wirepas_gateway-1.4.3rc5...copying LICENSE -> wirepas_gateway-1.4.3rc5copying README.md -> wirepas_gateway-1.4.3rc5copying requirements.txt -> wirepas_gateway-1.4.3rc5copying setup.py -> wirepas_gateway-1.4.3rc5copying wirepas_gateway/__about__.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/__main__.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/configure_node.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/dbus_print_client.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/transport_service.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway.egg-info/PKG-INFO -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/SOURCES.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/dependency_links.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/entry_points.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/requires.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/top_level.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway/dbus/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/dbus_client.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/return_code.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/sink_manager.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/c-extension/dbus_c.c -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbus/c-extensioncopying wirepas_gateway/protocol/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcopying wirepas_gateway/protocol/mqtt_wrapper.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcopying wirepas_gateway/protocol/topic_helper.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcopying wirepas_gateway/utils/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/utilscopying wirepas_gateway/utils/argument_tools.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/utilscopying wirepas_gateway/utils/serialization_tools.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/utilsWriting wirepas_gateway-1.4.3rc5/setup.cfgCreating tar archiveremoving 'wirepas_gateway-1.4.3rc5' (and everything under it)running bdist_wheelrunning buildrunning build_pycreating buildcreating build/lib.linux-riscv64-3.8creating build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/configure_node.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/dbus_print_client.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/transport_service.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/__about__.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/__main__.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycreating build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/sink_manager.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/dbus_client.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/return_code.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscreating build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcopying wirepas_gateway/protocol/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcopying wirepas_gateway/protocol/mqtt_wrapper.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcopying wirepas_gateway/protocol/topic_helper.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcreating build/lib.linux-riscv64-3.8/wirepas_gateway/utilscopying wirepas_gateway/utils/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/utilscopying wirepas_gateway/utils/argument_tools.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/utilscopying wirepas_gateway/utils/serialization_tools.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/utilscreating build/lib.linux-riscv64-3.8/wirepas_gateway/dbus/c-extensioncopying wirepas_gateway/dbus/c-extension/dbus_c.c -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbus/c-extensionrunning build_extbuilding 'dbusCExtension' extensioncreating build/temp.linux-riscv64-3.8creating build/temp.linux-riscv64-3.8/wirepas_gatewaycreating build/temp.linux-riscv64-3.8/wirepas_gateway/dbuscreating build/temp.linux-riscv64-3.8/wirepas_gateway/dbus/c-extensionriscv64-poky-linux-gcc -fstack-protector-strong -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security -Wno-unused-result -Wsign-compare -DNDEBUG -g -O3 -Wall -O2 -pipe -g -feliminate-unused-debug-types -fmacro-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map== -fdebug-prefix-map== -O2 -pipe -g -feliminate-unused-debug-types -fmacro-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map== -fdebug-prefix-map== -fPIC -I/usr/include/python3.8 -c wirepas_gateway/dbus/c-extension/dbus_c.c -o build/temp.linux-riscv64-3.8/wirepas_gateway/dbus/c-extension/dbus_c.oduring RTL pass: sched1wirepas_gateway/dbus/c-extension/dbus_c.c: In function 'on_packet_received':wirepas_gateway/dbus/c-extension/dbus_c.c:100:1: internal compiler error: Segmentation fault } ^Please submit a full bug report,with preprocessed source if appropriate.See <https://gcc.gnu.org/bugs/> for instructions.error: command 'riscv64-poky-linux-gcc' failed with exit status 1root@smarc-rzfive:~/wirepas/gateway/python_transport# ./generate_package.shTraceback (most recent call last): File "/usr/bin/py3clean", line 8, in <module> sys.exit(py3clean()) File "/usr/lib/python3.8/site-packages/pyclean/cli.py", line 183, in py3clean main('CPython3') File "/usr/lib/python3.8/site-packages/pyclean/cli.py", line 161, in main impl = compat.get_implementation(override=override) File "/usr/lib/python3.8/site-packages/pyclean/compat.py", line 28, in get_implementation return import_module(module_name) File "/usr/lib/python3.8/importlib/__init__.py", line 127, in import_module return _bootstrap._gcd_import(name[level:], package, level) File "<frozen importlib._bootstrap>", line 1014, in _gcd_import File "<frozen importlib._bootstrap>", line 991, in _find_and_load File "<frozen importlib._bootstrap>", line 975, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 671, in _load_unlocked File "<frozen importlib._bootstrap_external>", line 843, in exec_module File "<frozen importlib._bootstrap>", line 219, in _call_with_frames_removed File "/usr/lib/python3.8/site-packages/pyclean/py3clean.py", line 32, in <module> from debpython import files as dpfModuleNotFoundError: No module named 'debpython'running cleanremoving 'build/temp.linux-riscv64-3.8' (and everything under it)removing 'build/lib.linux-riscv64-3.8' (and everything under it)'build/bdist.linux-riscv64' does not exist -- can't clean it'build/scripts-3.8' does not exist -- can't clean itremoving 'build'running sdistrunning egg_infowriting wirepas_gateway.egg-info/PKG-INFOwriting dependency_links to wirepas_gateway.egg-info/dependency_links.txtwriting entry points to wirepas_gateway.egg-info/entry_points.txtwriting requirements to wirepas_gateway.egg-info/requires.txtwriting top-level names to wirepas_gateway.egg-info/top_level.txtreading manifest file 'wirepas_gateway.egg-info/SOURCES.txt'writing manifest file 'wirepas_gateway.egg-info/SOURCES.txt'running checkcreating wirepas_gateway-1.4.3rc5creating wirepas_gateway-1.4.3rc5/wirepas_gatewaycreating wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocreating wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscreating wirepas_gateway-1.4.3rc5/wirepas_gateway/dbus/c-extensioncreating wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcreating wirepas_gateway-1.4.3rc5/wirepas_gateway/utilscopying files to wirepas_gateway-1.4.3rc5...copying LICENSE -> wirepas_gateway-1.4.3rc5copying README.md -> wirepas_gateway-1.4.3rc5copying requirements.txt -> wirepas_gateway-1.4.3rc5copying setup.py -> wirepas_gateway-1.4.3rc5copying wirepas_gateway/__about__.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/__main__.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/configure_node.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/dbus_print_client.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway/transport_service.py -> wirepas_gateway-1.4.3rc5/wirepas_gatewaycopying wirepas_gateway.egg-info/PKG-INFO -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/SOURCES.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/dependency_links.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/entry_points.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/requires.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway.egg-info/top_level.txt -> wirepas_gateway-1.4.3rc5/wirepas_gateway.egg-infocopying wirepas_gateway/dbus/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/dbus_client.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/return_code.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/sink_manager.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbuscopying wirepas_gateway/dbus/c-extension/dbus_c.c -> wirepas_gateway-1.4.3rc5/wirepas_gateway/dbus/c-extensioncopying wirepas_gateway/protocol/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcopying wirepas_gateway/protocol/mqtt_wrapper.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcopying wirepas_gateway/protocol/topic_helper.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/protocolcopying wirepas_gateway/utils/__init__.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/utilscopying wirepas_gateway/utils/argument_tools.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/utilscopying wirepas_gateway/utils/serialization_tools.py -> wirepas_gateway-1.4.3rc5/wirepas_gateway/utilsWriting wirepas_gateway-1.4.3rc5/setup.cfgCreating tar archiveremoving 'wirepas_gateway-1.4.3rc5' (and everything under it)running bdist_wheelrunning buildrunning build_pycreating buildcreating build/lib.linux-riscv64-3.8creating build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/configure_node.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/dbus_print_client.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/transport_service.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/__about__.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycopying wirepas_gateway/__main__.py -> build/lib.linux-riscv64-3.8/wirepas_gatewaycreating build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/sink_manager.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/dbus_client.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscopying wirepas_gateway/dbus/return_code.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbuscreating build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcopying wirepas_gateway/protocol/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcopying wirepas_gateway/protocol/mqtt_wrapper.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcopying wirepas_gateway/protocol/topic_helper.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/protocolcreating build/lib.linux-riscv64-3.8/wirepas_gateway/utilscopying wirepas_gateway/utils/__init__.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/utilscopying wirepas_gateway/utils/argument_tools.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/utilscopying wirepas_gateway/utils/serialization_tools.py -> build/lib.linux-riscv64-3.8/wirepas_gateway/utilscreating build/lib.linux-riscv64-3.8/wirepas_gateway/dbus/c-extensioncopying wirepas_gateway/dbus/c-extension/dbus_c.c -> build/lib.linux-riscv64-3.8/wirepas_gateway/dbus/c-extensionrunning build_extbuilding 'dbusCExtension' extensioncreating build/temp.linux-riscv64-3.8creating build/temp.linux-riscv64-3.8/wirepas_gatewaycreating build/temp.linux-riscv64-3.8/wirepas_gateway/dbuscreating build/temp.linux-riscv64-3.8/wirepas_gateway/dbus/c-extensionriscv64-poky-linux-gcc -fstack-protector-strong -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security -Wno-unused-result -Wsign-compare -DNDEBUG -g -O3 -Wall -O2 -pipe -g -feliminate-unused-debug-types -fmacro-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map== -fdebug-prefix-map== -O2 -pipe -g -feliminate-unused-debug-types -fmacro-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map=/python3/3.8.14-r0=/usr/src/debug/python3/3.8.14-r0 -fdebug-prefix-map== -fdebug-prefix-map== -fPIC -I/usr/include/python3.8 -c wirepas_gateway/dbus/c-extension/dbus_c.c -o build/temp.linux-riscv64-3.8/wirepas_gateway/dbus/c-extension/dbus_c.oduring RTL pass: sched1wirepas_gateway/dbus/c-extension/dbus_c.c: In function 'on_packet_received':wirepas_gateway/dbus/c-extension/dbus_c.c:100:1: internal compiler error: Segmentation fault } ^Please submit a full bug report,with preprocessed source if appropriate.See <https://gcc.gnu.org/bugs/> for instructions.error: command 'riscv64-poky-linux-gcc' failed with exit 1
Tanks and regards,
Umesh
Hi umesh, You can check this thread for your reference. It might help.Kind Regards.