RZ/V2L: MIPI Display probe issue

Hi, 

We trying to test MIPI Display in RZ/V2L board.

HW connection:

MIPI DSI lanes from CPU is connected to a Winstar MIPI DSI (P/N WF70A8TYAHMNGB).

We are not using any bridge.

Issue is, while booting probe is getting differed. We tried to debug some more and got that in below driver, a function is failing.

driver : drivers/gpu/drm/rcar-du/rcar_du_encoder.c

function: rcar_du_encoder_init

line : ret = drm_bridge_attach(encoder, bridge, NULL, 0);

In above function, attaching display fails with error code 517.

Kindly suggest if any changes in dts and driver is required.

Regards.

Parents
  • You should debug inside function drm_bridge_attach() and find out why it is failing. Then you will know your answer.

  • If driver : drivers/gpu/drm/drm_bridge.c in function "drm_bridge_attach" there is a condition like below

    if (bridge->funcs->attach) {
    ret = bridge->funcs->attach(bridge, flags);
    if (ret < 0)
    goto err_reset_bridge;
    }

    exactly in this condition, error occurs and excution will directly go to "err_reset_bridge".

    So, I am stuck here.

  • You have to see what function is bridge->funcs->attach()

    That is one thing about the kernel that is annoying....all the function pointers that are filled in at run time.

    You can print out the value of bridge->funcs->attach and see what matches up with it in your system.map file.

    But, it is probably the function rzg2l_mipi_dsi_attach() in file drivers/gpu/drm/rcar-du/rzg2l_mipi_dsi.c

    You can see where it fills in all the function pointers:

    static const struct drm_bridge_funcs rzg2l_mipi_dsi_bridge_ops = {
    .attach = rzg2l_mipi_dsi_attach,
    .detach = rzg2l_mipi_dsi_detach,
    .mode_set = rzg2l_mipi_dsi_mode_set,
    .enable = rzg2l_mipi_dsi_enable,
    .disable = rzg2l_mipi_dsi_disable,
    .mode_valid = rzg2l_mipi_dsi_bridge_mode_valid,
    };

    I would put a printk in that rzg2l_mipi_dsi_attach() function to see if that is what it is calling.

    And if so, why it is failing.

    Basically, you just keep doing this procedure over and over again until you finally find the line that fails.

    I had helped someone once that we did this for a several hours....only to find that the reason for the failure was a spelling mistake in the Device Tree. It was a very simple fix, but took hours to find. That's Linux.

  • Hi,

    According to the suggestion i have put print statements in drivers and check what is failing.
    Below are my observations:

    In driver "drivers/gpu/drm/rcar-du/rzg2l_mipi_dsi.c" function "rzg2l_mipi_dsi_attach"
    ret = rzg2l_mipi_dsi_find_panel_or_bridge(mipi_dsi);
    This function is called and this is pointing to "rzg2l_mipi_dsi_find_panel_or_bridge" in same driver.
    There is an if-else condition checking if bridge or not.

    Our display is not connected to any brige. Direct MIPI lanes from CPU is connected to display.
    Hence it goes to "else" condition and tries to find the display with below function
    mipi_dsi->panel = of_drm_find_panel(remote);

    This call points to driver "drivers/gpu/drm/drm_panel.c" function "of_drm_find_panel"
    This function executes and directly returns "-EPROBE_DEFER".

    Below is our dts configuration:
    &dsi0 {
        status = "okay";

         panel@0 { /* MIPI_DSI: MIPI DSI Host */
             compatible = "panel-winstar";
             v3p3-supply = <&reg_3p3v>;
             v1p8-supply = <&reg_1p8v>;
             dsi-lanes = <4>;
             video-mode = <2>;
             width-mm = <154>;
             height-mm = <85>;
             status = "okay";

             port@0 {
                  panel_in: endpoint {
                       remote-endpoint = <&dsi0_out>;
                  };
             };
          };

          ports {
             port@1 {
                   reg = <1>;
                   dsi0_out: endpoint {
                                  remote-endpoint = <&panel_in>;
                                  data-lanes = <1 2 3 4>;
                                  attach-bridge;
                   };
                };
          };
    };

    &du {
          status = "okay";
    };

    Kindly help in solving this issue.

Reply
  • Hi,

    According to the suggestion i have put print statements in drivers and check what is failing.
    Below are my observations:

    In driver "drivers/gpu/drm/rcar-du/rzg2l_mipi_dsi.c" function "rzg2l_mipi_dsi_attach"
    ret = rzg2l_mipi_dsi_find_panel_or_bridge(mipi_dsi);
    This function is called and this is pointing to "rzg2l_mipi_dsi_find_panel_or_bridge" in same driver.
    There is an if-else condition checking if bridge or not.

    Our display is not connected to any brige. Direct MIPI lanes from CPU is connected to display.
    Hence it goes to "else" condition and tries to find the display with below function
    mipi_dsi->panel = of_drm_find_panel(remote);

    This call points to driver "drivers/gpu/drm/drm_panel.c" function "of_drm_find_panel"
    This function executes and directly returns "-EPROBE_DEFER".

    Below is our dts configuration:
    &dsi0 {
        status = "okay";

         panel@0 { /* MIPI_DSI: MIPI DSI Host */
             compatible = "panel-winstar";
             v3p3-supply = <&reg_3p3v>;
             v1p8-supply = <&reg_1p8v>;
             dsi-lanes = <4>;
             video-mode = <2>;
             width-mm = <154>;
             height-mm = <85>;
             status = "okay";

             port@0 {
                  panel_in: endpoint {
                       remote-endpoint = <&dsi0_out>;
                  };
             };
          };

          ports {
             port@1 {
                   reg = <1>;
                   dsi0_out: endpoint {
                                  remote-endpoint = <&panel_in>;
                                  data-lanes = <1 2 3 4>;
                                  attach-bridge;
                   };
                };
          };
    };

    &du {
          status = "okay";
    };

    Kindly help in solving this issue.

Children