Hii Team,
Currently i am using VLP3.0.5 Update-3
in boot log i am getting the messgae like below
gpio gpiochip0: (11030000.pinctrl): detected irqchip that is shared with multiple gpiochips: please fix the driver
What will be the cause for the above print?
Regards,
Ashritha
Hi Ashritha,Can you please share your full bootlog?Kind Regards.
NOTICE: BL2: v2.9(release):4319873-dirtyNOTICE: BL2: Built : 12:14:16, May 24 2024NOTICE: BL2: eMMC boot from partition 1NOTICE: BL2: Load dst=0x1f740 src=(p:1)0x20000(256) len=0x10(1)NOTICE: BL2: eMMC boot from partition 1NOTICE: BL2: Load dst=0x1f8a0 src=(p:1)0x20010(256) len=0x28(1)NOTICE: BL2: eMMC boot from partition 1NOTICE: BL2: Load dst=0x44000000 src=(p:1)0x20090(256) len=0x6069(49)NOTICE: BL2: eMMC boot from partition 1NOTICE: BL2: Load dst=0x1f740 src=(p:1)0x20000(256) len=0x10(1)NOTICE: BL2: eMMC boot from partition 1NOTICE: BL2: Load dst=0x1f8a0 src=(p:1)0x20010(256) len=0x28(1)NOTICE: BL2: Load dst=0x1f8a0 src=(p:1)0x20038(256) len=0x28(1)NOTICE: BL2: eMMC boot from partition 1NOTICE: BL2: Load dst=0x50000000 src=(p:1)0x26100(304) len=0xb2e70(1432)NOTICE: BL2: Booting BL31NOTICE: BL31: v2.9(release):4319873-dirtyNOTICE: BL31: Built : 12:14:16, May 24 2024
U-Boot 2021.10 (May 31 2024 - 06:44:29 +0000)
CPU: Renesas Electronics CPU rev 1.0Model: iW-RainboW-G53M-RZ/G2UL-OSMDRAM: 1.9 GiBWDT: watchdog@0000000012800800WDT: Started with servicing (60s timeout)MMC: sd@11c00000: 0, sd@11c10000: 1Loading Environment from MMC... OKIn: serial@1004b800Out: serial@1004b800Err: serial@1004b800U-boot WDT started!
Board Info: BSP Version : iW-PRHGZ-SC-01-R2.0-REL1.0a-Linux5.10.184 SOM Version : iW-PRHGZ-AP-01-R2.0
Net: eth0: ethernet@11c20000 [PRIME]Hit any key to stop autoboot: 2 1 0 switch to partitions #0, OKmmc0(part 0) is current device17773056 bytes read in 770 ms (22 MiB/s)Booting from mmc ...28846 bytes read in 14 ms (2 MiB/s)Moving Image from 0x48080000 to 0x48200000, end=49360000## Flattened Device Tree blob at 48000000 Booting using the fdt blob at 0x48000000 Loading Device Tree to 0000000057ff5000, end 0000000057fff0ad ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050][ 0.000000] Linux version 5.10.184-cip36-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 8.3.0, GNU ld (GNU Binutils) 2.31.1) #1 SMP PREEMPT Mon May 27 12:25:05 UTC 2024[ 0.000000] Machine model: iW-RainboW-G53M-RZG2UL-OSM[ 0.000000] earlycon: scif0 at MMIO 0x000000001004b800 (options '115200n8')[ 0.000000] printk: bootconsole [scif0] enabled[ 0.000000] efi: UEFI not found.[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000058000000, size 256 MiB[ 0.000000] OF: reserved mem: initialized node linux,cma@58000000, compatible id shared-dma-pool[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000068000000, size 128 MiB[ 0.000000] OF: reserved mem: initialized node linux,multimedia, compatible id shared-dma-pool[ 0.000000] Zone ranges:[ 0.000000] DMA [mem 0x0000000048000000-0x00000000bfffffff][ 0.000000] DMA32 empty[ 0.000000] Normal empty[ 0.000000] Movable zone start for each node[ 0.000000] Early memory node ranges[ 0.000000] node 0: [mem 0x0000000048000000-0x00000000bfffffff][ 0.000000] Initmem setup node 0 [mem 0x0000000048000000-0x00000000bfffffff][ 0.000000] psci: probing for conduit method from DT.[ 0.000000] psci: PSCIv1.1 detected in firmware.[ 0.000000] psci: Using standard PSCI v0.2 function IDs[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.[ 0.000000] psci: SMC Calling Convention v1.2[ 0.000000] percpu: Embedded 23 pages/cpu s55384 r8192 d30632 u94208[ 0.000000] Detected VIPT I-cache on CPU0[ 0.000000] CPU features: detected: GIC system register CPU interface[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 483840[ 0.000000] Kernel command line: console=ttySC0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw wdt_overflow=0[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off[ 0.000000] Memory: 1515112K/1966080K available (10816K kernel code, 1036K rwdata, 3364K rodata, 2048K init, 387K bss, 57752K reserved, 393216K cma-reserved)[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1[ 0.000000] rcu: Preemptible hierarchical RCU implementation.[ 0.000000] rcu: RCU event tracing is enabled.[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=1.[ 0.000000] Trampoline variant of Tasks RCU enabled.[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0[ 0.000000] GICv3: 480 SPIs implemented[ 0.000000] GICv3: 0 Extended SPIs implemented[ 0.000000] GICv3: Distributor has no Range Selector support[ 0.000000] GICv3: 16 PPIs implemented[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000011940000[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (virt).[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns[ 0.000005] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns[ 0.008237] Console: colour dummy device 80x25[ 0.012736] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)[ 0.023044] pid_max: default: 32768 minimum: 301[ 0.027827] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)[ 0.035265] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)[ 0.044830] rcu: Hierarchical SRCU implementation.[ 0.050334] Detected Renesas RZ/G2UL r9a07g043 Rev 1[ 0.055441] [ 0.055441] Board Info:[ 0.059393] BSP Version : iW-PRHGZ-SC-01-R2.0-REL1.0a-Linux5.10.184[ 0.066294] SOM Version : iW-PRHGZ-AP-01-R2.0[ 0.066294] [ 0.073000] EFI services will not be available.[ 0.077752] smp: Bringing up secondary CPUs ...[ 0.082319] smp: Brought up 1 node, 1 CPU[ 0.086345] SMP: Total of 1 processors activated.[ 0.091073] CPU features: detected: Privileged Access Never[ 0.096666] CPU features: detected: LSE atomic instructions[ 0.102259] CPU features: detected: User Access Override[ 0.107591] CPU features: detected: 32-bit EL0 Support[ 0.112748] CPU features: detected: Common not Private translations[ 0.119039] CPU features: detected: Data cache clean to the PoU not required for I/D coherence[ 0.127679] CPU features: detected: CRC32 instructions[ 0.132836] CPU features: detected: Speculative Store Bypassing Safe (SSBS)[ 0.139826] CPU features: detected: 32-bit EL1 Support[ 0.161174] CPU: All CPU(s) started at EL1[ 0.165355] alternatives: patching kernel code[ 0.172353] devtmpfs: initialized[ 0.181184] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns[ 0.191042] futex hash table entries: 256 (order: 2, 16384 bytes, linear)[ 0.208379] pinctrl core: initialized pinctrl subsystem[ 0.214558] DMI not present or invalid.[ 0.218982] NET: Registered protocol family 16[ 0.225047] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations[ 0.232316] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations[ 0.240261] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations[ 0.248336] audit: initializing netlink subsys (disabled)[ 0.254578] thermal_sys: Registered thermal governor 'step_wise'[ 0.254909] cpuidle: using governor menu[ 0.264922] audit: type=2000 audit(0.172:1): state=initialized audit_enabled=0 res=1[ 0.272905] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.[ 0.279764] ASID allocator initialised with 65536 entries[ 0.308658] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages[ 0.315484] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages[ 0.322316] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages[ 0.329053] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages[ 0.337610] cryptd: max_cpu_qlen set to 1000[ 0.345801] debugfs: Directory 'fixed-1.8V' with parent 'regulator' already present![ 0.354452] iommu: Default domain type: Translated [ 0.360339] vgaarb: loaded[ 0.363372] SCSI subsystem initialized[ 0.367702] usbcore: registered new interface driver usbfs[ 0.373339] usbcore: registered new interface driver hub[ 0.378714] usbcore: registered new device driver usb[ 0.384496] mc: Linux media interface: v0.10[ 0.388820] videodev: Linux video capture interface: v2.00[ 0.394403] pps_core: LinuxPPS API ver. 1 registered[ 0.399390] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>[ 0.408572] PTP clock support registered[ 0.412536] EDAC MC: Ver: 3.0.0[ 0.416934] Advanced Linux Sound Architecture Driver Initialized.[ 0.424003] clocksource: Switched to clocksource arch_sys_counter[ 0.430451] VFS: Disk quotas dquot_6.6.0[ 0.434477] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)[ 0.447530] NET: Registered protocol family 2[ 0.452219] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)[ 0.461133] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)[ 0.469879] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)[ 0.477959] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)[ 0.485600] TCP: Hash tables configured (established 16384 bind 16384)[ 0.492358] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)[ 0.499149] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)[ 0.506533] NET: Registered protocol family 1[ 0.511457] RPC: Registered named UNIX socket transport module.[ 0.517467] RPC: Registered udp transport module.[ 0.522196] RPC: Registered tcp transport module.[ 0.526920] RPC: Registered tcp NFSv4.1 backchannel transport module.[ 0.533395] PCI: CLS 0 bytes, default 64[ 0.538113] kvm [1]: HYP mode not available[ 0.544374] workingset: timestamp_bits=46 max_order=19 bucket_order=0[ 0.557750] squashfs: version 4.0 (2009/01/31) Phillip Lougher[ 0.564599] NFS: Registering the id_resolver key type[ 0.569768] Key type id_resolver registered[ 0.573978] Key type id_legacy registered[ 0.578106] nfs4filelayout_init: NFSv4 File Layout Driver Registering...[ 0.584840] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...[ 0.592292] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.[ 0.599134] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)[ 0.606593] io scheduler mq-deadline registered[ 0.611147] io scheduler kyber registered[ 0.661383] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled[ 0.668963] SuperH (H)SCI(F) driver initialized[ 0.685718] loop: module loaded[ 0.691650] tun: Universal TUN/TAP device driver, 1.6[ 0.697056] CAN device driver interface[ 0.701388] e1000e: Intel(R) PRO/1000 Network Driver[ 0.706412] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.[ 0.713089] VFIO - User Level meta-driver version: 0.3[ 0.718592] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver[ 0.725209] ehci-pci: EHCI PCI platform driver[ 0.729740] ehci-platform: EHCI generic platform driver[ 0.735728] ehci-platform 11c70100.usb: EHCI Host Controller[ 0.741472] ehci-platform 11c70100.usb: new USB bus registered, assigned bus number 1[ 0.749456] ehci-platform 11c70100.usb: irq 94, io mem 0x11c70100[ 0.768018] ehci-platform 11c70100.usb: USB 2.0 started, EHCI 1.10[ 0.774933] hub 1-0:1.0: USB hub found[ 0.778784] hub 1-0:1.0: 1 port detected[ 0.783449] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver[ 0.789716] ohci-pci: OHCI PCI platform driver[ 0.794256] ohci-platform: OHCI generic platform driver[ 0.800140] ohci-platform 11c70000.usb: Generic Platform OHCI controller[ 0.807120] ohci-platform 11c70000.usb: new USB bus registered, assigned bus number 2[ 0.815128] ohci-platform 11c70000.usb: irq 92, io mem 0x11c70000[ 0.910684] hub 2-0:1.0: USB hub found[ 0.914531] hub 2-0:1.0: 1 port detected[ 0.920079] usbcore: registered new interface driver usb-storage[ 0.927007] renesas_usbhs 11c60000.usb: host probed[ 0.931969] renesas_usbhs 11c60000.usb: no transceiver found[ 0.937799] renesas_usbhs 11c60000.usb: gadget probed[ 0.943931] usbcore: registered new interface driver usbtouchscreen[ 0.950511] i2c /dev entries driver[ 0.958683] rzg2l-csi2 10830400.csi2: 2 lanes found[ 0.966939] EDAC rzg2l-edac: IO mapped reg addr: 0x11410000[ 0.972889] EDAC MC0: Giving out device to module rzg2l-edac controller renesas,r9a07g043-edac: DEV 11410000.edac (INTERRUPT)[ 0.986921] ledtrig-cpu: registered to indicate activity on CPUs[ 0.993095] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....[ 1.000233] clocksource: timer@12801400: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns[ 1.010214] sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns[ 1.018175] /soc/timer@12801400: used for clocksource[ 1.023321] usb usb1-port1: over-current condition[ 1.028464] /soc/timer@12801800: used for clock events[ 1.034689] usbcore: registered new interface driver usbhid[ 1.040316] usbhid: USB HID core driver[ 1.044752] optee: probing for conduit method.[ 1.049238] optee: api uid mismatch[ 1.052760] optee: probe of firmware:optee failed with error -22[ 1.060941] NET: Registered protocol family 10[ 1.066463] Segment Routing with IPv6[ 1.070307] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver[ 1.076796] NET: Registered protocol family 17[ 1.081295] can: controller area network core[ 1.085745] NET: Registered protocol family 29[ 1.090271] can: raw protocol[ 1.093294] can: broadcast manager protocol[ 1.097524] can: netlink gateway - max_hops=1[ 1.101992] usb usb2-port1: over-current condition[ 1.107038] Key type dns_resolver registered[ 1.111921] registered taskstats version 1[ 1.123298] thermal emergency: not set value[ 1.129576] gpio gpiochip0: (11030000.pinctrl): detected irqchip that is shared with multiple gpiochips: please fix the driver.[ 1.141447] pinctrl-rzg2l 11030000.pinctrl: pinctrl-rzg2l support registered[ 1.151602] 1004b800.serial: ttySC0 at MMIO 0x1004b800 (irq = 15, base_baud = 0) is a scif[ 1.160104] printk: console [ttySC0] enabled[ 1.160104] printk: console [ttySC0] enabled[ 1.168628] printk: bootconsole [scif0] disabled[ 1.168628] printk: bootconsole [scif0] disabled[ 1.184969] ravb 11c20000.ethernet eth0: Base address at 0x11c20000, 00:01:02:03:04:05, IRQ 88.[ 1.220048] ehci-platform 11c50100.usb: EHCI Host Controller[ 1.225741] ehci-platform 11c50100.usb: new USB bus registered, assigned bus number 3[ 1.233692] ehci-platform 11c50100.usb: irq 93, io mem 0x11c50100[ 1.252011] ehci-platform 11c50100.usb: USB 2.0 started, EHCI 1.10[ 1.258878] hub 3-0:1.0: USB hub found[ 1.262697] hub 3-0:1.0: 1 port detected[ 1.267650] ohci-platform 11c50000.usb: Generic Platform OHCI controller[ 1.274436] ohci-platform 11c50000.usb: new USB bus registered, assigned bus number 4[ 1.282405] ohci-platform 11c50000.usb: irq 91, io mem 0x11c50000[ 1.378715] hub 4-0:1.0: USB hub found[ 1.382537] hub 4-0:1.0: 1 port detected[ 1.387501] renesas_usbhs 11c60000.usb: host probed[ 1.392460] renesas_usbhs 11c60000.usb: no transceiver found[ 1.398279] renesas_usbhs 11c60000.usb: gadget probed[ 1.403590] renesas_usbhs 11c60000.usb: probed[ 1.411191] da9062 0-0058: Device detected (device-ID: 0x62, var-ID: 0x32, DA9062)[ 1.424995] da9063-rtc da9062-rtc: DMA mask not set[ 1.441087] da9063-rtc da9062-rtc: registered as rtc0[ 1.447013] da9063-rtc da9062-rtc: setting system clock to 2000-01-01T00:00:08 UTC (946684808)[ 1.456662] da9063-onkey da9062-onkey: DMA mask not set[ 1.463558] input: da9062-onkey as /devices/platform/soc/10058000.i2c/i2c-0/0-0058/da9062-onkey/input/input0[ 1.474781] i2c-riic 10058000.i2c: registered with 400000Hz bus speed[ 1.483051] pca953x 1-0020: supply vcc not found, using dummy regulator[ 1.489881] pca953x 1-0020: using no AI[ 1.544036] ov5640 1-003c: ov5640_read_reg: error: reg=300a[ 1.549612] ov5640 1-003c: ov5640_check_chip_id: failed to read chip identifier[ 1.557538] i2c-riic 10058400.i2c: registered with 100000Hz bus speed[ 1.567987] renesas_mtu3 10001200.timer: ch3: used for pwm mode 1 output at pin MTIOC3A[ 1.577955] renesas_mtu3 10001200.timer: used for pwm controller of mtu3[ 1.584767] renesas_mtu3 10001200.timer: ch0: used as clock source[ 1.591168] clocksource: 10001200.timer: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 18664368 ns[ 1.600126] renesas_mtu3 10001200.timer: ch1: used for clock events[ 1.606561] renesas_mtu3 10001200.timer: Renesas MTU3 driver probed[ 1.617035] panel-simple rgb_panel: Specify missing connector_type[ 1.625617] [drm] Initialized rcar-du 1.0.0 20130110 for 10890000.display on minor 0[ 1.633475] [drm] Device 10890000.display probed[ 1.638307] renesas_sdhi_internal_dmac 11c00000.mmc: mmc0 base at 0x0000000011c00000, max clock rate 100 MHz[ 1.648232] renesas_sdhi_internal_dmac 11c10000.mmc: mmc1 base at 0x0000000011c10000, max clock rate 100 MHz[ 1.698027] Console: switching to colour frame buffer device 100x30[ 1.720244] rcar-du 10890000.display: [drm] fb0: rcar-dudrmfb frame buffer device[ 1.729048] ALSA device list:[ 1.732185] No soundcards found.[ 1.736469] Waiting for root device /dev/mmcblk0p2...[ 1.798925] mmc0: new HS200 MMC card at address 0001[ 1.804597] mmcblk0: mmc0:0001 DG4016 14.7 GiB [ 1.809332] mmcblk0boot0: mmc0:0001 DG4016 partition 1 4.00 MiB[ 1.815411] mmcblk0boot1: mmc0:0001 DG4016 partition 2 4.00 MiB[ 1.821563] mmcblk0rpmb: mmc0:0001 DG4016 partition 3 4.00 MiB, chardev (242:0)[ 1.830006] mmcblk0: p1 p2[ 1.856375] EXT4-fs (mmcblk0p2): recovery complete[ 1.861915] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)[ 1.870135] VFS: Mounted root (ext4 filesystem) on device 179:2.[ 1.878678] devtmpfs: mounted[ 1.883501] Freeing unused kernel memory: 2048K[ 1.888207] Run /sbin/init as init process[ 2.061170] systemd[1]: System time before build time, advancing clock.[ 2.086925] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)[ 2.109175] systemd[1]: Detected architecture arm64.
Welcome to Poky (Yocto Project Reference Distro) 3.1.26 (dunfell)!
[ 2.144904] systemd[1]: Set hostname to <iWave-G53M>.[ 2.155411] mmc1: new ultra high speed SDR104 SDXC card at address 59b4[ 2.169062] mmcblk1: mmc1:59b4 EC1S5 59.7 GiB [ 2.180584] mmcblk1: p1 p2[ 2.655342] random: systemd: uninitialized urandom read (16 bytes read)[ 2.662419] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.[ 2.674791] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)[ 2.687306] systemd[1]: Created slice system-getty.slice.[ OK ] Created slice system-getty.slice.[ 2.708251] random: systemd: uninitialized urandom read (16 bytes read)[ 2.716542] systemd[1]: Created slice system-serial\x2dgetty.slice.[ OK ] Created slice system-serial\x2dgetty.slice.[ 2.740527] random: systemd: uninitialized urandom read (16 bytes read)[ 2.748744] systemd[1]: Created slice User and Session Slice.[ OK ] Created slice User and Session Slice.[ 2.768655] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.[ OK ] Started Dispatch Password …ts to Console Directory Watch.[ 2.796594] systemd[1]: Started Forward Password Requests to Wall Directory Watch.[ OK ] Started Forward Password R…uests to Wall Directory Watch.[ 2.820453] systemd[1]: Reached target Host and Network Name Lookups.[ OK ] Reached target Host and Network Name Lookups.[ 2.844343] systemd[1]: Reached target Paths.[ OK ] Reached target Paths.[ 2.864337] systemd[1]: Reached target Remote File Systems.[ OK ] Reached target Remote File Systems.[ 2.884332] systemd[1]: Reached target Slices.[ OK ] Reached target Slices.[ 2.904353] systemd[1]: Reached target Swap.[ OK ] Reached target Swap.[ 2.926684] systemd[1]: Listening on RPCbind Server Activation Socket.[ OK ] Listening on RPCbind Server Activation Socket.[ 2.952357] systemd[1]: Reached target RPC Port Mapper.[ OK ] Reached target RPC Port Mapper.[ 2.974811] systemd[1]: Listening on Syslog Socket.[ OK ] Listening on Syslog Socket.[ 2.996755] systemd[1]: Listening on initctl Compatibility Named Pipe.[ OK ] Listening on initctl Compatibility Named Pipe.[ 3.021190] systemd[1]: Listening on Journal Audit Socket.[ OK ] Listening on Journal Audit Socket.[ 3.044877] systemd[1]: Listening on Journal Socket (/dev/log).[ OK ] Listening on Journal Socket (/dev/log).[ 3.068992] systemd[1]: Listening on Journal Socket.[ OK ] Listening on Journal Socket.[ 3.089178] systemd[1]: Listening on Network Service Netlink Socket.[ OK ] Listening on Network Service Netlink Socket.[ 3.113033] systemd[1]: Listening on udev Control Socket.[ OK ] Listening on udev Control Socket.[ 3.132760] systemd[1]: Listening on udev Kernel Socket.[ OK ] Listening on udev Kernel Socket.[ 3.157436] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System...[ 3.185355] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System...[ 3.221236] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System...[ 3.254757] systemd[1]: Mounting Temporary Directory (/tmp)... Mounting Temporary Directory (/tmp)...[ 3.291289] systemd[1]: Starting Create list of static device nodes for the current kernel... Starting Create list of st…odes for the current kernel...[ 3.329353] systemd[1]: Starting RPC Bind... Starting RPC Bind...[ 3.352450] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.[ 3.376687] systemd[1]: Starting Journal Service... Starting Journal Service...[ 3.417163] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules...[ 3.465101] systemd[1]: Starting Remount Root and Kernel File Systems...[ 3.494470] mmngr: loading out-of-tree module taints kernel. Starting Remount Root and Kernel File Systems...[ 3.516764] rgnmm_drv mmngr: assigned reserved memory node linux,multimedia[ 3.540747] systemd[1]: Starting udev Coldplug all Devices... Starting udev Coldplug all Devices...[ 3.617784] systemd[1]: Started RPC Bind.[ OK ] Started RPC Bind.[ 3.673363] systemd[1]: Mounted Huge Pages File System.[ OK ] Mounted Huge Pages File System.[ 3.698402] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)[ 3.711442] systemd[1]: Mounted POSIX Message Queue File System.[ OK ] Mounted POSIX Message Queue File System.[ 3.766277] systemd[1]: Mounted Kernel Debug File System.[ 3.786761] random: systemd-journal: uninitialized urandom read (16 bytes read)[ OK ] Mounted Kernel Debug File System.[ 3.817594] random: systemd-journal: uninitialized urandom read (16 bytes read)[ 3.826225] systemd[1]: Started Journal Service.[ OK ] Started Journal Service.[ 3.853473] random: systemd-journal: uninitialized urandom read (16 bytes read)[ OK ] Mounted Temporary Directory (/tmp).[ OK ] Started Create list of sta… nodes for the current kernel.[ OK ] Started Remount Root and Kernel File Systems.[ OK ] Started Load Kernel Modules. Mounting NFSD configuration filesystem... Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage...[ 4.053883] systemd-journald[124]: Received client request to flush runtime journal. Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev...[FAILED] Failed to mount NFSD configuration filesystem.See 'systemctl status proc-fs-nfsd.mount' for details.[DEPEND] Dependency failed for NFS server and services.[DEPEND] Dependency failed for NFS Mount Daemon.[ OK ] Mounted Kernel Configuration File System.[ OK ] Started Flush Journal to Persistent Storage.[ OK ] Started Apply Kernel Variables.[ OK ] Started Create Static Device Nodes in /dev.[ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Starting udev Kernel Device Manager...[ OK ] Mounted /var/volatile. Starting Load/Save Random Seed...[ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories...[ OK ] Started udev Kernel Device Manager.[ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown...[ 4.839929] random: systemd: uninitialized urandom read (16 bytes read)[ OK ] Started Update UTMP about System Boot/Shutdown.[ 5.488089] random: crng init done[ 5.491532] random: 60 urandom warning(s) missed due to ratelimiting[ OK ] Started Load/Save Random Seed.[ OK ] Started Network Time Synchronization.[ OK ] Reached target System Time Set.[ OK ] Reached target System Time Synchronized.[ OK ] Started udev Coldplug all Devices.[ OK ] Reached target System Initialization.[ OK ] Started Daily Cleanup of Temporary Directories.[ OK ] Reached target Timers.[ OK ] Listening on D-Bus System Message Bus Socket.[ OK ] Listening on dropbear.socket.[ OK ] Reached target Sockets.[ OK ] Reached target Basic System.[ OK ] Started Kernel Logging Service.[ OK ] Started System Logging Service.[ OK ] Started D-Bus System Message Bus. Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... Starting LSB: Kernel NFS server support... Starting Telephony service...[ OK ] Started optee services. Starting Login Service...[ OK ] Started VIN initializing setting.[ OK ] Started WatchdogTimer.[ OK ] Started IPv6 Packet Filtering Framework.[ OK ] Started IPv4 Packet Filtering Framework.[FAILED] Failed to start LSB: Kernel NFS server support.See 'systemctl status nfsserver.service' for details.[ OK ] Started Telephony service.[ OK ] Reached target Network (Pre). Starting Connection service... Starting Network Service...[ OK ] Created slice system-systemd\x2dbacklight.slice. Starting Load/Save Screen … backlight:lvds_backlight@1...[ OK ] Started Network Service.[ OK ] Started Connection service.[ OK ] Reached target Network.[ OK ] Started NFS status monitor for NFSv2/3 locking.. Starting Permit User Sessions... Starting Target Communication Framework agent...[ 7.682011] ADIN1300 11c20000.ethernet-ffffffff:04: attached PHY driver [ADIN1300] (mii_bus:phy_addr=11c20000.ethernet-ffffffff:04, irq=POLL)[ OK ] Started Load/Save Screen B…of backlight:lvds_backlight@1.[ OK ] Started Permit User Sessions.[ OK ] Started Target Communication Framework agent.[ OK ] Started Login Service.[ OK ] Started Getty on tty1.[ OK ] Started Serial Getty on ttySC0.[ OK ] Reached target Login Prompts.[ OK ] Reached target Multi-User System. Starting Hostname Service... Starting Update UTMP about System Runlevel Changes... Starting WPA supplicant...[ OK ] Started Update UTMP about System Runlevel Changes.[ OK ] Started WPA supplicant.[ OK ] Started Hostname Service.
Rootfs Version : iW-PRHGZ-SC-01-R2.0-REL1.0a-Yocto-Dunfell Poky (Yocto Project Reference Distro) 3.1.26 iWave-G53M ttySC0
BSP: RZG2UL/iW-RainboW-G53M-RZG2UL-OSM/3.0.5LSI: RZG2ULVersion: 3.0.5iWave-G53M login: [ 10.101167] [HYS] Firmware version = 0x3[ 10.138555] input: hy46xx_ts as /devices/virtual/input/input1[ 10.255774] Successfully added driver hy46xx_ts[ 11.925065] ravb 11c20000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off[ 11.932897] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes readyroot[ 15.350508] audit: type=1006 audit(1717493697.518:2): pid=423 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1[ 15.856611] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.[ 16.165222] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.[ 16.409794] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)root@iWave-G53M:~# root@iWave-G53M:~# root@iWave-G53M:~#
Hiii,
Any updates?
Ashritha S
Hi Ashritha,Seems an interesting issue. We will have a look on it.Kind Regards.
Hii,
Can u update it as soon as possibe?
Regards
Hi Ashrita,
Could you try below change?
From:
ret = gpiochip_irqchip_add(chip, irq_chip, 0, handle_level_irq, IRQ_TYPE_NONE);
to:
ret = gpiochip_irqchip_add(chip, &pctrl->irq_chip, 0, handle_level_irq, IRQ_TYPE_NONE);
in drivers/pinctrl/renesas/pinctrl-rzg2l.c
I have tried the changes accordingly, but still it is same
Could you try below patch?
From 25540760d07af4d0d99bcf49db6ed3d852a32d21 Mon Sep 17 00:00:00 2001 From: hienhuynh <[email protected]> Date: Tue, 11 Jun 2024 07:42:09 +0700 Subject: [PATCH] pinctr: renesas: pinctrl-rzg2l: fix support for multiple gpiochips There is a warning when booting to Linux: "gpio gpiochip0: (11030000.pinctrl): detected irqchip that is shared with multiple gpiochips: please fix the driver." Refer commit "gpio: dln2: Use irqchip template" to fix this warning. <ecb55df8f3a8f30cb188a8bd3c9d0b977eb92e09> This makes the driver use the irqchip template to assign properties to the gpio_irq_chip instead of using the explicit calls to gpiochip_irqchip_add(). The irqchip is instead added while adding the gpiochip. Signed-off-by: hienhuynh <[email protected]> --- drivers/pinctrl/renesas/pinctrl-rzg2l.c | 74 ++++++++++++------------- 1 file changed, 36 insertions(+), 38 deletions(-) diff --git a/drivers/pinctrl/renesas/pinctrl-rzg2l.c b/drivers/pinctrl/renesas/pinctrl-rzg2l.c index 1f4cc5eebcff..e83d961bf997 100644 --- a/drivers/pinctrl/renesas/pinctrl-rzg2l.c +++ b/drivers/pinctrl/renesas/pinctrl-rzg2l.c @@ -2251,8 +2251,7 @@ static struct rzg2l_dedicated_configs rzg3s_dedicated_pins[] = { static int rzg2l_gpio_register(struct rzg2l_pinctrl *pctrl) { struct device_node *np = pctrl->dev->of_node; - struct gpio_chip *chip = &pctrl->gpio_chip; - struct irq_chip *irq_chip = &pctrl->irq_chip; + struct gpio_irq_chip *girq; const char *name = dev_name(pctrl->dev); struct of_phandle_args of_args; int ret; @@ -2269,46 +2268,45 @@ static int rzg2l_gpio_register(struct rzg2l_pinctrl *pctrl) return -EINVAL; } - chip->names = pctrl->data->port_pins; - chip->request = rzg2l_gpio_request; - chip->free = rzg2l_gpio_free; - chip->get_direction = rzg2l_gpio_get_direction; - chip->direction_input = rzg2l_gpio_direction_input; - chip->direction_output = rzg2l_gpio_direction_output; - chip->get = rzg2l_gpio_get; - chip->set = rzg2l_gpio_set; - chip->set_config = rzg2l_gpio_set_config; - chip->label = name; - chip->parent = pctrl->dev; - chip->owner = THIS_MODULE; - chip->base = -1; - chip->ngpio = of_args.args[2]; + pctrl->gpio_chip.names = pctrl->data->port_pins; + pctrl->gpio_chip.request = rzg2l_gpio_request; + pctrl->gpio_chip.free = rzg2l_gpio_free; + pctrl->gpio_chip.get_direction = rzg2l_gpio_get_direction; + pctrl->gpio_chip.direction_input = rzg2l_gpio_direction_input; + pctrl->gpio_chip.direction_output = rzg2l_gpio_direction_output; + pctrl->gpio_chip.get = rzg2l_gpio_get; + pctrl->gpio_chip.set = rzg2l_gpio_set; + pctrl->gpio_chip.set_config = rzg2l_gpio_set_config; + pctrl->gpio_chip.label = name; + pctrl->gpio_chip.parent = pctrl->dev; + pctrl->gpio_chip.owner = THIS_MODULE; + pctrl->gpio_chip.base = -1; + pctrl->gpio_chip.ngpio = of_args.args[2]; pctrl->gpio_range.id = 0; pctrl->gpio_range.pin_base = 0; pctrl->gpio_range.base = 0; - pctrl->gpio_range.npins = chip->ngpio; - pctrl->gpio_range.name = chip->label; - pctrl->gpio_range.gc = chip; - - irq_chip->name = dev_name(pctrl->dev); - irq_chip->irq_shutdown = rzg2l_gpio_irq_shutdown; - irq_chip->irq_mask = rzg2l_gpio_irq_mask; - irq_chip->irq_unmask = rzg2l_gpio_irq_unmask; - irq_chip->irq_set_type = rzg2l_gpio_irq_set_type; - irq_chip->irq_set_wake = rzg2l_gpio_irq_set_wake; - irq_chip->flags = IRQCHIP_SET_TYPE_MASKED | IRQCHIP_MASK_ON_SUSPEND; - - ret = gpiochip_irqchip_add(chip, irq_chip, 0, handle_level_irq, - IRQ_TYPE_NONE); - if (ret) { - dev_err(pctrl->dev, "cannot add irqchip\n"); - return ret; - } - - dev_dbg(pctrl->dev, "Registered interrupt controller\n"); - - ret = devm_gpiochip_add_data(pctrl->dev, chip, pctrl); + pctrl->gpio_range.npins = pctrl->gpio_chip.ngpio; + pctrl->gpio_range.name = pctrl->gpio_chip.label; + pctrl->gpio_range.gc = &pctrl->gpio_chip; + + pctrl->irq_chip.name = dev_name(pctrl->dev); + pctrl->irq_chip.irq_shutdown = rzg2l_gpio_irq_shutdown; + pctrl->irq_chip.irq_mask = rzg2l_gpio_irq_mask; + pctrl->irq_chip.irq_unmask = rzg2l_gpio_irq_unmask; + pctrl->irq_chip.irq_set_type = rzg2l_gpio_irq_set_type; + pctrl->irq_chip.irq_set_wake = rzg2l_gpio_irq_set_wake; + pctrl->irq_chip.flags = IRQCHIP_SET_TYPE_MASKED | IRQCHIP_MASK_ON_SUSPEND; + + girq = &pctrl->gpio_chip.irq; + girq->chip = &pctrl->irq_chip; + girq->parent_handler = NULL; + girq->num_parents = 0; + girq->parents = NULL; + girq->default_type = IRQ_TYPE_NONE; + girq->handler = handle_level_irq; + + ret = devm_gpiochip_add_data(pctrl->dev, &pctrl->gpio_chip, pctrl); if (ret) { dev_err(pctrl->dev, "failed to add GPIO controller\n"); return ret; -- 2.25.1
After doing changes according to the patch i am getting errors during compilation,
Below is the error,
CALL scripts/atomic/check-atomics.sh CALL scripts/checksyscalls.sh CHK include/generated/compile.h CC drivers/pinctrl/renesas/pinctrl-rzg2l.odrivers/pinctrl/renesas/pinctrl-rzg2l.c: In function 'rzg2l_gpio_register':drivers/pinctrl/renesas/pinctrl-rzg2l.c:1724:32: error: 'rzg2l_gpio_set_config' undeclared (first use in this function); did you mean 'rzg2l_gpio_configs'? pctrl->gpio_chip.set_config = rzg2l_gpio_set_config; ^~~~~~~~~~~~~~~~~~~~~ rzg2l_gpio_configsdrivers/pinctrl/renesas/pinctrl-rzg2l.c:1724:32: note: each undeclared identifier is reported only once for each function it appears inmake[3]: *** [scripts/Makefile.build:286: drivers/pinctrl/renesas/pinctrl-rzg2l.o] Error 1make[2]: *** [scripts/Makefile.build:503: drivers/pinctrl/renesas] Error 2make[1]: *** [scripts/Makefile.build:503: drivers/pinctrl] Error 2make[1]: *** Waiting for unfinished jobs....make: *** [Makefile:1832: drivers] Error 2make: *** Waiting for unfinished jobs....
Hi Ashritha,
Sorry, I forgot that you are using 3.0.5 (cip36). I based on cip41 (3.0.6). So, please remove this line
pctrl->gpio_chip.set_config = rzg2l_gpio_set_config;
It is supported in later kernel version.
Thanks for the reply, The error got resolved, But can u just brief the changes that u have done?
Basically, I just update the pinctrl driver to adapt with the latest change from GPIO IRQ linux framework.
There is nothing big changes about the implementation.
Thanks for the response
Is this fix is added in the 3.0.6 VLP?
Any updates