hello,
I have read the pdf of project of 'an-r01an3169jj0110-rzt1-ethercat' and 'EtherCAT_SSC_DC'. Ihave compile and download programs success, but EtherCAT not success.
I want to know do I need to start peripherals or add other configurations based on the routine?
What is the EtherCAT debugging process like?How do I debug step by step?
Thank you
The RZ/T1 routine project is base on R7S910017, and I use the IC is R7S910035. What is the difference between these two chips? What modifications should I make to adapt to R7S910035.
Hi Chen,
I recommend you to get the RTK7910022C00000BR board with R7S910017. And the difference between R7S910017 and R7S910035 is described in the TZ/T1 Group datasheet.
The application note and sample program you downloaded were probably tested with the RTK7910022C00000BR board and are provided by Renesas "AS IS". You run it on a board whose specifications are unknown to forum readers, and just say "not success" without giving any detailed explanation.
I don't know your situation, but I think the best thing a kind moderator can do is ask you to explain in more detail.
BR