Error in RZ-V2M v3.0.4 build after DRP-AI and ISP inclusion in the build with respect to 'libcomctl'

The following error was encountered during build time after adding the following line in local conf :

"IMAGE_INSTALL_append = " libcomctl"

This line has been added when I got the following error while running HDMI connectivity with RZ-V2M:

" MACHINE=rzv2m bitbake core-image-bsp
Loading cache: 100% |##########################################################################################################| Time: 0:00:00
Loaded 5298 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'libcomctl' (but /home/cyphertek2/_rzv_vlp_v3.0.4/build/../meta-renesas/meta-rz-common/recipes-core/images/core-image-bsp.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'libcomctl' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['libcomctl']
ERROR: Required build target 'core-image-bsp' has no buildable providers.
Missing or unbuildable dependency chain was: ['core-image-bsp', 'libcomctl'] "

Awaiting for the reply at the earliest

Regards

Sonu S Y

[email protected]