The following error was encountered during build time after adding the following line in local conf :
"IMAGE_INSTALL_append = " libcomctl"
This line has been added when I got the following error while running HDMI connectivity with RZ-V2M:
" MACHINE=rzv2m bitbake core-image-bsp Loading cache: 100% |##########################################################################################################| Time: 0:00:00 Loaded 5298 entries from dependency cache. NOTE: Resolving any missing task queue dependencies ERROR: Nothing RPROVIDES 'libcomctl' (but /home/cyphertek2/_rzv_vlp_v3.0.4/build/../meta-renesas/meta-rz-common/recipes-core/images/core-image-bsp.bb RDEPENDS on or otherwise requires it) NOTE: Runtime target 'libcomctl' is unbuildable, removing... Missing or unbuildable dependency chain was: ['libcomctl'] ERROR: Required build target 'core-image-bsp' has no buildable providers. Missing or unbuildable dependency chain was: ['core-image-bsp', 'libcomctl'] "
Awaiting for the reply at the earliest
Regards
Sonu S Y
[email protected]