Hey Folks,
My Board is not booting up in normal mode instead Its showing SCIF download mode due to parameter error. I tried to flash the bootloader again and i was not being able to write the flash writer to the board it was simply showing the same screen as if it hasn't received the flashwriter. What might be the issue please can anybody help.
Hi anzal,Do you have the EVK or custom board?Also, do you build the flash writer with Yocto?Kind Regards.
I have a custom board and I buit the flashwriter from the source itself using the renesas porting guide and it is working for other board but this one is having some issue. Is it because of malfunctioning spi flash??
logan3c3 said:Is it because of malfunctioning spi flash??
You can put a scope on the spi flash pins to make sure it is reading in data.
If it is working with one board, but not another, it sounds like a hardware issue (yes, SPI Flash)
Okay will do that. When writing the flashwriter there is no response why is that???
Also what hardware issue might be there. Are there any debug methods invoking JTAG tools??