Hi Can you list supported parallel(not lvds parallel bridge) displays for kernel version 5.10 Also if possible can you provide dts entry for parallel display
Hi anzal,
You can refer here (Example of Parallel(RGB) Panel on RZ/G2L (5.10))
Device Tree and Device Drivers - Renesas-wiki - Confluence
He hienhuynh can you list any displays you have used with the above dts entry???
I saw this:
CONFIG_DRM_PANEL_SIMPLE=ySo, is it correct Image that you are deploying your board?
yes, do i have to clean the old build to build new one after modification??
If you build mannually by "make", just need to source SDK, run "make rzv2l_calixto_default_defconfig && make" then get the latest Image + dtb from "arch/arm64/boot/Image" and "arch/arm64/boot/dts"
yes i am following the same method
i will try cleaning all and try to build again
i cleaned the build and tried again same issue
hell hienhuynh, I have found out the issue i have been loading the wrong image all along. Now the display is being probed and halting after that not booting.
this is where the boot is being halted. Can you help?
Could you give us full bootlog?
Maybe halted due to your display.
Could you reboot your board without enable display?
If it can boot normally without display, please share us your devicetree.
we were using an older kernel version now. i have tried it in a 5.10 cip 41 and now booting is happening but some serros were coming i will share you the bootlog and dts
i can reboot my board without display.
Please send me full log when enable display.
thanks for the support hienhuynh the display is up and working.
Nice to hear that. But by the way, could you share the reason why the display can work now?
Is there any missing before?
It will be nice if you share to us. We can improve our support in the future.
yeah i was using old kernel version.
hey, hienhuynh why does parallel display only work in kernel 5.10 cip 41 no other versions??
There was a bug in the driver code when calculating the pixel clock for slow frequencies. Since a parallel LCD is usually slower pixel clock than a MIPI-DSI LCD, maybe that is the reason.