Hi Can you list supported parallel(not lvds parallel bridge) displays for kernel version 5.10 Also if possible can you provide dts entry for parallel display
i did make the config and kernel
here is the defconfig file should i add anything else to this
Please send us file ".config" in your linux directory.
I saw this:
CONFIG_DRM_PANEL_SIMPLE=ySo, is it correct Image that you are deploying your board?
yes, do i have to clean the old build to build new one after modification??
If you build mannually by "make", just need to source SDK, run "make rzv2l_calixto_default_defconfig && make" then get the latest Image + dtb from "arch/arm64/boot/Image" and "arch/arm64/boot/dts"
yes i am following the same method
i will try cleaning all and try to build again
i cleaned the build and tried again same issue
hell hienhuynh, I have found out the issue i have been loading the wrong image all along. Now the display is being probed and halting after that not booting.
this is where the boot is being halted. Can you help?
Hi anzal,
Could you give us full bootlog?
Maybe halted due to your display.
Could you reboot your board without enable display?
If it can boot normally without display, please share us your devicetree.
we were using an older kernel version now. i have tried it in a 5.10 cip 41 and now booting is happening but some serros were coming i will share you the bootlog and dts
i can reboot my board without display.
Please send me full log when enable display.
thanks for the support hienhuynh the display is up and working.