Error obtained, when tried to run the source file after integrating acconeer sensor with RZ/V2M v3.0.4


"root@rzv2m:~# python3 -m HRBR -u
Traceback (most recent call last):
  File "/usr/lib64/python3.8/runpy.py", line 194, in _run_module_as_main
    return _run_code(code, main_globals, None,
  File "/usr/lib64/python3.8/runpy.py", line 87, in _run_code
    exec(code, run_globals)
  File "/home/root/HRBR/_main_.py", line 9, in <module>
    main(module_info)
  File "/usr/lib64/python3.8/site-packages/acconeer/exptool/a111/algo/_standalone_main.py", line 13, in main
    client = et.a111.Client(**et.a111.get_client_args(args))
  File "/usr/lib64/python3.8/site-packages/acconeer/exptool/a111/clients/client.py", line 59, in __init_
    self.subclient = ClientFactory.from_kwargs(protocol=protocol, link=link, **kwargs)
  File "/usr/lib64/python3.8/site-packages/acconeer/exptool/a111/_clients/client_factory.py", line 39, in from_kwargs
    port = cls._handle_passed_serial_port(kwargs.pop("serial_port", None))
  File "/usr/lib64/python3.8/site-packages/acconeer/exptool/a111/_clients/client_factory.py", line 143, in _handle_passed_serial_port
    return cls._get_single_acconeer_module_port(et.utils.get_tagged_serial_ports())
  File "/usr/lib64/python3.8/site-packages/acconeer/exptool/a111/_clients/client_factory.py", line 163, in _get_single_acconeer_module_port
    raise ValueError("Could not auto-detect any Acconeer modules.")
ValueError: Could not auto-detect any Acconeer modules."

Note :Coming to connectivity with USB Cof  RZ/V2M, it's working fine, no problem with connectivity.

In the line of debugging trials, when I am installing acconeer-exptool module through TeratTerm with the command "pip3 install acconeeer-exptool", fetching the following warning:

"

root@rzv2m:~# pip3 install acconeer-exptool
Requirement already satisfied: acconeer-exptool in /usr/lib64/python3.8/site-packages (7.11.1)
Requirement already satisfied: attributes-doc==0.3.0 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (0.3.0)
Requirement already satisfied: attrs>=22.1.0 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (23.2.0)
Requirement already satisfied: cbor2 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (5.6.4)
Requirement already satisfied: exceptiongroup==1.1.1 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (1.1.1)
Requirement already satisfied: h5py<4,>=3.8 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (3.10.0)
Requirement already satisfied: numpy<2,>=1.20 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (1.24.4)
Requirement already satisfied: packaging in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (24.1)
Requirement already satisfied: pandas>=1.3.5 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (2.0.3)
Requirement already satisfied: pyserial>=3.5 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (3.5)
Requirement already satisfied: pyusb>=1.2.1 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (1.2.1)
Requirement already satisfied: pyyaml in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (6.0.1)
Requirement already satisfied: requests<3,>=2.0 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (2.32.3)
Requirement already satisfied: result==0.16.1 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (0.16.1)
Requirement already satisfied: textual==0.1.18 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (0.1.18)
Requirement already satisfied: typing-extensions<5,>=4 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (4.12.2)
Requirement already satisfied: xlsxwriter>=3.1.9 in /usr/lib64/python3.8/site-packages (from acconeer-exptool) (3.2.0)
Requirement already satisfied: rich<13.0.0,>=12.3.0 in /usr/lib64/python3.8/site-packages (from textual==0.1.18->acconeer-exptool) (12.6.0)
Requirement already satisfied: python-dateutil>=2.8.2 in /usr/lib64/python3.8/site-packages (from pandas>=1.3.5->acconeer-exptool) (2.9.0.post0)
Requirement already satisfied: pytz>=2020.1 in /usr/lib64/python3.8/site-packages (from pandas>=1.3.5->acconeer-exptool) (2024.1)
Requirement already satisfied: tzdata>=2022.1 in /usr/lib64/python3.8/site-packages (from pandas>=1.3.5->acconeer-exptool) (2024.1)
Requirement already satisfied: charset-normalizer<4,>=2 in /usr/lib64/python3.8/site-packages (from requests<3,>=2.0->acconeer-exptool) (3.3.2)
Requirement already satisfied: idna<4,>=2.5 in /usr/lib64/python3.8/site-packages (from requests<3,>=2.0->acconeer-exptool) (3.7)
Requirement already satisfied: urllib3<3,>=1.21.1 in /usr/lib64/python3.8/site-packages (from requests<3,>=2.0->acconeer-exptool) (2.2.2)
Requirement already satisfied: certifi>=2017.4.17 in /usr/lib64/python3.8/site-packages (from requests<3,>=2.0->acconeer-exptool) (2024.7.4)
Requirement already satisfied: six>=1.5 in /usr/lib64/python3.8/site-packages (from python-dateutil>=2.8.2->pandas>=1.3.5->acconeer-exptool) (1.16.0)
Requirement already satisfied: commonmark<0.10.0,>=0.9.0 in /usr/lib64/python3.8/site-packages (from rich<13.0.0,>=12.3.0->textual==0.1.18->acconeer-exptool) (0.9.1)
Requirement already satisfied: pygments<3.0.0,>=2.6.0 in /usr/lib64/python3.8/site-packages (from rich<13.0.0,>=12.3.0->textual==0.1.18->acconeer-exptool) (2.18.0)
WARNING: Running pip as the 'root' user can result in broken permissions and conflicting behaviour with the system package manager, possibly rendering your system unusable.It is recommended to use a virtual environment instead: pip.pypa.io/.../venv. Use the --root-user-action option if you know what you are doing and want to suppress this warning.
root@rzv2m:~#"

Note: Here root itself is the user, how can we use another environment to do the task

PFA regarding the queries