RZ/V2L OPENEMP FRAMEWORK

Currently, I am working on the RZ/V2L EVK. I am writing an application on the M33 side using FreeRTOS. In this application, I have a use case where I need to access the file system from the host side (Linux). Is there any example code that can be used on both the M33 side and the Linux side to access the file system?