Hi,
We are working on RZ/G2L using VLP3.0.6 source.
During YOCTO build, gstreamer1.0-omx package fails to fetch.
Tried cleaning and re-compiling the package, but still the issue exists.
Below is the error message from YOCTO build.WARNING: gstreamer1.0-omx-1.16.3-r0 do_fetch: Failed to fetch URL git://anongit.freedesktop.org/gstreamer/common;destsuffix=git/common;name=common, attempting MIRRORS if availableERROR: gstreamer1.0-omx-1.16.3-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export PATH="/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/sysroots-uninative/x86_64-linux/usr/bin:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/recipe-sysroot-native/usr/bin/python3-native:/mnt/xvdb1/Maruti/PRHOZ/g2l/poky/scripts:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/recipe-sysroot/usr/bin/crossscripts:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/recipe-sysroot-native/usr/sbin:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/recipe-sysroot-native/usr/bin:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/recipe-sysroot-native/sbin:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/recipe-sysroot-native/bin:/mnt/xvdb1/Maruti/PRHOZ/g2l/poky/bitbake/bin:/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/hosttools"; export HOME="/home/iwave"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://anongit.freedesktop.org/gstreamer/common /mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/downloads/git2/anongit.freedesktop.org.gstreamer.common --progress failed with exit code 128, no outputERROR: gstreamer1.0-omx-1.16.3-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://anongit.freedesktop.org/gstreamer/common;destsuffix=git/common;name=common')ERROR: Logfile of failure stored in: /mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/tmp/work/aarch64-poky-linux/gstreamer1.0-omx/1.16.3-r0/temp/log.do_fetch.1514050ERROR: Task (/mnt/xvdb1/Maruti/PRHOZ/g2l/build_2/../poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-omx_1.16.3.bb:do_fetch) failed with exit code '1'
Kindly help in resolving the issue.
Hi Maruti,Your error indicates an issue with your internet connection.The repository is up and running.Please make sure you have set this variable from conf/local.conf to:BB_NO_NETWORK = "0"Kind Regards.
Hi Maruti,please switch to VLP 3.0.6-update3 that has just been released today.update3 fixes the gstreamer fetch error.Kind Regards,Stefan