Hello~
When I use the r12an0123xx0300-cn032-ac-servo-solution, I connect to TWINCAT 3.1 on my computer, and I can reach the OP state normally, and I can switch from the OP state to the SO PO IT state.
However, when I try to access the online object dictionary, TWINCAT gives me an error and I can't switch states anymore, it stays in the original state (OP).When I try to locate it, I find that the program is running to Default_Handler.
Is this a CN032 project problem or something else?
Thanks.
I also encountered this problem, at present there is a solution is that the ECAT related interrupt priority low seems to work do not know whether there is a risk. I checked that this interruption should be caused by an unpredictable system error. The key is that it is difficult to locate the cause of the failure. I hope Renesas can solve this bug completely!
I also encountered this problem on the T2L, but the IAR project will not have this problem
Yeah, Recently,I found this ,too.