pcie-mhi
pci_mhi.ko
r8a774b1-hihope-rzg2n-ex.dts
lspci
Hi,
I had a quick look at Quectel's "RM500Q-GL Hardware Design" document, and found the following:
- Turn on the RM500Q-GL module by setting the module's FULL_CARD_POWER_OFF# signal to HIGH (for example, by using the host CPU's GPIO).
- Use AT commands to switch the PCIe operating mode (endpoint mode / root complex mode).
Just to confirm, you performed the initial settings described in the RM500Q-GL manual to make the RM500Q-GL module's PCIe interface operational (for example, as mentioned above), and then tested it, right?
BR
Hi Chris/egret,
Thanks for the reply , Yes we enabled in the kernel
CONFIG_PCIE_RCAR_HOST=yCONFIG_PCIE_RCAR_EP=y.
And Also Done: Modem setings to work in PCIE mode like below
AT+QCFG="data_interface",1,1 //Set network port communication through PCIe interface, and diagnostic port through PCIe interface.
AT+QCFG="pcie/mode",1 //RC Mode:
In the kernel debug we are getting below error:
[ 0.133274] gpio-370 (usb1-reset): hogged as output/low[ 0.133463] gpio_rcar e6055400.gpio: driving 32 GPIOs[ 0.133770] gpio_rcar e6055800.gpio: driving 4 GPIOs[ 0.135466] rcar-pcie fe000000.pcie: host bridge /soc/pcie@fe000000 ranges:[ 0.135492] rcar-pcie fe000000.pcie: Parsing ranges property...[ 0.135509] rcar-pcie fe000000.pcie: IO 0x00fe100000..0x00fe1fffff -> 0x0000000000[ 0.135534] rcar-pcie fe000000.pcie: MEM 0x00fe200000..0x00fe3fffff -> 0x00fe200000[ 0.135554] rcar-pcie fe000000.pcie: MEM 0x0030000000..0x0037ffffff -> 0x0030000000[ 0.135570] rcar-pcie fe000000.pcie: MEM 0x0038000000..0x003fffffff -> 0x0038000000[ 0.135585] rcar-pcie fe000000.pcie: Parsing dma-ranges property...[ 0.135596] rcar-pcie fe000000.pcie: IB MEM 0x0040000000..0x00bfffffff -> 0x0040000000[ 0.199776] rcar-pcie fe000000.pcie: PCIe link down[ 0.200014] rcar-pcie ee800000.pcie: host bridge /soc/pcie@ee800000 ranges:[ 0.200029] rcar-pcie ee800000.pcie: Parsing ranges property...[ 0.200044] rcar-pcie ee800000.pcie: IO 0x00ee900000..0x00ee9fffff -> 0x0000000000[ 0.200066] rcar-pcie ee800000.pcie: MEM 0x00eea00000..0x00eebfffff -> 0x00eea00000[ 0.200085] rcar-pcie ee800000.pcie: MEM 0x00c0000000..0x00c7ffffff -> 0x00c0000000[ 0.200100] rcar-pcie ee800000.pcie: MEM 0x00c8000000..0x00cfffffff -> 0x00c8000000[ 0.200111] rcar-pcie ee800000.pcie: Parsing dma-ranges property...[ 0.200145] rcar-pcie ee800000.pcie: IB MEM 0x0040000000..0x00bfffffff -> 0x0040000000[ 0.267751] rcar-pcie ee800000.pcie: PCIe link down[ 0.304727] SuperH (H)SCI(F) driver initialized.
My dts entries is as below:
&pciec1 { status = "okay";};&pciec0_ep { status = "okay";
}.
And I followed the instruction given in the :
https://github.com/renesas-rz/rzg2-pcie-endpoint.
root@hihope-rzg2n:~# ls /sys/class/pci_epc/fe000000.pcie-eproot@hihope-rzg2n:~# ls /sys/bus/pci-epf/driverspci_epf_testroot@hihope-rzg2n:~# mount -t configfs none /sys/kernel/configmount: /sys/kernel/config: none already mounted or mount point busy.root@hihope-rzg2n:~# cd /sys/kernel/config/pci_eproot@hihope-rzg2n:/sys/kernel/config/pci_ep# mkdir functions/pci_epf_test/func1root@hihope-rzg2n:/sys/kernel/config/pci_ep# ls functions/pci_epf_test/func1/baseclass_code cache_line_size deviceid interrupt_pin msi_interrupts msix_interrupts progif_code revid subclass_code subsys_id subsys_vendor_id vendoridroot@hihope-rzg2n:/sys/kernel/config/pci_ep# cd /sys/kernel/config/pci_ep/functions/pci_epf_test/func1/root@hihope-rzg2n:/sys/kernel/config/pci_ep/functions/pci_epf_test/func1# cat vendorid0xffffroot@hihope-rzg2n:/sys/kernel/config/pci_ep/functions/pci_epf_test/func1# cat interrupt_pin0x0001root@hihope-rzg2n:/sys/kernel/config/pci_ep/functions/pci_epf_test/func1# lsbaseclass_code cache_line_size deviceid interrupt_pin msi_interrupts msix_interrupts progif_code revid subclass_code subsys_id subsys_vendor_id vendoridroot@hihope-rzg2n:/sys/kernel/config/pci_ep/functions/pci_epf_test/func1# cd /sys/kernel/config/pci_eproot@hihope-rzg2n:/sys/kernel/config/pci_ep# echo 0x1912 > functions/pci_epf_test/func1/vendoridroot@hihope-rzg2n:/sys/kernel/config/pci_ep# echo 0x002b > functions/pci_epf_test/func1/deviceid # RZ/G2Nroot@hihope-rzg2n:/sys/kernel/config/pci_ep# echo 16 > functions/pci_epf_test/func1/msi_interruptsroot@hihope-rzg2n:/sys/kernel/config/pci_ep# cd /sys/kernel/config/pci_eproot@hihope-rzg2n:/sys/kernel/config/pci_ep# ln -s functions/pci_epf_test/func1/ controllers/fe000000.pcie_ep/ln: target `controllers/fe000000.pcie_ep/' is not a directory: No such file or directoryroot@hihope-rzg2n:/sys/kernel/config/pci_ep# ln -s functions/pci_epf_test/func1/ controllers/fe000000.pcie-ep/root@hihope-rzg2n:/sys/kernel/config/pci_ep# cd /sys/kernel/config/pci_eproot@hihope-rzg2n:/sys/kernel/config/pci_ep# echo 1 > controllers/fe000000.pcie_ep/start-sh: controllers/fe000000.pcie_ep/start: No such file or directoryroot@hihope-rzg2n:/sys/kernel/config/pci_ep# echo 1 > controllers/fe000000.pcie-ep/ func1/ start root@hihope-rzg2n:/sys/kernel/config/pci_ep# echo 1 > controllers/fe000000.pcie-ep/start root@hihope-rzg2n:/sys/kernel/config/pci_ep# lspci -vvxxroot@hihope-rzg2n:/sys/kernel/config/pci_ep#
SO lspci -vvxx is not showing any device attached to PCI.
Please guide us what are we missing here.
Thanks for your time and guidance.Please help how can we go about it.
BR,
Nagaraja
I think that the PCIe of the RM500Q-GL module is not working for some reason.
As you may know, "PCIe link down" means that the connection between the RM500Q-GL module and the custom board has been lost. Some of common causes are:
2. to 5. aside, what about 1.?As I wrote in my previous comment, the RM500Q-GL module may need to be woken up by the FULL_CARD_POWER_OFF# signal.
By the way, what is the OC of your RM500Q-GL module?
Hi egret,
Thanks for the reply, we are using RM500QGLAB-M20-SGASA, and the Kernel version is 5.10.158 from renesas 3.0.3-SDK. We have checked the common causes that you mensnioned above and look fine
We tested , FULL_CARD_POWER_OFF# signal.
Reset singnal is high and reference clock is 100MHZ
Thanks and Regards,
Reading some Quectel forum threads, it seems like this module has some quirks.
RM500Q-GL - PCIe interface not workingRM500Q-GL not enumeratedRM500Q-GL PCIe efuse
I think it's hard to get advice from people familiar with the RM500Q-GL quirks on this forum, so a good first step would be to search/ask for solutions on Quectel forums to detect your module..
You may have already done this...