[FAILED] Failed to start Comctl daemon in RZV2M based custom board boot up.

Hi All,

I am trying to bring up the OnSemi AR1335 image sensor on an RZV2M-based custom board. I included all the ISP packages for AR1335 and related packages with VLP 3.0.4 in the Yocto build. The AR1335 is connected over the MIPI-CSI Channel 0 interface.

I prepared the SD card as mentioned in the startup guide, but during the custom board boot-up, I am getting the message "[FAILED] Failed to start Comctl daemon." However, when the same SD card is used in the RZV2M EVK board, it does not show any failed messages related to "comctl" and boots up successfully. For your reference, the complete boot-up log and short logs are attached.

[  OK  ] Reached target Login Prompts.
[FAILED] Failed to start Comctl daemon.
See 'systemctl status comctld.service' for details.
[  OK  ] Started Target Communication Framework agent.
[  OK  ] Started Modem Manager.
[  OK  ] Reached target Multi-User System.
         Starting Hostname Service...
         Starting Update UTMP about System Runlevel Changes...
         Starting WPA supplicant...
[  OK  ] Started Update UTMP about System Runlevel Changes.
[  OK  ] Stopped Comctl daemon.
         Starting Comctl daemon...
[  OK  ] Started WPA supplicant.
[   12.498740] audit: type=1701 audit(1724849725.582:4): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=207 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1
[FAILED] Failed to start Comctl daemon.
See 'systemctl status comctld.service' for details.
[  OK  ] Stopped Comctl daemon.
         Starting Comctl daemon...
[  OK  ] Started Hostname Service.
[   13.047115] audit: type=1701 audit(1724849726.130:5): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=223 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1
[FAILED] Failed to start Comctl daemon.
See 'systemctl status comctld.service' for details.
[   13.790765] audit: type=1701 audit(1724849726.874:6): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=240 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1

If anyone has any ideas, please suggest a fix.

Thanks

[BL1] Boot Loader VLP V3.0.4 for RZV2M
                                      [BL1] eMMC initialized
                                                            [BL1] Loaded the boot parameter for 2nd boot
                                                                                                        [BL1] Loaded the 2nd boot loader
       [BL1] the 2nd bootloader start
                                     [BL2] 2nd boot loader entered for RZV2M_EVK
                                                                                [BL2] DDR initialization completed_M_RZV2M_EVK
                                                                                                                              [BL2] Loaded the boot parameter for U-Boot
                                       [BL2] Loaded the U-Boot
                                                              [BL2] the U-Boot start


U-Boot 2021.10 (May 31 2023 - 08:04:36 +0000) for RZ/V2M Linux Package VLP V3.0.4

Model: RZ/V2M
DRAM:  4 GiB
MMC:   sd@85000000: 0, sd@85020000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
Net:   No ethernet found.

Hit any key to stop autoboot:  0 
19522048 bytes read in 895 ms (20.8 MiB/s)
24031 bytes read in 3 ms (7.6 MiB/s)
Moving Image from 0x180080000 to 0x180200000, end=181510000
## Flattened Device Tree blob at 180000000
   Booting using the fdt blob at 0x180000000
   Loading Device Tree to 000000007fff7000, end 000000007ffffdde ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.10.175-cip29-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 8.3.0, GNU ld (GNU Binutils) 2.31.1) #1 SMP PREEMPT Tue Apr 5 23:00:00 UTC 2011
[    0.000000] Machine model: Renesas EVK based on r9a09g011gbg
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x00000001b8000000, size 128 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma@1B8000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x00000001ff800000, size 4 MiB
[    0.000000] OF: reserved mem: initialized node image_buf@0, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x000000007c000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000001ffbfffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x000000007c000000-0x000000007fefffff]
[    0.000000]   node   0: [mem 0x000000007ff00000-0x000000007fffffff]
[    0.000000]   node   0: [mem 0x0000000180000000-0x00000001ffbfffff]
[    0.000000] Initmem setup node 0 [mem 0x000000007c000000-0x00000001ffbfffff]
[    0.000000] percpu: Embedded 23 pages/cpu s55384 r8192 d30632 u94208
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 531216
[    0.000000] Kernel command line: root=/dev/mmcblk0p2 rootwait rootfstype=ext4 rw
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: Cannot allocate buffer
[    0.000000] Memory: 1355460K/2158592K available (12096K kernel code, 1144K rwdata, 3732K rodata, 1984K init, 391K bss, 667964K reserved, 135168K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x000000008202f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
[    0.000005] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
[    0.000275] Console: colour dummy device 80x25
[    0.000688] printk: console [tty0] enabled
[    0.000732] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
[    0.000759] pid_max: default: 32768 minimum: 301
[    0.000915] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.000957] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.002490] rcu: Hierarchical SRCU implementation.
[    0.003010] Detected Renesas RZ/V2M (r9a09g011gbg)
[    0.003030] EFI services will not be available.
[    0.003133] smp: Bringing up secondary CPUs ...
[    0.003149] smp: Brought up 1 node, 1 CPU
[    0.003161] SMP: Total of 1 processors activated.
[    0.003180] CPU features: detected: 32-bit EL0 Support
[    0.003196] CPU features: detected: CRC32 instructions
[    0.003211] CPU features: detected: 32-bit EL1 Support
[    0.010509] CPU: All CPU(s) started at EL2
[    0.010559] alternatives: patching kernel code
[    0.011474] devtmpfs: initialized
[    0.015948] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.015994] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
[    0.020537] pinctrl core: initialized pinctrl subsystem
[    0.021317] DMI not present or invalid.
[    0.021813] NET: Registered protocol family 16
[    0.023482] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.023575] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.023635] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.023712] audit: initializing netlink subsys (disabled)
[    0.024404] thermal_sys: Registered thermal governor 'step_wise'
[    0.024547] cpuidle: using governor menu
[    0.024782] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.024825] ASID allocator initialised with 65536 entries
[    0.028180] audit: type=2000 audit(0.020:1): state=initialized audit_enabled=0 res=1
[    0.041593] PFC_RZV2M b6250000.pin-controller: Init external interrupt controller success.
[    0.041634] PFC_RZV2M b6250000.pin-controller: RZ/V pin controller successfully registered
[    0.051312] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.051346] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.051363] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.051379] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.053087] cryptd: max_cpu_qlen set to 1000
[    0.057354] PFC_RZV2M b6250000.pin-controller: 20 GPIO nodes are registered
[    0.059960] iommu: Default domain type: Translated 
[    0.060888] vgaarb: loaded
[    0.061201] SCSI subsystem initialized
[    0.061607] usbcore: registered new interface driver usbfs
[    0.061658] usbcore: registered new interface driver hub
[    0.061699] usbcore: registered new device driver usb
[    0.062306] mc: Linux media interface: v0.10
[    0.062342] videodev: Linux video capture interface: v2.00
[    0.062415] pps_core: LinuxPPS API ver. 1 registered
[    0.062429] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[    0.062458] PTP clock support registered
[    0.063213] Advanced Linux Sound Architecture Driver Initialized.
[    0.063963] clocksource: Switched to clocksource arch_sys_counter
[    0.064151] VFS: Disk quotas dquot_6.6.0
[    0.064211] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.070140] NET: Registered protocol family 2
[    0.070478] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.072575] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[    0.072654] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.072921] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[    0.073414] TCP: Hash tables configured (established 32768 bind 32768)
[    0.073546] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.073651] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.073874] NET: Registered protocol family 1
[    0.074399] RPC: Registered named UNIX socket transport module.
[    0.074416] RPC: Registered udp transport module.
[    0.074428] RPC: Registered tcp transport module.
[    0.074440] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.075285] PCI: CLS 0 bytes, default 64
[    0.075874] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    0.076349] kvm [1]: IPA Size Limit: 40 bits
[    0.077142] kvm [1]: vgic interrupt IRQ11
[    0.077231] kvm [1]: Hyp mode initialized successfully
[    0.078853] Initialise system trusted keyrings
[    0.079003] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[    0.085572] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.086246] NFS: Registering the id_resolver key type
[    0.086314] Key type id_resolver registered
[    0.086328] Key type id_legacy registered
[    0.086424] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.086442] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.086478] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    0.087074] Key type asymmetric registered
[    0.087090] Asymmetric key parser 'x509' registered
[    0.087131] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.087153] io scheduler mq-deadline registered
[    0.087167] io scheduler kyber registered
[    0.091395] rzv2m-pcie 85030000.pcie: host bridge /soc/pcie@85030000 ranges:
[    0.091454] rzv2m-pcie 85030000.pcie:      MEM 0x00c0000000..0x00c01fffff -> 0x00c0000000
[    0.091484] rzv2m-pcie 85030000.pcie:      MEM 0x00c0300000..0x00c82fffff -> 0x00c0300000
[    0.091524] rzv2m-pcie 85030000.pcie:   IB MEM 0x0180000000..0x01ffffffff -> 0x0180000000
[    0.899966] rzv2m-pcie 85030000.pcie: PCIe link down
[    0.934385] Serial: 8250/16550 driver, 2 ports, IRQ sharing disabled
[    0.935873] a4040000.serial: ttyS0 at MMIO 0xa4040000 (irq = 68, base_baud = 3000000) is a R8ARZV2M16750
[    1.758641] printk: console [ttyS0] enabled
[    1.763272] SuperH (H)SCI(F) driver initialized
[    1.776976] loop: module loaded
[    1.782170] rzv2m_csi a4020200.spi: probed
[    1.787382] tun: Universal TUN/TAP device driver, 1.6
[    1.792640] CAN device driver interface
[    1.796805] e1000e: Intel(R) PRO/1000 Network Driver
[    1.801827] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    1.808123] PPP generic driver version 2.4.2
[    1.812563] Broadcom 43xx driver loaded [ Features: PNS ]
[    1.818090] usbcore: registered new interface driver asix
[    1.823564] usbcore: registered new interface driver ax88179_178a
[    1.829751] usbcore: registered new interface driver cdc_ether
[    1.835647] usbcore: registered new interface driver net1080
[    1.841374] usbcore: registered new interface driver cdc_subset
[    1.847359] usbcore: registered new interface driver zaurus
[    1.853015] usbcore: registered new interface driver cdc_ncm
[    1.858744] usbcore: registered new interface driver qmi_wwan_q
[    1.864730] usbcore: registered new interface driver qmi_wwan
[    1.870640] VFIO - User Level meta-driver version: 0.3
[    1.876069] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.882660] ehci-pci: EHCI PCI platform driver
[    1.887162] ehci-platform: EHCI generic platform driver
[    1.892555] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[    1.898790] ohci-pci: OHCI PCI platform driver
[    1.903294] ohci-platform: OHCI generic platform driver
[    1.908988] xhci-hcd 85060000.usb: xHCI Host Controller
[    1.914285] xhci-hcd 85060000.usb: new USB bus registered, assigned bus number 1
[    1.921765] xhci-hcd 85060000.usb: USB bus 1 deregistered
[    1.927482] usbcore: registered new interface driver cdc_acm
[    1.933196] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.941292] usbcore: registered new interface driver cdc_wdm
[    1.947029] usbcore: registered new interface driver usb-storage
[    1.953148] usbcore: registered new interface driver option
[    1.958778] usbserial: USB Serial support registered for GSM modem (1-port)
[    1.965807] usbcore: registered new interface driver qcaux
[    1.971344] usbserial: USB Serial support registered for qcaux
[    1.977239] usbcore: registered new interface driver qcserial
[    1.983037] usbserial: USB Serial support registered for Qualcomm USB modem
[    1.991461] xhci-hcd 85060000.usb: xHCI Host Controller
[    1.996744] renesas_usb3 85070000.usb: probed
[    2.001149] xhci-hcd 85060000.usb: new USB bus registered, assigned bus number 1
[    2.009118] mousedev: PS/2 mouse device common for all mice
[    2.015926] xhci-hcd 85060000.usb: hcc params 0x0140fe8d hci version 0x110 quirks 0x0000000000010010
[    2.025190] usbcore: registered new interface driver usbtouchscreen
[    2.031636] i2c /dev entries driver
[    2.035563] xhci-hcd 85060000.usb: irq 63, io mem 0x85060000
[    2.041479] rzv2m-i2c a4030000.i2c: probed
[    2.046083] rzv2m-i2c a4030100.i2c: probed
[    2.050368] xhci-hcd 85060000.usb: xHCI Host Controller
[    2.057371] v4l2-comctl0: V4L2 capture device registered as 'video0'
[    2.063788] xhci-hcd 85060000.usb: new USB bus registered, assigned bus number 2
[    2.071234] comctl_probe is successfully.
[    2.075299] xhci-hcd 85060000.usb: Host supports USB 3.1 Enhanced SuperSpeed
[    2.082424] allocated comctl device '241 0'
[    2.086726] comctl_device : created correctly
[    2.091647] hub 1-0:1.0: USB hub found
[    2.095578] rzv2m_poweroff_reset a3700000.poweroff-reset: RZ/V2M poweroff-reset driver registered
[    2.104552] hub 1-0:1.0: 1 port detected
[    2.108812] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    2.117396] timeout_min = 21845
[    2.120964] timeout_max = 89478485
[    2.124492] hub 2-0:1.0: USB hub found
[    2.129521] renesas_sdhi_internal_dmac 85000000.sd: Got CD GPIO
[    2.135695] hub 2-0:1.0: 1 port detected
[    2.139960] ledtrig-cpu: registered to indicate activity on CPUs
[    2.147999] usbcore: registered new interface driver usbhid
[    2.153618] usbhid: USB HID core driver
[    2.158253] a4000400.timer:probed
[    2.162017] a4000480.timer:probed
[    2.165616] a4000500.timer:probed
[    2.169381] a4000580.timer:probed
[    2.172984] a4000600.timer:probed
[    2.176699] a4000680.timer:probed
[    2.180287] a4000700.timer:probed
[    2.183868] a4000780.timer:probed
[    2.187463] a4000800.timer:probed
[    2.191128] a4000880.timer:probed
[    2.194814] a4000900.timer:probed
[    2.198417] a4000980.timer:probed
[    2.201884] renesas_sdhi_internal_dmac 85000000.sd: mmc0 base at 0x0000000085000000, max clock rate 200 MHz
[    2.212066] a4000a00.timer:probed
[    2.215695] a4000a80.timer:probed
[    2.219672] a4000b00.timer:probed
[    2.223324] a4000b80.timer:probed
[    2.227670] drpai-rz 83000000.drpai: DRP-AI Driver version : 2.10 rel.1 V2M
[    2.234750] drpai-rz 83000000.drpai: sysctrl register region start 0x00000000A3F03000
[    2.242770] drpai-rz 83000000.drpai: DRP-AI memory region start 0x00000001C0000000, size 0x20000000
[    2.252013] drpai-rz 83000000.drpai: linux-memory-region start 0x0000000180000000, size 0x7FC00000
[    2.261131] drpai-rz 83000000.drpai: DRP base address 0x83000000, size 0x01000000
[    2.268710] drpai-rz 83000000.drpai: AI-MAC base address 0x84000000, size 0x00400000
[    2.278514] NET: Registered protocol family 10
[    2.283852] Segment Routing with IPv6
[    2.287668] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    2.294252] NET: Registered protocol family 17
[    2.298851] can: controller area network core
[    2.303324] NET: Registered protocol family 29
[    2.307833] can: raw protocol
[    2.310923] can: broadcast manager protocol
[    2.315168] can: netlink gateway - max_hops=1
[    2.319745] Key type dns_resolver registered
[    2.324531] registered taskstats version 1
[    2.328689] Loading compiled-in X.509 certificates
[    2.342381] mmc0: new high speed SDHC card at address 59b4
[    2.348409] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    2.356855] mmcblk0: mmc0:59b4 SDU1  3.67 GiB 
[    2.362455]  mmcblk0: p1 p2
[    2.367629] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    2.374530] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    2.383255] ALSA device list:
[    2.386345]   No soundcards found.
[    2.389828] cfg80211: failed to load regulatory.db
[    2.421244] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.429573] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.436967] devtmpfs: mounted
[    2.441124] Freeing unused kernel memory: 1984K
[    2.445857] Run /sbin/init as init process
[    2.904480] systemd[1]: System time before build time, advancing clock.
[    2.956716] systemd[1]: systemd 244 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[    2.978560] systemd[1]: Detected architecture arm64.

Welcome to Poky (Yocto Project Reference Distro) 3.1.21 (dunfell)!

[    3.008906] systemd[1]: Set hostname to <rzv2m>.
[    3.353193] systemd[1]: Configuration file /lib/systemd/system/watchdog.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[    3.520285] random: systemd: uninitialized urandom read (16 bytes read)
[    3.527244] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[    3.540047] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[    3.551447] systemd[1]: Created slice system-getty.slice.
[  OK  ] Created slice system-getty.slice.
[    3.572146] random: systemd: uninitialized urandom read (16 bytes read)
[    3.580068] systemd[1]: Created slice system-serial\x2dgetty.slice.
[  OK  ] Created slice system-serial\x2dgetty.slice.
[    3.604124] random: systemd: uninitialized urandom read (16 bytes read)
[    3.611996] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    3.632437] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password …ts to Console Directory Watch.
[    3.656302] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R…uests [    3.667995] usb 1-1: new high-speed USB device number 2 using xhci-hcd
to Wall Directory Watch.
[    3.688241] systemd[1]: Reached target Host and Network Name Lookups.
[  OK  ] Reached target Host and Network Name Lookups.
[    3.712119] systemd[1]: Reached target Paths.
[  OK  ] Reached target Paths.
[    3.732118] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    3.752105] systemd[1]: Reached target Slices.
[  OK  ] Reached target Slices.
[    3.772119] systemd[1]: Reached target Swap.
[  OK  ] Reached target Swap.
[    3.793603] systemd[1]: Listening on Syslog Socket.
[  OK  ] Listening on Syslog Socket.
[    3.816464] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    3.841040] systemd[1]: Listening on Journal Audit Socket.
[  OK  ] Listening on Journal Audit Socket    3.850925] option 1-1:1.0: GSM modem (1-port) converter detected
0m.
[    3.859084] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0
[    3.868700] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/l[    3.880098] option 1-1:1.1: GSM modem (1-port) converter detected
og).
[    3.887160] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1
[    3.895072] option 1-1:1.2: GSM modem (1-port) converter detected
[    3.902013] systemd[1]: Listening on Journal Socket.
[    3.907273] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2
[  OK  ] Listening on Journal Socket.[    3.915166] option 1-1:1.3: GSM modem (1-port) converter detected

[    3.926242] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB3
[    3.934563] qmi_wwan_q 1-1:1.4: cdc-wdm0: USB WDM device
[    3.941016] systemd[1]: Listening on Network Service Netlink Socket.
[    3.947854] qmi_wwan_q 1-1:1.4: Quectel RM520N-GL work on RawIP mode
[  OK  ] Listening on Network Service Netlin[    3.956835] qmi_wwan_q 1-1:1.4: rx_urb_size = 31744
k Socket.
[    3.965542] qmi_wwan_q 1-1:1.4 wwan0: register 'qmi_wwan_q' at usb-85060000.usb-1, RMNET/USB device, be:8e:01:50:5a:36
[    3.977816] systemd[1]: Listening on udev Control Socket.
[    3.983850] net wwan0: qmap_register_device wwan0_1
[  OK  ] Listening on udev Control Socket.
[    4.004583] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    4.028243] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    4.056239] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    4.088131] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    4.120647] systemd[1]: Mounting Temporary Directory (/tmp)...
         Mounting Temporary Directory (/tmp)...
[    4.149759] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[    4.161350] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[    4.175479] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    4.208756] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    4.250056] systemd[1]: Starting Remount Root and Kernel File Systems...
[    4.265860] u_dma_buf: loading out-of-tree module taints kernel.
         Starting Remount Root and Kernel File Systems...
[    4.292709] u-dma-buf udmabuf@0: assigned reserved memory node image_buf@0
[    4.303599] systemd[1]: Starting udev Coldplug all Devices...
[    4.321811] u-dma-buf udmabuf0: driver version = 3.2.4
         Starting udev Coldplug all Devices...
[    4.350686] u-dma-buf udmabuf0: major number   = 237
[    4.366994] systemd[1]: Mounted Huge Pages File System.
[    4.384176] u-dma-buf udmabuf0: minor number   = 0
[  OK  ] Mounted Huge Pages File System.[    4.400162] u-dma-buf udmabuf0: phys address   = 0x00000001ff800000

[    4.410247] systemd[1]: Mounted POSIX Message Queue File System.
[    4.422155] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[  OK  ] Mounted POSIX Message Queue File System.
[    4.446092] u-dma-buf udmabuf0: buffer size    = 4194304
[    4.456909] systemd[1]: Mounted Kernel Debug File System.
[  OK  ] Mounted Kernel Debug File System    4.478860] u-dma-buf udmabuf@0: driver installed.
m.
[    4.498661] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Temporary Directory (/tmp).
[  OK  ] Started Load Kernel Modules.
[  OK  ] Started Remount Root and Kernel File Systems.
[    4.590411] random: systemd: uninitialized urandom read (16 bytes read)
         Mounting Kernel Configuration File System.[    4.615876] random: systemd-journal: uninitialized urandom read (16 bytes read)
..
[    4.632520] random: systemd: uninitialized urandom read (16 bytes read)
         Starting Flush Journal to Persistent Storage...
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev...
[    4.712310] systemd-journald[96]: Received client request to flush runtime journal.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Started Flush Journal to Persistent Storage.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started Create Static Device Nodes in /dev.
[  OK  ] Reached target Local File Systems (Pre).
         Mounting /var/volatile...
         Starting udev Kernel Device Manager...
[  OK  ] Mounted /var/volatile.
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Update UTMP about System Boot/Shutdown...
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Started udev Kernel Device Manager.
[  OK  ] Started udev Coldplug all Devices.
[    5.824815] random: systemd: uninitialized urandom read (16 bytes read)
[    5.864079] random: systemd-journal: uninitialized urandom read (16 bytes read)
         Starting udev Wait for Complete Device Initialization...
[  OK  ] Started Network Time Synchronizatio[    5.952435] random: systemd-journal: uninitialized urandom read (16 bytes read)
n.
[  OK  ] Reached target System Time Set.
[  OK  ] Reached target System Time Synchronized.
[    6.876032] random: crng init done
[    6.879479] random: 56 urandom warning(s) missed due to ratelimiting
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Reached target Hardware activated USB gadget.
[  OK  ] Started udev Wait for Complete Device Initialization.
[  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target Timers.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting sshd.socket.
[  OK  ] Listening on sshd.socket.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
         Starting Modem Manager...
[  OK  ] Started Kernel Logging Service.
[  OK  ] Started System Logging Service.
         Starting Comctl daemon...
[  OK  ] Started D-Bus System Message Bus.
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
         Starting Telephony service...
         Starting rng-tools.service...
         Starting Login Service...
[  OK  ] Started VIN initializing setting.
[  OK  ] Started WatchdogTimer.
[  OK  ] Started IPv6 Packet Filtering Framework.
[  OK  ] Started IPv4 Packet Filtering Framework.
[  OK  ] Started rng-tools.service.
[  OK  ] Reached target Network (Pre).[   10.532389] audit: type=1701 audit(1724849723.618:2): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=143 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1

         Starting Connection service...
         Starting Network Service...
[  OK  ] Started Telephony service.
[FAILED] Failed to start Comctl daemon.
See 'systemctl status comctld.service' for details.
[  OK  ] Stopped Comctl daemon.
         Starting Comctl daemon...
[  OK  ] Started Network Service.
[   11.423085] audit: type=1701 audit(1724849724.506:3): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=179 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1
[  OK  ] Started Connection service.
[  OK  ] Reached target Network.
         Starting Permit User Sessions...
         Starting Target Communication Framework agent...
[  OK  ] Started Login Service.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS0.
[  OK  ] Reached target Login Prompts.
[FAILED] Failed to start Comctl daemon.
See 'systemctl status comctld.service' for details.
[  OK  ] Started Target Communication Framework agent.
[  OK  ] Started Modem Manager.
[  OK  ] Reached target Multi-User System.
         Starting Hostname Service...
         Starting Update UTMP about System Runlevel Changes...
         Starting WPA supplicant...
[  OK  ] Started Update UTMP about System Runlevel Changes.
[  OK  ] Stopped Comctl daemon.
         Starting Comctl daemon...
[  OK  ] Started WPA supplicant.
[   12.498740] audit: type=1701 audit(1724849725.582:4): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=207 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1
[FAILED] Failed to start Comctl daemon.
See 'systemctl status comctld.service' for details.
[  OK  ] Stopped Comctl daemon.
         Starting Comctl daemon...
[  OK  ] Started Hostname Service.
[   13.047115] audit: type=1701 audit(1724849726.130:5): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=223 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1
[FAILED] Failed to start Comctl daemon.
See 'systemctl status comctld.service' for details.
[   13.790765] audit: type=1701 audit(1724849726.874:6): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=240 comm="comctld" exe="/usr/bin/comctld" sig=11 res=1

Poky (Yocto Project Reference Distro) 3.1.21 rzv2m ttyS0

BSP: RZV2M/RZV2M Evaluation Board Kit/3.0.4
LSI: RZV2M
Version: 3.0.4
rzv2m login: root
[   16.573992] audit: type=1006 audit(1724849729.658:7): pid=254 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
root@rzv2m:~# 
root@rzv2m:~# 
root@rzv2m:~# 
root@rzv2m:~# ls
PCIe_MHI_Driver  RZV_AI_Eva_SW	image_capture_app  image_capture_app_with_logs	minicom.log  qConnManager