Hello,
We are using VLP 305 u3 on a custom G2LC board, after running Firefox no GPU error is indicated and Firefox crashes.
sh-5.0 firefox https://vekatech.comCrash Annotation GraphicsCriticalError: | [0][GFX1-]: No GPUs detected via PCI (t=3.51055) [GFX1-]: No GPUs detected via PCICrash Annotation GraphicsCriticalError: 1[0][GFX1-]: No GPUs detected via PCI (t=3.51055) |[1][GFX1-]: Failed to create EGLCo ntext!: 0x300c (t=3.57566) [GFX1-]: Failed to create EGLContext!: 0x300c[Parent 287, Main Thread] WARNING: gak_window_get_scale_factor: assertion 'GDK_IS_WINDOW (window)' failed: 'glib warning', fi le /hone/rzv21/work_data/yocto/work/krzg21c/vip_305/yocto/yocto_305/build/tmp/vork/aarch64-poky-linux/firefox/102.15.1esr-r0/firefox-102.15.1/toolkit/xre/nsSigHandlers.cpp:167(firefox-default:287): Gdk-CRITICAL **: 15:49:31.279: gdk_ window_get_scale_factor: assertion 'GDK_IS_WINDOU (window)' failedCrash Annotation GraphicsCriticalError: |[0][GFX1-]: No GPUs detected via PCI (t=3.51055) | [1][GFX1-]: Failed to create ntextl: 0x300c (t=3.57566) |[2][GFX1-]: Wayland protocol error: dg_un_base@18: error 4: xg_surface buffer (921 x 577) does not natch the configured maximized state (1024 x 568)(t=11.5872) [GFX1-]: Wayland protocol error: xg_un_base@18: error 4: xg_surface buffer (921 x 577) does not match the conf igured maxinized state (1024 x 568)Gdk-Message: 15:49:38.335: Error 71 (Protocol error) dispatching to Wayland display.Exiting dueto channel error.Exiting due to channel error. sh-5.0# Exiting due to channel error.Exiting due to channel error.
Any suggestions how to proceed?
BR,
Teodor
Hi Teodor,Please provide more details about your issue.What command do you execute to launch Firefox?Did you use the HTML5 package provided on Renesas Website for VLP 3.0.5.Kind Regards.
Yes, the same package.
We use "firefox https://vekatech.com" for launching .
Hi !
Is anything that I could provide as information in order to get some hint?
Hi Teodor,What is the output of the command:cat /etc/environmentKind Regards.
Hi!
This is the output!
root@vkrzg2lc:~# cat /etc/environment
#
# This file is parsed by pam_env module
# Syntax: simple "KEY=VAL" pairs on separate lines
MOZ_ENABLE_WAYLAND=1
MOZ_WAYLAND_GL_LIBRARY=libGLESv2.so
MOZ_WEBRENDER=1
MOZ_GLXTEST_RESULT=VENDOR\\nARM\\nRENDERER\\nMali-G31\\nVERSION\\nOpenGL ES 3.2\\nTFP\\nTRUE\\nSCREEN_INFO\\n1920x1080:1;\\nTEST_TYPE\\nEGL
MOZ_OMX_RZG2L=1
root@vkrzg2lc:~#
Hi Teodor,Normally, you should not face any issue if you follow the instructions carefully in RZ MPU HTML5 Start-up Guide. Can you please share your dmesg/kernel log?Kind Regards.
Please se below:
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050] [ 0.000000] Linux version 5.10.184-cip36-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 8.3.0, GNU ld (GNU Binutils) 2.31.1) #1 SMP PREEMPT Sun Sep 15 07:06:33 UTC 2024 [ 0.000000] Machine model: Vekatech,vkrzg2lc [ 0.000000] earlycon: scif0 at MMIO 0x000000001004b800 (options '115200n8') [ 0.000000] printk: bootconsole [scif0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000058000000, size 256 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma@58000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000068000000, size 128 MiB [ 0.000000] OF: reserved mem: initialized node linux,multimedia, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000048000000-0x00000000bfffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000048000000-0x00000000bfffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000048000000-0x00000000bfffffff] [ 0.000000] On node 0 totalpages: 491520 [ 0.000000] DMA zone: 7680 pages used for memmap [ 0.000000] DMA zone: 0 pages reserved [ 0.000000] DMA zone: 491520 pages, LIFO batch:63 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 31 pages/cpu s88600 r8192 d30184 u126976 [ 0.000000] pcpu-alloc: s88600 r8192 d30184 u126976 alloc=31*4096 [ 0.000000] pcpu-alloc: [0] 0 [0] 1 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 483840 [ 0.000000] Kernel command line: rw rootwait earlycon root=/dev/mmcblk0p2 wdt_overflow=0 [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1511568K/1966080K available (12032K kernel code, 1820K rwdata, 3788K rodata, 2944K init, 404K bss, 61296K reserved, 393216K cma-reserved) [ 0.000000] SLUB: HWalign=***, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: ***, nr_irqs: ***, preallocated irqs: 0 [ 0.000000] GICv3: 480 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000011940000 [ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (virt). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns [ 0.000004] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns [ 0.008259] Console: colour dummy device 80x25 [ 0.012728] printk: console [tty0] enabled [ 0.016845] printk: bootconsole [scif0] disabled [ 0.021519] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000) [ 0.021543] pid_max: default: 32768 minimum: 301 [ 0.021687] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.021709] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.023392] rcu: Hierarchical SRCU implementation. [ 0.024238] Detected Renesas RZ/G2L r9a07g044 Rev 4 [ 0.024495] EFI services will not be available. [ 0.024776] smp: Bringing up secondary CPUs ... [ 0.025332] Detected VIPT I-cache on CPU1 [ 0.025374] GICv3: CPU1: found redistributor 100 region 0:0x0000000011960000 [ 0.025424] CPU1: Booted secondary processor 0x0000000100 [0x412fd050] [ 0.025561] smp: Brought up 1 node, 2 CPUs [ 0.025605] SMP: Total of 2 processors activated. [ 0.025616] CPU features: detected: Privileged Access Never [ 0.025627] CPU features: detected: LSE atomic instructions [ 0.025637] CPU features: detected: User Access Override [ 0.025648] CPU features: detected: 32-bit EL0 Support [ 0.025659] CPU features: detected: Common not Private translations [ 0.025670] CPU features: detected: Data cache clean to the PoU not required for I/D coherence [ 0.025686] CPU features: detected: CRC32 instructions [ 0.025697] CPU features: detected: Speculative Store Bypassing Safe (SSBS) [ 0.025709] CPU features: detected: 32-bit EL1 Support [ 0.041747] CPU: All CPU(s) started at EL1 [ 0.041823] alternatives: patching kernel code [ 0.044301] devtmpfs: initialized [ 0.050657] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.050712] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.059953] pinctrl core: initialized pinctrl subsystem [ 0.060770] DMI not present or invalid. [ 0.061263] NET: Registered protocol family 16 [ 0.062840] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.063003] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.063157] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.063289] audit: initializing netlink subsys (disabled) [ 0.063607] audit: type=2000 audit(0.056:1): state=initialized audit_enabled=0 res=1 [ 0.064171] thermal_sys: Registered thermal governor 'step_wise' [ 0.064504] cpuidle: using governor menu [ 0.064698] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.064794] ASID allocator initialised with 65536 entries [ 0.087091] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.087129] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.087143] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.087156] HugeTLB registered ***.0 KiB page size, pre-allocated 0 pages [ 0.088890] cryptd: max_cpu_qlen set to 1000 [ 0.093858] iommu: Default domain type: Translated [ 0.094773] vgaarb: loaded [ 0.095098] SCSI subsystem initialized [ 0.095359] libata version 3.00 loaded. [ 0.095547] usbcore: registered new interface driver usbfs [ 0.095607] usbcore: registered new interface driver hub [ 0.095646] usbcore: registered new device driver usb [ 0.096298] mc: Linux media interface: v0.10 [ 0.096334] videodev: Linux video capture interface: v2.00 [ 0.096416] pps_core: LinuxPPS API ver. 1 registered [ 0.096429] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]> [ 0.096454] PTP clock support registered [ 0.096491] EDAC MC: Ver: 3.0.0 [ 0.097733] Advanced Linux Sound Architecture Driver Initialized. [ 0.098731] clocksource: Switched to clocksource arch_sys_counter [ 0.684362] VFS: Disk quotas dquot_6.6.0 [ 0.684449] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.690768] NET: Registered protocol family 2 [ 0.691041] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.692125] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear) [ 0.692264] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.692379] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear) [ 0.692641] TCP: Hash tables configured (established 16384 bind 16384) [ 0.692850] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.692904] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.693131] NET: Registered protocol family 1 [ 0.693824] RPC: Registered named UNIX socket transport module. [ 0.693858] RPC: Registered udp transport module. [ 0.693869] RPC: Registered tcp transport module. [ 0.693880] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.693900] PCI: CLS 0 bytes, default *** [ 0.694688] kvm [1]: HYP mode not available [ 0.696498] Initialise system trusted keyrings [ 0.696813] workingset: timestamp_bits=46 max_order=19 bucket_order=0 [ 0.702658] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.703528] NFS: Registering the id_resolver key type [ 0.703592] Key type id_resolver registered [ 0.703604] Key type id_legacy registered [ 0.703698] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.703715] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.703756] jffs2: version 2.2. (NAND) \xc2\xa9 2001-2006 Red Hat, Inc. [ 0.704441] Key type asymmetric registered [ 0.704468] Asymmetric key parser 'x509' registered [ 0.704509] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.704530] io scheduler mq-deadline registered [ 0.704542] io scheduler kyber registered [ 0.705251] rzg2l_irqc 110a0000.intc_ex: driving 9 irqs [ 0.751229] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.752409] SuperH (H)SCI(F) driver initialized [ 0.756189] ek79007ad-dsi 10860000.dsi.0: Couldn't get our reset GPIO [ 0.765016] loop: module loaded [ 0.767653] tun: Universal TUN/TAP device driver, 1.6 [ 0.767904] CAN device driver interface [ 0.768282] e1000e: Intel(R) PRO/1000 Network Driver [ 0.768298] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 0.768713] usbcore: registered new interface driver asix [ 0.768772] usbcore: registered new interface driver ax88179_178a [ 0.768819] usbcore: registered new interface driver cdc_ether [ 0.768865] usbcore: registered new interface driver net1080 [ 0.768900] usbcore: registered new interface driver cdc_subset [ 0.768940] usbcore: registered new interface driver zaurus [ 0.769000] usbcore: registered new interface driver cdc_ncm [ 0.769212] VFIO - User Level meta-driver version: 0.3 [ 0.769481] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 0.769500] ehci-pci: EHCI PCI platform driver [ 0.769550] ehci-platform: EHCI generic platform driver [ 0.770254] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 0.770310] ohci-pci: OHCI PCI platform driver [ 0.770386] ohci-platform: OHCI generic platform driver [ 0.771565] usbcore: registered new interface driver usb-storage [ 0.772033] renesas_usbhs 11c60000.usb: host probed [ 0.772056] renesas_usbhs 11c60000.usb: no transceiver found [ 0.772199] renesas_usbhs 11c60000.usb: gadget probed [ 0.772318] renesas_usbhs 11c60000.usb: platform init failed. [ 0.772339] renesas_usbhs 11c60000.usb: unregistering gadget [ 0.772431] udc 11c60000.usb: releasing '11c60000.usb' [ 0.772459] gadget: usb_udc_nop_release [ 0.772469] renesas_usbhs 11c60000.usb: probe failed (-517) [ 0.773264] usbcore: registered new interface driver usbtouchscreen [ 0.773330] i2c /dev entries driver [ 0.779749] EDAC rzg2l-edac: IO mapped reg addr: 0x11410000 [ 0.780104] EDAC MC0: Giving out device to module rzg2l-edac controller renesas,r9a07g044-edac: DEV 11410000.edac (INTERRUPT) [ 0.783070] ledtrig-cpu: registered to indicate activity on CPUs [ 0.783116] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.783703] clocksource: timer@12801400: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns [ 0.783742] sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns [ 0.783767] /soc/timer@12801400: used for clocksource [ 0.784678] usbcore: registered new interface driver usbhid [ 0.784701] usbhid: USB HID core driver [ 0.785164] optee: probing for conduit method. [ 0.785188] optee: api uid mismatch [ 0.785209] optee: probe of firmware:optee failed with error -22 [ 0.787396] NET: Registered protocol family 10 [ 0.788368] Segment Routing with IPv6 [ 0.788452] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 0.788939] NET: Registered protocol family 17 [ 0.788968] can: controller area network core [ 0.789045] NET: Registered protocol family 29 [ 0.789060] can: raw protocol [ 0.789074] can: broadcast manager protocol [ 0.789092] can: netlink gateway - max_hops=1 [ 0.789284] Key type dns_resolver registered [ 0.789842] registered taskstats version 1 [ 0.789866] Loading compiled-in X.509 certificates [ 0.797874] thermal emergency: set temperature to 110 celsius [ 0.798008] thermal emergency: shutdown target cpus 1 [ 0.798023] thermal emergency: freq scaled target cpus 0 [ 0.800674] gpio gpiochip0: (11030000.pinctrl): detected irqchip that is shared with multiple gpiochips: please fix the driver. [ 0.801034] pinctrl-rzg2l 11030000.pinctrl: pinctrl-rzg2l support registered [ 0.805079] gpt-rzg2l 10048300.gpt: RZ/G2L GPT Driver probed [ 0.806208] 1004b800.serial: ttySC0 at MMIO 0x1004b800 (irq = 24, base_baud = 0) is a scif [ 1.968485] printk: console [ttySC0] enabled [ 1.978672] ravb 11c20000.ethernet eth0: Base address at 0x11c20000, 5e:c5:01:00:21:c6, IRQ 106. [ 2.014781] ehci-platform 11c50100.usb: EHCI Host Controller [ 2.020508] ehci-platform 11c50100.usb: new USB bus registered, assigned bus number 1 [ 2.028472] ehci-platform 11c50100.usb: irq 111, io mem 0x11c50100 [ 2.046739] ehci-platform 11c50100.usb: USB 2.0 started, EHCI 1.10 [ 2.053617] hub 1-0:1.0: USB hub found [ 2.057414] hub 1-0:1.0: 1 port detected [ 2.062366] ehci-platform 11c70100.usb: EHCI Host Controller [ 2.068074] ehci-platform 11c70100.usb: new USB bus registered, assigned bus number 2 [ 2.076004] ehci-platform 11c70100.usb: irq 112, io mem 0x11c70100 [ 2.094742] ehci-platform 11c70100.usb: USB 2.0 started, EHCI 1.10 [ 2.101590] hub 2-0:1.0: USB hub found [ 2.105390] hub 2-0:1.0: 1 port detected [ 2.110253] ohci-platform 11c50000.usb: Generic Platform OHCI controller [ 2.117016] ohci-platform 11c50000.usb: new USB bus registered, assigned bus number 3 [ 2.124975] ohci-platform 11c50000.usb: irq 109, io mem 0x11c50000 [ 2.221424] hub 3-0:1.0: USB hub found [ 2.225225] hub 3-0:1.0: 1 port detected [ 2.230095] ohci-platform 11c70000.usb: Generic Platform OHCI controller [ 2.236839] ohci-platform 11c70000.usb: new USB bus registered, assigned bus number 4 [ 2.244792] ohci-platform 11c70000.usb: irq 110, io mem 0x11c70000 [ 2.341434] hub 4-0:1.0: USB hub found [ 2.345235] hub 4-0:1.0: 1 port detected [ 2.350100] renesas_usbhs 11c60000.usb: host probed [ 2.355031] renesas_usbhs 11c60000.usb: no transceiver found [ 2.360793] renesas_usbhs 11c60000.usb: gadget probed [ 2.366111] renesas_usbhs 11c60000.usb: probed [ 2.372389] raa215300 0-0012: RTC enabled [ 2.376472] raa215300 0-0012: RAA215300 initialized [ 2.381634] at24 0-0050: supply vcc not found, using dummy regulator [ 2.388666] at24 0-0050: 256 byte 24c02 EEPROM, writable, 8 bytes/write [ 2.406487] i2c-riic 10058000.i2c: registered with 100000Hz bus speed [ 2.414610] i2c-riic 10058400.i2c: registered with 100000Hz bus speed [ 2.425030] spi-nor spi0.0: mx25l51245g (65536 Kbytes) [ 2.431075] 3 fixed-partitions partitions found on MTD device spi0.0 [ 2.437454] Creating 3 MTD partitions on "spi0.0": [ 2.442252] 0x000000000000-0x000001ffe000 : "u-boot" [ 2.448464] 0x000001ffe000-0x000002000000 : "env" [ 2.454394] 0x000002000000-0x000004000000 : "rootfs" [ 2.462275] [drm] Initialized rcar-du 1.0.0 20130110 for 10890000.display on minor 0 [ 2.470069] [drm] Device 10890000.display probed [ 2.470938] renesas_sdhi_internal_dmac 11c10000.mmc: mmc1 base at 0x0000000011c10000, max clock rate 133 MHz [ 2.478997] renesas_sdhi_internal_dmac 11c00000.mmc: mmc0 base at 0x0000000011c00000, max clock rate 133 MHz [ 2.589514] mmc0: new HS200 MMC card at address 0001 [ 2.590275] mmcblk0: mmc0:0001 TY2964 58.3 GiB [ 2.590423] mmcblk0boot0: mmc0:0001 TY2964 partition 1 4.00 MiB [ 2.590564] mmcblk0boot1: mmc0:0001 TY2964 partition 2 4.00 MiB [ 2.590850] mmcblk0rpmb: mmc0:0001 TY2964 partition 3 4.00 MiB, chardev (243:0) [ 2.592069] mmcblk0: p1 p2 [ 2.686055] Console: switching to colour frame buffer device 128x37 [ 2.740250] rcar-du 10890000.display: [drm] fb0: rcar-dudrmfb frame buffer device [ 2.751018] input: keys as /devices/platform/keys/input/input0 [ 2.760077] ALSA device list: [ 2.765316] No soundcards found. [ 2.791229] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 2.801855] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 2.811272] devtmpfs: mounted [ 2.819334] Freeing unused kernel memory: 2944K [ 2.826386] Run /sbin/init as init process [ 2.832817] with arguments: [ 2.832822] /sbin/init [ 2.832826] with environment: [ 2.832829] HOME=/ [ 2.832832] TERM=linux [ 2.832835] wdt_overflow=0 [ 2.968406] systemd[1]: System time before build time, advancing clock. [ 2.999350] systemd[1]: systemd 244 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 3.026493] systemd[1]: Detected architecture arm64. [ 3.071527] systemd[1]: Set hostname to <vkrzg2lc>. [ 3.443969] random: systemd: uninitialized urandom read (16 bytes read) [ 3.453681] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 3.471711] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 3.486253] systemd[1]: Created slice system-getty.slice. [ 3.510976] random: systemd: uninitialized urandom read (16 bytes read) [ 3.522059] systemd[1]: Created slice system-serial\x2dgetty.slice. [ 3.546991] random: systemd: uninitialized urandom read (16 bytes read) [ 3.557948] systemd[1]: Created slice User and Session Slice. [ 3.583405] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ 3.611322] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ 3.639272] systemd[1]: Reached target Host and Network Name Lookups. [ 3.663067] systemd[1]: Reached target Paths. [ 3.683132] systemd[1]: Reached target Remote File Systems. [ 3.707077] systemd[1]: Reached target Slices. [ 3.731081] systemd[1]: Reached target Swap. [ 3.761085] systemd[1]: Listening on RPCbind Server Activation Socket. [ 3.787092] systemd[1]: Reached target RPC Port Mapper. [ 3.812717] systemd[1]: Listening on Syslog Socket. [ 3.835429] systemd[1]: Listening on initctl Compatibility Named Pipe. [ 3.863874] systemd[1]: Listening on Journal Audit Socket. [ 3.887584] systemd[1]: Listening on Journal Socket (/dev/log). [ 3.911712] systemd[1]: Listening on Journal Socket. [ 3.935874] systemd[1]: Listening on Network Service Netlink Socket. [ 3.963756] systemd[1]: Listening on udev Control Socket. [ 3.987465] systemd[1]: Listening on udev Kernel Socket. [ 4.015936] systemd[1]: Mounting Huge Pages File System... [ 4.043721] systemd[1]: Mounting POSIX Message Queue File System... [ 4.071680] systemd[1]: Mounting Kernel Debug File System... [ 4.103916] systemd[1]: Mounting Temporary Directory (/tmp)... [ 4.136585] systemd[1]: Starting Create list of static device nodes for the current kernel... [ 4.172476] systemd[1]: Starting Start psplash boot splash screen... [ 4.200294] systemd[1]: Starting RPC Bind... [ 4.223185] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 4.238232] systemd[1]: Starting Journal Service... [ 4.262327] systemd[1]: Starting Load Kernel Modules... [ 4.288618] systemd[1]: Starting Remount Root and Kernel File Systems... [ 4.319386] mali_kbase: loading out-of-tree module taints kernel. [ 4.320920] systemd[1]: Starting udev Coldplug all Devices... [ 4.366134] systemd[1]: Started Start psplash boot splash screen. [ 4.372143] mali 11840000.gpu: Kernel DDK version r45p0-01eac0 [ 4.379765] mali 11840000.gpu: Register LUT 00070000 initialized for GPU arch 0x00070009 [ 4.396465] mali 11840000.gpu: GPU identified as 0x3 arch 7.0.9 r0p0 status 0 [ 4.419745] systemd[1]: Started RPC Bind. [ 4.434021] systemd[1]: Started Journal Service. [ 4.439084] mali 11840000.gpu: No priority control manager is configured [ 4.448313] random: systemd-journal: uninitialized urandom read (16 bytes read) [ 4.449434] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) [ 4.458075] mali 11840000.gpu: No memory group manager is configured [ 4.470342] random: systemd-journal: uninitialized urandom read (16 bytes read) [ 4.482558] random: systemd-journal: uninitialized urandom read (16 bytes read) [ 4.490703] mali 11840000.gpu: Probed as mali0 [ 4.514171] rgnmm_drv mmngr: assigned reserved memory node linux,multimedia [ 4.772772] systemd-journald[140]: Received client request to flush runtime journal. [ 5.596692] random: systemd: uninitialized urandom read (16 bytes read) [ 5.778092] random: systemd: uninitialized urandom read (16 bytes read) [ 5.791627] random: systemd: uninitialized urandom read (16 bytes read) [ 5.955443] Goodix-TS 1-005d: supply AVDD28 not found, using dummy regulator [ 6.006088] Goodix-TS 1-005d: supply VDDIO not found, using dummy regulator [ 6.194577] Goodix-TS 1-005d: ID 9271, version: 1050 [ 6.208796] Goodix-TS 1-005d: Direct firmware load for goodix_9271_cfg.bin failed with error -2 [ 6.238965] input: Goodix Capacitive TouchScreen as /devices/platform/soc/10058400.i2c/i2c-1/1-005d/input/input1 [ 6.426800] random: crng init done [ 6.430216] random: 89 urandom warning(s) missed due to ratelimiting [ 6.743381] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. [ 7.519837] input: dummy-input device as /devices/virtual/input/input2 [ 7.755925] Bluetooth: Core ver 2.22 [ 7.766011] NET: Registered protocol family 31 [ 7.785019] Bluetooth: HCI device and connection manager initialized [ 7.799156] Bluetooth: HCI socket layer initialized [ 7.810845] Bluetooth: L2CAP socket layer initialized [ 7.822877] Bluetooth: SCO socket layer initialized [ 8.102360] mousedev: PS/2 mouse device common for all mice [ 9.103955] RTL8211F Gigabit Ethernet 11c20000.ethernet-ffffffff:00: attached PHY driver [RTL8211F Gigabit Ethernet] (mii_bus:phy_addr=11c20000.ethernet-ffffffff:00, irq=141) [ 9.800127] audit: type=1006 audit(1727182802.550:2): pid=240 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1 [ 33.762775] SDHI1 VccQ: disabling
Hello!
We have moved to VLP306 and the behavior is the same:
Crash Annotation GraphicsCriticalError: |[0][GFX1-]: No GPUs detected via PCI (t=1.63093) [GFX1-]: No GPUs detected via PCICrash Annotation GraphicsCriticalError: |[0][GFX1-]: No GPUs detected via PCI (t=1.63093) |[1][GFX1-]: Failed to create EGLContext!: 0x300c (t=1.65524) [GFX1-]: Failed to create EGLContext!: 0x300c[Parent 1948, Main Thread] WARNING: gdk_window_get_scale_factor: assertion 'GDK_IS_WINDOW (window)' failed: 'glib warning', file /work_data/work/vkrzg2lc/vlp_306/yocto-gecko/yocto_306u3-gecko/vkrzg2lc/tmp/work/aarch64-poky-linux/webviewer/102.15.1esr-r0/firefox-102.15.1/toolkit/xre/nsSigHandlers.cpp:167
(webviewer-default:1948): Gdk-CRITICAL **: 10:09:31.582: gdk_window_get_scale_factor: assertion 'GDK_IS_WINDOW (window)' failedCrash Annotation GraphicsCriticalError: |[0][GFX1-]: No GPUs detected via PCI (t=1.63093) |[1][GFX1-]: Failed to create EGLContext!: 0x300c (t=1.65524) |[2][GFX1-]: Wayland protocol error: xdg_wm_base@18: error 4: xdg_surface buffer (800 x 480) does not match the configured maximized state (1280 x 800) (t=4.41112) [GFX1-]: Wayland protocol error: xdg_wm_base@18: error 4: xdg_surface buffer (800 x 480) does not match the configured maximized state (1280 x 800)
Gdk-Message: 10:09:33.297: Error 71 (Protocol error) dispatching to Wayland display.Exiting due to channel error.