V4l2-comctl0 custom board issue RZV2M

Hello,

I am trying to interface AR1335 camera with a custom board. I am facing an issue here. both custom board and rzv2m evk registers and recognise the device alike.The custom board couldnt  do video capture. I checked and compared the boot logs of both the boards and found out that  v4l2-comctl called open()  this was not present in the custom board. Can anybody please explain what is going wrong here?

  • custom board bootlog

    [BL1] Boot Loader VLP V3.0.4 for RZV2M
                                          [BL1] eMMC initialized
                                                                [BL1] Loaded the boot parameter for 2nd boot
                                                                                                            [BL1] Loaded the 2nd boot loader
           [BL1] the 2nd bootloader start
                                         [BL2] 2nd boot loader entered for RZV2M_EVK
                                                                                    [BL2] DDR initialization completed_M_RZV2M_EVK
                                                                                                                                  [BL2] Loaded the boot parameter for U-Boot
                                           [BL2] Loaded the U-Boot
                                                                  [BL2] the U-Boot start
    
    
    U-Boot 2021.10 (May 31 2023 - 08:04:36 +0000) for RZ/V2M Linux Package VLP V3.0.4
    
    Model: RZ/V2M
    DRAM:  4 GiB
    MMC:   sd@85000000: 0, sd@85020000: 1
    Loading Environment from MMC... OK
    In:    serial
    Out:   serial
    Err:   serial
    Net:   No ethernet found.
    
    Hit any key to stop autoboot:  0 
    13144768 bytes read in 575 ms (21.8 MiB/s)
    19522048 bytes read in 952 ms (19.6 MiB/s)
    24067 bytes read in 6 ms (3.8 MiB/s)
    [DEBUG]Reset vector address 0x02000000
    Wakeup for Secondary CPU
    Moving Image from 0x180080000 to 0x180200000, end=181510000
    ## Flattened Device Tree blob at 180000000
       Booting using the fdt blob at 0x180000000
       Loading Device Tree to 000000017fff7000, end 000000017ffffe02 ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 5.10.175-cip29-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 8.3.0, GNU ld (GNU Binutils) 2.31.1) #1 SMP PREEMPT Tue Apr 5 23:00:00 UTC 2011
    [    0.000000] Machine model: Renesas EVK based on r9a09g011gbg
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000001b8000000, size 128 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma@1B8000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000001ff800000, size 4 MiB
    [    0.000000] OF: reserved mem: initialized node image_buf@0, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x000000007c000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x00000001ffbfffff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x000000007c000000-0x000000007fefffff]
    [    0.000000]   node   0: [mem 0x000000007ff00000-0x000000007fffffff]
    [    0.000000]   node   0: [mem 0x0000000180000000-0x00000001ffbfffff]
    [    0.000000] Initmem setup node 0 [mem 0x000000007c000000-0x00000001ffbfffff]
    [    0.000000] percpu: Embedded 23 pages/cpu s55384 r8192 d30632 u94208
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 531216
    [    0.000000] Kernel command line: root=/dev/mmcblk0p2 rootwait rootfstype=ext4 rw
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] software IO TLB: Cannot allocate buffer
    [    0.000000] Memory: 1355484K/2158592K available (12096K kernel code, 1144K rwdata, 3732K rodata, 1984K init, 391K bss, 667940K reserved, 135168K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu: 	RCU event tracing is enabled.
    [    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
    [    0.000000] 	Trampoline variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x000000008202f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
    [    0.000005] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
    [    0.000254] Console: colour dummy device 80x25
    [    0.000670] printk: console [tty0] enabled
    [    0.000714] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
    [    0.000742] pid_max: default: 32768 minimum: 301
    [    0.000896] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.000938] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.002476] rcu: Hierarchical SRCU implementation.
    [    0.002963] Detected Renesas RZ/V2M (r9a09g011gbg)
    [    0.002982] EFI services will not be available.
    [    0.003092] smp: Bringing up secondary CPUs ...
    [    0.003108] smp: Brought up 1 node, 1 CPU
    [    0.003120] SMP: Total of 1 processors activated.
    [    0.003140] CPU features: detected: 32-bit EL0 Support
    [    0.003157] CPU features: detected: CRC32 instructions
    [    0.003172] CPU features: detected: 32-bit EL1 Support
    [    0.010515] CPU: All CPU(s) started at EL2
    [    0.010563] alternatives: patching kernel code
    [    0.011474] devtmpfs: initialized
    [    0.015969] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.016014] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
    [    0.020534] pinctrl core: initialized pinctrl subsystem
    [    0.021311] DMI not present or invalid.
    [    0.021805] NET: Registered protocol family 16
    [    0.023477] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [    0.023564] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.023623] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.023703] audit: initializing netlink subsys (disabled)
    [    0.024398] thermal_sys: Registered thermal governor 'step_wise'
    [    0.024542] cpuidle: using governor menu
    [    0.024773] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.024816] ASID allocator initialised with 65536 entries
    [    0.028194] audit: type=2000 audit(0.020:1): state=initialized audit_enabled=0 res=1
    [    0.041029] PFC_RZV2M b6250000.pin-controller: Init external interrupt controller success.
    [    0.041070] PFC_RZV2M b6250000.pin-controller: RZ/V pin controller successfully registered
    [    0.050394] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.050428] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.050445] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.050461] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.052108] cryptd: max_cpu_qlen set to 1000
    [    0.056256] PFC_RZV2M b6250000.pin-controller: 20 GPIO nodes are registered
    [    0.059070] iommu: Default domain type: Translated 
    [    0.059734] vgaarb: loaded
    [    0.060043] SCSI subsystem initialized
    [    0.060604] usbcore: registered new interface driver usbfs
    [    0.060655] usbcore: registered new interface driver hub
    [    0.060694] usbcore: registered new device driver usb
    [    0.061253] mc: Linux media interface: v0.10
    [    0.061289] videodev: Linux video capture interface: v2.00
    [    0.061361] pps_core: LinuxPPS API ver. 1 registered
    [    0.061375] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
    [    0.061404] PTP clock support registered
    [    0.062136] Advanced Linux Sound Architecture Driver Initialized.
    [    0.062889] clocksource: Switched to clocksource arch_sys_counter
    [    0.063079] VFS: Disk quotas dquot_6.6.0
    [    0.063138] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.069066] NET: Registered protocol family 2
    [    0.069404] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.071506] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
    [    0.071583] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.071849] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
    [    0.072342] TCP: Hash tables configured (established 32768 bind 32768)
    [    0.072476] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.072584] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.072800] NET: Registered protocol family 1
    [    0.073335] RPC: Registered named UNIX socket transport module.
    [    0.073351] RPC: Registered udp transport module.
    [    0.073364] RPC: Registered tcp transport module.
    [    0.073376] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.074217] PCI: CLS 0 bytes, default 64
    [    0.074811] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
    [    0.075239] kvm [1]: IPA Size Limit: 40 bits
    [    0.076038] kvm [1]: vgic interrupt IRQ11
    [    0.076129] kvm [1]: Hyp mode initialized successfully
    [    0.077768] Initialise system trusted keyrings
    [    0.077908] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [    0.084486] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.085158] NFS: Registering the id_resolver key type
    [    0.085199] Key type id_resolver registered
    [    0.085212] Key type id_legacy registered
    [    0.085309] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.085327] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.085362] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    [    0.085971] Key type asymmetric registered
    [    0.085988] Asymmetric key parser 'x509' registered
    [    0.086028] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
    [    0.086050] io scheduler mq-deadline registered
    [    0.086063] io scheduler kyber registered
    [    0.090149] rzv2m-pcie 85030000.pcie: host bridge /soc/pcie@85030000 ranges:
    [    0.090208] rzv2m-pcie 85030000.pcie:      MEM 0x00c0000000..0x00c01fffff -> 0x00c0000000
    [    0.090238] rzv2m-pcie 85030000.pcie:      MEM 0x00c0300000..0x00c82fffff -> 0x00c0300000
    [    0.090278] rzv2m-pcie 85030000.pcie:   IB MEM 0x0180000000..0x01ffffffff -> 0x0180000000
    [    0.898892] rzv2m-pcie 85030000.pcie: PCIe link down
    [    0.933271] Serial: 8250/16550 driver, 2 ports, IRQ sharing disabled
    [    0.934750] a4040000.serial: ttyS0 at MMIO 0xa4040000 (irq = 68, base_baud = 3000000) is a R8ARZV2M16750
    [    1.757527] printk: console [ttyS0] enabled
    [    1.762127] SuperH (H)SCI(F) driver initialized
    [    1.775540] loop: module loaded
    [    1.780678] rzv2m_csi a4020200.spi: probed
    [    1.785884] tun: Universal TUN/TAP device driver, 1.6
    [    1.791135] CAN device driver interface
    [    1.795274] e1000e: Intel(R) PRO/1000 Network Driver
    [    1.800294] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    [    1.806558] PPP generic driver version 2.4.2
    [    1.811010] Broadcom 43xx driver loaded [ Features: PNS ]
    [    1.816538] usbcore: registered new interface driver asix
    [    1.822008] usbcore: registered new interface driver ax88179_178a
    [    1.828199] usbcore: registered new interface driver cdc_ether
    [    1.834095] usbcore: registered new interface driver net1080
    [    1.839820] usbcore: registered new interface driver cdc_subset
    [    1.845805] usbcore: registered new interface driver zaurus
    [    1.851462] usbcore: registered new interface driver cdc_ncm
    [    1.857191] usbcore: registered new interface driver qmi_wwan_q
    [    1.863178] usbcore: registered new interface driver qmi_wwan
    [    1.869090] VFIO - User Level meta-driver version: 0.3
    [    1.874495] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    1.881092] ehci-pci: EHCI PCI platform driver
    [    1.885601] ehci-platform: EHCI generic platform driver
    [    1.890989] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
    [    1.897221] ohci-pci: OHCI PCI platform driver
    [    1.901726] ohci-platform: OHCI generic platform driver
    [    1.907401] xhci-hcd 85060000.usb: xHCI Host Controller
    [    1.912694] xhci-hcd 85060000.usb: new USB bus registered, assigned bus number 1
    [    1.920173] xhci-hcd 85060000.usb: USB bus 1 deregistered
    [    1.925861] usbcore: registered new interface driver cdc_acm
    [    1.931575] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
    [    1.939670] usbcore: registered new interface driver cdc_wdm
    [    1.945406] usbcore: registered new interface driver usb-storage
    [    1.951529] usbcore: registered new interface driver option
    [    1.957155] usbserial: USB Serial support registered for GSM modem (1-port)
    [    1.964183] usbcore: registered new interface driver qcaux
    [    1.969720] usbserial: USB Serial support registered for qcaux
    [    1.975614] usbcore: registered new interface driver qcserial
    [    1.981412] usbserial: USB Serial support registered for Qualcomm USB modem
    [    1.989783] xhci-hcd 85060000.usb: xHCI Host Controller
    [    1.995065] renesas_usb3 85070000.usb: probed
    [    1.999470] xhci-hcd 85060000.usb: new USB bus registered, assigned bus number 1
    [    2.007424] mousedev: PS/2 mouse device common for all mice
    [    2.014231] xhci-hcd 85060000.usb: hcc params 0x0140fe8d hci version 0x110 quirks 0x0000000000010010
    [    2.023494] usbcore: registered new interface driver usbtouchscreen
    [    2.029939] i2c /dev entries driver
    [    2.033859] xhci-hcd 85060000.usb: irq 63, io mem 0x85060000
    [    2.039769] rzv2m-i2c a4030000.i2c: probed
    [    2.044373] rzv2m-i2c a4030100.i2c: probed
    [    2.048658] xhci-hcd 85060000.usb: xHCI Host Controller
    [    2.055558] v4l2-comctl0: V4L2 capture device registered as 'video0'
    [    2.061976] xhci-hcd 85060000.usb: new USB bus registered, assigned bus number 2
    [    2.069423] comctl_probe is successfully.
    [    2.073491] xhci-hcd 85060000.usb: Host supports USB 3.1 Enhanced SuperSpeed
    [    2.080615] allocated comctl device '241 0'
    [    2.084916] comctl_device : created correctly
    [    2.089832] hub 1-0:1.0: USB hub found
    [    2.093768] rzv2m_poweroff_reset a3700000.poweroff-reset: RZ/V2M poweroff-reset driver registered
    [    2.102745] hub 1-0:1.0: 1 port detected
    [    2.107016] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [    2.115593] timeout_min = 21845
    [    2.118749] timeout_max = 89478485
    [    2.122659] hub 2-0:1.0: USB hub found
    [    2.127755] renesas_sdhi_internal_dmac 85000000.sd: Got CD GPIO
    [    2.133766] hub 2-0:1.0: 1 port detected
    [    2.137995] ledtrig-cpu: registered to indicate activity on CPUs
    [    2.145891] usbcore: registered new interface driver usbhid
    [    2.151518] usbhid: USB HID core driver
    [    2.156112] a4000400.timer:probed
    [    2.159886] a4000480.timer:probed
    [    2.163485] a4000500.timer:probed
    [    2.167251] a4000580.timer:probed
    [    2.170851] a4000600.timer:probed
    [    2.174482] a4000680.timer:probed
    [    2.178161] a4000700.timer:probed
    [    2.181754] a4000780.timer:probed
    [    2.185348] a4000800.timer:probed
    [    2.189014] a4000880.timer:probed
    [    2.192695] a4000900.timer:probed
    [    2.196297] a4000980.timer:probed
    [    2.199761] renesas_sdhi_internal_dmac 85000000.sd: mmc0 base at 0x0000000085000000, max clock rate 200 MHz
    [    2.209933] a4000a00.timer:probed
    [    2.213570] a4000a80.timer:probed
    [    2.217530] a4000b00.timer:probed
    [    2.221186] a4000b80.timer:probed
    [    2.225527] drpai-rz 83000000.drpai: DRP-AI Driver version : 2.10 rel.1 V2M
    [    2.232605] drpai-rz 83000000.drpai: sysctrl register region start 0x00000000A3F03000
    [    2.240631] drpai-rz 83000000.drpai: DRP-AI memory region start 0x00000001C0000000, size 0x20000000
    [    2.249865] drpai-rz 83000000.drpai: linux-memory-region start 0x0000000180000000, size 0x7FC00000
    [    2.258985] drpai-rz 83000000.drpai: DRP base address 0x83000000, size 0x01000000
    [    2.266564] drpai-rz 83000000.drpai: AI-MAC base address 0x84000000, size 0x00400000
    [    2.276375] NET: Registered protocol family 10
    [    2.281716] Segment Routing with IPv6
    [    2.285524] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    2.292159] NET: Registered protocol family 17
    [    2.296666] can: controller area network core
    [    2.301137] NET: Registered protocol family 29
    [    2.305647] can: raw protocol
    [    2.308760] can: broadcast manager protocol
    [    2.312998] can: netlink gateway - max_hops=1
    [    2.317575] Key type dns_resolver registered
    [    2.322299] registered taskstats version 1
    [    2.326526] Loading compiled-in X.509 certificates
    [    2.340603] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    2.348996] mmc0: new high speed SDHC card at address 0001
    [    2.355373] mmcblk0: mmc0:0001 SD 3.72 GiB 
    [    2.361674] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    2.368392]  mmcblk0: p1 p2
    [    2.372313] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    [    2.381106] ALSA device list:
    [    2.384114]   No soundcards found.
    [    2.387594] cfg80211: failed to load regulatory.db
    [    2.590196] EXT4-fs (mmcblk0p2): recovery complete
    [    2.596695] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    2.604999] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    2.612786] devtmpfs: mounted
    [    2.616910] Freeing unused kernel memory: 1984K
    [    2.621570] Run /sbin/init as init process
    [    3.338523] systemd[1]: System time before build time, advancing clock.
    [    3.406505] systemd[1]: systemd 244 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    3.428365] systemd[1]: Detected architecture arm64.
    
    Welcome to Poky (Yocto Project Reference Distro) 3.1.21 (dunfell)!
    
    [    3.460249] systemd[1]: Set hostname to <rzv2m>.
    [    3.925613] systemd[1]: Configuration file /lib/systemd/system/watchdog.service is marked executable. Please remove executable permission bits. Proceeding anyway.
    [    4.143233] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.150205] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
    [    4.162662] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
    [    4.173999] systemd[1]: Created slice system-getty.slice.
    [  OK  ] Created slice system-getty.slice.
    [    4.195068] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.202976] systemd[1]: Created slice system-serial\x2dgetty.slice.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    4.227047] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.234783] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    4.255347] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password …ts to Console Directory Watch.
    [    4.279236] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password R…uests to Wall Directory Watch.
    [    4.303163] systemd[1]: Reached target Host and Network Name Lookups.
    [  OK  ] Reached target Host and Network Name Lookups.
    [    4.327060] systemd[1]: Reached target Paths.
    [  OK  ] Reached target Paths.
    [    4.347045] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    4.367026] systemd[1]: Reached target Slices.
    [  OK  ] Reached target Slices.
    [    4.387052] systemd[1]: Reached target Swap.
    [  OK  ] Reached target Swap.
    [    4.408998] systemd[1]: Listening on Syslog Socket.
    [  OK  ] Listening on Syslog Socket.
    [    4.431407] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    4.455793] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    4.479458] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    4.503534] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    4.523758] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    4.547594] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    4.571395] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    4.595196] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    4.624849] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    4.659081] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    4.692013] systemd[1]: Mounting Temporary Directory (/tmp)...
             Mounting Temporary Directory (/tmp)...
    [    4.721789] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
    [    4.733385] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
    [    4.747570] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.798230] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.831804] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.873664] u_dma_buf: loading out-of-tree module taints kernel.
    [    4.880629] systemd[1]: Starting udev Coldplug all Devices...
    [    4.896290] u-dma-buf udmabuf@0: assigned reserved memory node image_buf@0
             Starting udev Coldplug all Devices...
    [    4.937008] systemd[1]: Mounted Huge Pages File System.
    [    4.950527] u-dma-buf udmabuf0: driver version = 3.2.4
    [    4.966955] u-dma-buf udmabuf0: major number   = 237
    [  OK  ] Mounted Huge Pages File System.
    [    4.980356] systemd[1]: Mounted POSIX Message Queue File System.
    [    4.992774] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
    [    5.002808] u-dma-buf udmabuf0: minor number   = 0
    [  OK  ] Mounted POSIX Message Queue File Sy[    5.018954] u-dma-buf udmabuf0: phys address   = 0x00000001ff800000
    stem.
    [    5.041548] systemd[1]: Mounted Kernel Debug File System.
    [    5.062066] u-dma-buf udmabuf0: buffer size    = 4194304
    [  OK  ] Mounted Kernel Debug File System.
    [    5.077905] u-dma-buf udmabuf@0: driver installed.
    [    5.086522] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted Temporary Directory (/tmp).
    [  OK  ] Started Load Kernel Modules.
    [  OK  ] Started Remount Root and Kernel File Systems.
    [    5.177532] random: systemd: uninitialized urandom read (16 bytes read)
             Mounting Kernel Configuration File System.[    5.201899] random: systemd-journal: uninitialized urandom read (16 bytes read)
    ..
    [    5.226079] random: systemd: uninitialized urandom read (16 bytes read)
             Starting Flush Journal to Persistent Storage...
             Starting Apply Kernel Variables...
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Mounted Kernel Configuration File System.
    [    5.315996] systemd-journald[95]: Received client request to flush runtime journal.
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /var/volatile...
             Starting udev Kernel Device Manager...
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Network Time Synchronization...
             Starting Update UTMP about System Boot/Shutdown...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started udev Kernel Device Manager.
    [  OK  ] Started udev Coldplug all Devices.
    [    6.492073] random: systemd: uninitialized urandom read (16 bytes read)
    [    6.515412] random: systemd-journal: uninitialized urandom read (16 bytes read)
             Starting udev Wait for Complete Device Initialization...
    [  OK  ] Started Network Time Synchronization.
    [    6.577274] random: systemd: uninitialized urandom read (16 bytes read)
    [  OK  ] Reached target System Time Set.
    [  OK  ] Reached target System Time Synchronized.
    [    7.446957] random: crng init done
    [    7.450406] random: 56 urandom warning(s) missed due to ratelimiting
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Reached target Hardware activated USB gadget.
    [  OK  ] Started udev Wait for Complete Device Initialization.
    [  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting sshd.socket.
    [  OK  ] Listening on sshd.socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
             Starting Modem Manager...
    [  OK  ] Started Kernel Logging Service.
    [  OK  ] Started System Logging Service.
             Starting Comctl daemon...
    [  OK  ] Started D-Bus System Message Bus.
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
             Starting Telephony service...
             Starting rng-tools.service...
             Starting Login Service...
    [  OK  ] Started VIN initializing setting.
    [  OK  ] Started WatchdogTimer.
    [  OK  ] Started IPv6 Packet Filtering Framework.
    [  OK  ] Started IPv4 Packet Filtering Framework.
    [  OK  ] Started rng-tools.service.
    [  OK  ] Started Comctl daemon.
    [  OK  ] Started Telephony service.
    [  OK  ] Reached target Network (Pre).
             Starting Connection service...
             Starting Network Service...
    [  OK  ] Started Modem Manager.
    [  OK  ] Started Login Service.
    [  OK  ] Started Network Service.
    [  OK  ] Started Connection service.
    [  OK  ] Reached target Network.
             Starting Permit User Sessions...
             Starting Target Communication Framework agent...
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS0.
    [  OK  ] Reached target Login Prompts.
    [  OK  ] Started Target Communication Framework agent.
    [  OK  ] Reached target Multi-User System.
             Starting Hostname Service...
             Starting Update UTMP about System Runlevel Changes...
             Starting WPA supplicant...
    [  OK  ] Started Update UTMP about System Runlevel Changes.
    [  OK  ] Started WPA supplicant.
    [  OK  ] Started Hostname Service.
    
    Poky (Yocto Project Reference Distro) 3.1.21 rzv2m ttyS0
    
    BSP: RZV2M/RZV2M Evaluation Board Kit/3.0.4
    LSI: RZV2M
    Version: 3.0.4
    rzv2m login: 
    

    RZV2M evk bootlogs

    [BL1] Boot Loader Version 1.20
                                  [BL1] eMMC initialized
                                                        [BL1] Loaded the boot parameter for 2nd boot
                                                                                                    [BL1] Loaded the 2nd boot loader
                                                                                                                                    [BL1] Kick the 2nd boot loader
                                 [BL2] 2nd boot loader entered
                                                              [BL2] DDR initialization completed_M
                                                                                                  [BL2] Loaded the boot parameter for U-Boot
           [BL2] Loaded the U-Boot
                                  [BL2] the U-Boot start
    
    
    U-Boot 2018.09 (Jan 12 2022 - 10:07:36 +0000)
    
    Model: RZ/V2M
    DRAM:  4 GiB
    MMC:   sd@85000000: 0, sd@85020000: 1
    Loading Environment from MMC... OK
    In:    serial
    Out:   serial
    Err:   serial
    Net:   eth0: ethernet@a3300000
    Hit any key to stop autoboot:  0 
    13144768 bytes read in 573 ms (21.9 MiB/s)
    19522048 bytes read in 844 ms (22.1 MiB/s)
    24067 bytes read in 5 ms (4.6 MiB/s)
    [DEBUG]Reset vector address 0x02000000
    Wakeup for Secondary CPU
    ## Flattened Device Tree blob at 180000000
       Booting using the fdt blob at 0x180000000
       Loading Device Tree to 000000007fe2e000, end 000000007fe36e02 ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 5.10.175-cip29-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 8.3.0, GNU ld (GNU Binutils) 2.31.1) #1 SMP PREEMPT Tue Apr 5 23:00:00 UTC 2011
    [    0.000000] Machine model: Renesas EVK based on r9a09g011gbg
    [    0.000000] efi: UEFI not found.
    [    0.000000] OF: fdt: Reserved memory: failed to reserve memory for node 'rtos_rpmsg@7C000000': base 0x000000007c000000, size 63 MiB
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000001b8000000, size 128 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma@1B8000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000001ff800000, size 4 MiB
    [    0.000000] OF: reserved mem: initialized node image_buf@0, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x000000007c000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x00000001ffbfffff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x000000007c000000-0x000000007fffffff]
    [    0.000000]   node   0: [mem 0x0000000180000000-0x00000001ffbfffff]
    [    0.000000] Initmem setup node 0 [mem 0x000000007c000000-0x00000001ffbfffff]
    [    0.000000] percpu: Embedded 23 pages/cpu s55384 r8192 d30632 u94208
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 531216
    [    0.000000] Kernel command line: root=/dev/mmcblk0p2 rootwait rootfstype=ext4 rw
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] software IO TLB: Cannot allocate buffer
    [    0.000000] Memory: 1419848K/2158592K available (12096K kernel code, 1144K rwdata, 3732K rodata, 1984K init, 391K bss, 603576K reserved, 135168K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu: 	RCU event tracing is enabled.
    [    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
    [    0.000000] 	Trampoline variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x000000008202f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
    [    0.000005] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
    [    0.000256] Console: colour dummy device 80x25
    [    0.000679] printk: console [tty0] enabled
    [    0.000723] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
    [    0.000751] pid_max: default: 32768 minimum: 301
    [    0.000907] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.000952] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.002503] rcu: Hierarchical SRCU implementation.
    [    0.002990] Detected Renesas RZ/V2M (r9a09g011gbg)
    [    0.003010] EFI services will not be available.
    [    0.003121] smp: Bringing up secondary CPUs ...
    [    0.003137] smp: Brought up 1 node, 1 CPU
    [    0.003149] SMP: Total of 1 processors activated.
    [    0.003168] CPU features: detected: 32-bit EL0 Support
    [    0.003184] CPU features: detected: CRC32 instructions
    [    0.003199] CPU features: detected: 32-bit EL1 Support
    [    0.010560] CPU: All CPU(s) started at EL2
    [    0.010607] alternatives: patching kernel code
    [    0.011540] devtmpfs: initialized
    [    0.016089] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.016135] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
    [    0.020018] pinctrl core: initialized pinctrl subsystem
    [    0.020914] DMI not present or invalid.
    [    0.021423] NET: Registered protocol family 16
    [    0.023016] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [    0.023085] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.023144] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.023222] audit: initializing netlink subsys (disabled)
    [    0.023874] thermal_sys: Registered thermal governor 'step_wise'
    [    0.024017] cpuidle: using governor menu
    [    0.024294] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.024340] ASID allocator initialised with 65536 entries
    [    0.028203] audit: type=2000 audit(0.020:1): state=initialized audit_enabled=0 res=1
    [    0.040614] PFC_RZV2M b6250000.pin-controller: Init external interrupt controller success.
    [    0.040655] PFC_RZV2M b6250000.pin-controller: RZ/V pin controller successfully registered
    [    0.050007] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.050041] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.050058] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.050074] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.051724] cryptd: max_cpu_qlen set to 1000
    [    0.055948] PFC_RZV2M b6250000.pin-controller: 20 GPIO nodes are registered
    [    0.058783] iommu: Default domain type: Translated 
    [    0.059422] vgaarb: loaded
    [    0.059735] SCSI subsystem initialized
    [    0.060142] usbcore: registered new interface driver usbfs
    [    0.060193] usbcore: registered new interface driver hub
    [    0.060233] usbcore: registered new device driver usb
    [    0.060878] mc: Linux media interface: v0.10
    [    0.060916] videodev: Linux video capture interface: v2.00
    [    0.060989] pps_core: LinuxPPS API ver. 1 registered
    [    0.061003] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
    [    0.061031] PTP clock support registered
    [    0.061760] Advanced Linux Sound Architecture Driver Initialized.
    [    0.062518] clocksource: Switched to clocksource arch_sys_counter
    [    0.062709] VFS: Disk quotas dquot_6.6.0
    [    0.062767] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.068699] NET: Registered protocol family 2
    [    0.069036] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.071140] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
    [    0.071220] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.071489] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
    [    0.072004] TCP: Hash tables configured (established 32768 bind 32768)
    [    0.072137] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.072241] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.072459] NET: Registered protocol family 1
    [    0.072993] RPC: Registered named UNIX socket transport module.
    [    0.073010] RPC: Registered udp transport module.
    [    0.073022] RPC: Registered tcp transport module.
    [    0.073034] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.073878] PCI: CLS 0 bytes, default 64
    [    0.074476] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
    [    0.074905] kvm [1]: IPA Size Limit: 40 bits
    [    0.075655] kvm [1]: vgic interrupt IRQ11
    [    0.075748] kvm [1]: Hyp mode initialized successfully
    [    0.077391] Initialise system trusted keyrings
    [    0.077540] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [    0.084142] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.084823] NFS: Registering the id_resolver key type
    [    0.084863] Key type id_resolver registered
    [    0.084876] Key type id_legacy registered
    [    0.084972] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.084990] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.085026] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    [    0.085631] Key type asymmetric registered
    [    0.085647] Asymmetric key parser 'x509' registered
    [    0.085689] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
    [    0.085711] io scheduler mq-deadline registered
    [    0.085725] io scheduler kyber registered
    [    0.089900] rzv2m-pcie 85030000.pcie: host bridge /soc/pcie@85030000 ranges:
    [    0.089962] rzv2m-pcie 85030000.pcie:      MEM 0x00c0000000..0x00c01fffff -> 0x00c0000000
    [    0.089991] rzv2m-pcie 85030000.pcie:      MEM 0x00c0300000..0x00c82fffff -> 0x00c0300000
    [    0.090030] rzv2m-pcie 85030000.pcie:   IB MEM 0x0180000000..0x01ffffffff -> 0x0180000000
    [    0.898522] rzv2m-pcie 85030000.pcie: PCIe link down
    [    0.932912] Serial: 8250/16550 driver, 2 ports, IRQ sharing disabled
    [    0.934383] a4040000.serial: ttyS0 at MMIO 0xa4040000 (irq = 68, base_baud = 3000000) is a R8ARZV2M16750
    [    1.762747] printk: console [ttyS0] enabled
    [    1.767357] SuperH (H)SCI(F) driver initialized
    [    1.780771] loop: module loaded
    [    1.785944] rzv2m_csi a4020200.spi: probed
    [    1.791176] tun: Universal TUN/TAP device driver, 1.6
    [    1.796434] CAN device driver interface
    [    1.800573] e1000e: Intel(R) PRO/1000 Network Driver
    [    1.805586] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    [    1.811850] PPP generic driver version 2.4.2
    [    1.816295] Broadcom 43xx driver loaded [ Features: PNS ]
    [    1.821821] usbcore: registered new interface driver asix
    [    1.827322] usbcore: registered new interface driver ax88179_178a
    [    1.833482] usbcore: registered new interface driver cdc_ether
    [    1.839376] usbcore: registered new interface driver net1080
    [    1.845103] usbcore: registered new interface driver cdc_subset
    [    1.851088] usbcore: registered new interface driver zaurus
    [    1.856743] usbcore: registered new interface driver cdc_ncm
    [    1.862475] usbcore: registered new interface driver qmi_wwan_q
    [    1.868462] usbcore: registered new interface driver qmi_wwan
    [    1.874374] VFIO - User Level meta-driver version: 0.3
    [    1.879783] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    1.886378] ehci-pci: EHCI PCI platform driver
    [    1.890888] ehci-platform: EHCI generic platform driver
    [    1.896271] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
    [    1.902516] ohci-pci: OHCI PCI platform driver
    [    1.907019] ohci-platform: OHCI generic platform driver
    [    1.912698] xhci-hcd 85060000.usb: xHCI Host Controller
    [    1.917988] xhci-hcd 85060000.usb: new USB bus registered, assigned bus number 1
    [    1.925465] xhci-hcd 85060000.usb: USB bus 1 deregistered
    [    1.931153] usbcore: registered new interface driver cdc_acm
    [    1.936867] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
    [    1.944962] usbcore: registered new interface driver cdc_wdm
    [    1.950699] usbcore: registered new interface driver usb-storage
    [    1.956821] usbcore: registered new interface driver option
    [    1.962447] usbserial: USB Serial support registered for GSM modem (1-port)
    [    1.969475] usbcore: registered new interface driver qcaux
    [    1.975010] usbserial: USB Serial support registered for qcaux
    [    1.980905] usbcore: registered new interface driver qcserial
    [    1.986703] usbserial: USB Serial support registered for Qualcomm USB modem
    [    1.994628] renesas_usb3 85070000.usb: probed
    [    1.999545] mousedev: PS/2 mouse device common for all mice
    [    2.005230] usbcore: registered new interface driver usbtouchscreen
    [    2.011678] i2c /dev entries driver
    [    2.015774] rzv2m-i2c a4030000.i2c: probed
    [    2.020426] rzv2m-i2c a4030100.i2c: probed
    [    2.026224] v4l2-comctl0: V4L2 capture device registered as 'video0'
    [    2.032627] comctl_probe is successfully.
    [    2.036691] allocated comctl device '241 0'
    [    2.040990] comctl_device : created correctly
    [    2.045492] rzv2m_poweroff_reset a3700000.poweroff-reset: RZ/V2M poweroff-reset driver registered
    [    2.054796] timeout_min = 21845
    [    2.057953] timeout_max = 89478485
    [    2.062573] renesas_sdhi_internal_dmac 85000000.sd: Got CD GPIO
    [    2.068820] ledtrig-cpu: registered to indicate activity on CPUs
    [    2.076047] usbcore: registered new interface driver usbhid
    [    2.081660] usbhid: USB HID core driver
    [    2.086204] a4000400.timer:probed
    [    2.089858] a4000480.timer:probed
    [    2.093453] a4000500.timer:probed
    [    2.097233] a4000580.timer:probed
    [    2.100841] a4000600.timer:probed
    [    2.104467] a4000680.timer:probed
    [    2.108071] a4000700.timer:probed
    [    2.111662] a4000780.timer:probed
    [    2.115316] a4000800.timer:probed
    [    2.118931] a4000880.timer:probed
    [    2.122540] a4000900.timer:probed
    [    2.126134] a4000980.timer:probed
    [    2.129601] renesas_sdhi_internal_dmac 85000000.sd: mmc0 base at 0x0000000085000000, max clock rate 200 MHz
    [    2.139699] a4000a00.timer:probed
    [    2.143333] a4000a80.timer:probed
    [    2.147306] a4000b00.timer:probed
    [    2.150963] a4000b80.timer:probed
    [    2.155183] drpai-rz 83000000.drpai: DRP-AI Driver version : 2.10 rel.1 V2M
    [    2.162250] drpai-rz 83000000.drpai: sysctrl register region start 0x00000000A3F03000
    [    2.170185] drpai-rz 83000000.drpai: DRP-AI memory region start 0x00000001C0000000, size 0x20000000
    [    2.179328] drpai-rz 83000000.drpai: linux-memory-region start 0x0000000180000000, size 0x7FC00000
    [    2.188389] drpai-rz 83000000.drpai: DRP base address 0x83000000, size 0x01000000
    [    2.195956] drpai-rz 83000000.drpai: AI-MAC base address 0x84000000, size 0x00400000
    [    2.205649] NET: Registered protocol family 10
    [    2.211024] Segment Routing with IPv6
    [    2.214820] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    2.221256] NET: Registered protocol family 17
    [    2.225759] can: controller area network core
    [    2.230229] NET: Registered protocol family 29
    [    2.234742] can: raw protocol
    [    2.237749] can: broadcast manager protocol
    [    2.241987] can: netlink gateway - max_hops=1
    [    2.246591] Key type dns_resolver registered
    [    2.251324] registered taskstats version 1
    [    2.255480] Loading compiled-in X.509 certificates
    [    2.269261] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    2.277926] mmc0: new high speed SDHC card at address 0001
    [    2.284177] mmcblk0: mmc0:0001 SD 3.72 GiB 
    [    2.289465] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    2.296885] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    [    2.305639] ALSA device list:
    [    2.308644]   No soundcards found.
    [    2.312090] cfg80211: failed to load regulatory.db
    [    2.317551]  mmcblk0: p1 p2
    [    2.524791] EXT4-fs (mmcblk0p2): recovery complete
    [    2.532686] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    2.540898] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    2.548583] devtmpfs: mounted
    [    2.552689] Freeing unused kernel memory: 1984K
    [    2.557346] Run /sbin/init as init process
    [    3.253550] systemd[1]: System time before build time, advancing clock.
    [    3.322606] systemd[1]: systemd 244 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    3.344447] systemd[1]: Detected architecture arm64.
    
    Welcome to Poky (Yocto Project Reference Distro) 3.1.21 (dunfell)!
    
    [    3.379877] systemd[1]: Set hostname to <rzv2m>.
    [    3.857057] systemd[1]: Configuration file /lib/systemd/system/watchdog.service is marked executable. Please remove executable permission bits. Proceeding anyway.
    [    4.074786] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.081748] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
    [    4.094213] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
    [    4.105584] systemd[1]: Created slice system-getty.slice.
    [  OK  ] Created slice system-getty.slice.
    [    4.126691] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.134630] systemd[1]: Created slice system-serial\x2dgetty.slice.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    4.158679] random: systemd: uninitialized urandom read (16 bytes read)
    [    4.166422] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    4.187002] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password …ts to Console Directory Watch.
    [    4.210861] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password R…uests to Wall Directory Watch.
    [    4.234784] systemd[1]: Reached target Host and Network Name Lookups.
    [  OK  ] Reached target Host and Network Name Lookups.
    [    4.258669] systemd[1]: Reached target Paths.
    [  OK  ] Reached target Paths.
    [    4.278675] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    4.298653] systemd[1]: Reached target Slices.
    [  OK  ] Reached target Slices.
    [    4.318682] systemd[1]: Reached target Swap.
    [  OK  ] Reached target Swap.
    [    4.340615] systemd[1]: Listening on Syslog Socket.
    [  OK  ] Listening on Syslog Socket.
    [    4.363026] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    4.387424] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    4.411089] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    4.435147] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    4.455408] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    4.479208] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    4.503033] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    4.526816] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    4.556455] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    4.590724] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    4.623643] systemd[1]: Mounting Temporary Directory (/tmp)...
             Mounting Temporary Directory (/tmp)...
    [    4.653425] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
    [    4.665018] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
    [    4.679149] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.731175] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.763397] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.802067] u_dma_buf: loading out-of-tree module taints kernel.
    [    4.815313] systemd[1]: Starting udev Coldplug all Devices...
    [    4.832173] u-dma-buf udmabuf@0: assigned reserved memory node image_buf@0
             Starting udev Coldplug all Devices...
    [    4.859370] u-dma-buf udmabuf0: driver version = 3.2.4
    [    4.878839] systemd[1]: Mounted Huge Pages File System.
    [    4.898607] u-dma-buf udmabuf0: major number   = 237
    [  OK  ] Mounted Huge Pages File System.[    4.915227] u-dma-buf udmabuf0: minor number   = 0
    
    [    4.923133] systemd[1]: Mounted POSIX Message Queue File System.
    [    4.940107] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
    [  OK  ] Mounted POSIX Message Queue File Sy[    4.954347] u-dma-buf udmabuf0: phys address   = 0x00000001ff800000
    stem.
    [    4.977095] systemd[1]: Started Journal Service.
    [    4.988673] u-dma-buf udmabuf0: buffer size    = 4194304
    [  OK  ] Started Journal Service.
    [    5.001886] u-dma-buf udmabuf@0: driver installed.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory (/tmp).
    [  OK  ] Started Load Kernel Modules.
    [  OK  ] Started Remount Root and Kernel File Systems.
    [    5.092908] random: systemd: uninitialized urandom read (16 bytes read)
             Mounting Kernel Configuration File System.[    5.118443] random: systemd-journal: uninitialized urandom read (16 bytes read)
    ..
    [    5.138075] random: systemd: uninitialized urandom read (16 bytes read)
             Starting Flush Journal to Persistent Storage...
             Starting Apply Kernel Variables...
             Starting Create Static Device Nodes in /dev...
    [    5.234743] systemd-journald[95]: Received client request to flush runtime journal.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /var/volatile...
             Starting udev Kernel Device Manager...
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Network Time Synchronization...
             Starting Update UTMP about System Boot/Shutdown...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started udev Kernel Device Manager.
    [  OK  ] Started Network Time Synchronizatio[    6.173938] random: systemd-journal: uninitialized urandom read (16 bytes read)
    n.
    [    6.195389] random: systemd: uninitialized urandom read (16 bytes read)
    [  OK  ] Reached target System Time Set.
    [    6.230800] random: systemd: uninitialized urandom read (16 bytes read)
    [  OK  ] Reached target System Time Synchronized.
    [  OK  ] Started udev Coldplug all Devices.
             Starting udev Wait for Complete Device Initialization...
    [  OK  ] Reached target Hardware activated USB gadget.
    [    7.269881] random: systemd: uninitialized urandom read (16 bytes read)
    [    8.346579] random: crng init done
    [    8.350024] random: 78 urandom warning(s) missed due to ratelimiting
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started udev Wait for Complete Device Initialization.
    [  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting sshd.socket.
    [  OK  ] Listening on sshd.socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
             Starting Modem Manager...
    [  OK  ] Started Kernel Logging Service.
    [  OK  ] Started System Logging Service.
             Starting Comctl daemon...
    [  OK  ] Started D-Bus System Message Bus.
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
             Starting Telephony service...
             Starting rng-tools.service...
             Starting Login Service...
    [  OK  ] Started VIN initializing setting.
    [  OK  ] Started WatchdogTimer.
    [   11.379335] v4l2-comctl0: device v4l2-comctl called open()
    [  OK  ] Started IPv6 Packet Filtering Framework.
    [  OK  ] Started IPv4 Packet Filtering Framework.
    [  OK  ] Started rng-tools.service.
    [  OK  ] Started Comctl daemon.
    [  OK  ] Started Telephony service.
    [  OK  ] Reached target Network (Pre).
             Starting Connection service...
             Starting Network Service...
    [  OK  ] Started Modem Manager.
    [  OK  ] Started Login Service.
    [  OK  ] Started Network Service.
    [  OK  ] Started Connection service.
    [  OK  ] Reached target Network.
             Starting Permit User Sessions...
             Starting Target Communication Framework agent...
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS0.
    [  OK  ] Reached target Login Prompts.
    [  OK  ] Started Target Communication Framework agent.
    [  OK  ] Reached target Multi-User System.
             Starting Update UTMP about System Runlevel Changes...
             Starting WPA supplicant...
    [  OK  ] Started Update UTMP about System Runlevel Changes.
             Starting Hostname Service...
    [  OK  ] Started WPA supplicant.
    [  OK  ] Started Hostname Service.
    
    Poky (Yocto Project Reference Distro) 3.1.21 rzv2m ttyS0
    
    BSP: RZV2M/RZV2M Evaluation Board Kit/3.0.4
    LSI: RZV2M
    Version: 3.0.4
    rzv2m login: 
    
    

  • Hi anzal,
    Did you use the same firmware (same kernel, rootfs and dtb) for both boards?
    Can you see this file on your rootfs: /bin/comctld ? 
    What is the output of the command: cat /lib/modules/$(uname -r)/modules.builtin ?
    Kind Regards.