Hello,
I use R7S910035,e2stdio and AP4 to configure Buses for SRAM, 32bit data length. CS0. when i write data to sram,I can see from the oscilloscope that it takes 1 second to send the second time, which is too slow. I want a microsecond level sending time. How can I set it?? When I read data, I can read continuously at the microsecond level.
Hi chen,Let me ask you what is the purpose of your project?Do you want to run an example?Kind Regards.
What I want is to read and write SRAM. Writing SRAM is too slow now. My code writes SRAM continuously, but the oscilloscope shows that it takes only 1 second to write, which should be abnormal. Reading is normal and can be read continuously. If only there were an instance code for RZT1, thank you