Request for Linux Kernel Modules for DA16600MOD UART Interface (Wi-Fi and BLE) Integration with RZG3S

Hello Renesas Community,

We are currently working on integrating the DA16600MOD Wi-Fi and Bluetooth module into our custom-made system that uses the RZG3S processor. Our system is designed to use only the UART interface to interface with the DA16600MOD for Wi-Fi (UART0) and BLE communication.

Could anyone please provide guidance on the following:

  1. Linux Kernel Modules: Are there existing kernel modules or sample drivers available for integrating the DA16600MOD with the RZG3S system using only the UART interface?
  2. Driver Support: Is there a specific driver available that can be used for both Wi-Fi and BLE functionality via UART, or would additional configurations be required?
  3. Integration Steps: If there are any specific steps or configurations that need to be followed for successfully integrating the UART-based DA16600MOD in a custom system, we would appreciate the details.

Your support and any examples of successfully integrating this module would be greatly appreciated!

Thank you in advance!

Parents Reply Children
No Data