My screen is not display when I connect it with RZ/V2l by micro hdmi cable

I built an OS for RZ/V2L using yocto with core-image-weston and booted from SD successfully. Console shows up and can login as root. However when I connect it to a monitor via micro hdmi nothing is displayed. Has anyone had similar problems that can help me?

  • Hi,
    Can you see any messages on the console when you connect the HDMI on board?
    Kind Rergards.

  • root@smarc-rzv2l:~# modetest -M rcar-du
    Encoders:
    id crtc type possible crtcs possible clones
    38 37 none 0x00000001 0x00000001
    44 0 Virtual 0x00000001 0x00000002

    Connectors:
    id encoder status name size (mm) modes encoders
    39 38 connected HDMI-A-1 370x230 31 38

  • My dmesg 

    NOTICE:  BL2: v2.9(release):v2.5/rzg2l-1.00-3892-gcc1869562-dirty
    NOTICE:  BL2: Built : 04:12:39, Dec 14 2023
    NOTICE:  BL2: Booting BL31
    NOTICE:  BL31: v2.9(release):v2.5/rzg2l-1.00-3892-gcc1869562-dirty
    NOTICE:  BL31: Built : 04:12:39, Dec 14 2023
    
    
    U-Boot 2021.10 (Apr 19 2024 - 01:37:50 +0000)
    
    CPU:   Renesas Electronics CPU rev 1.0
    Model: smarc-rzv2l
    DRAM:  1.9 GiB
    WDT:   watchdog@0000000012800800
    WDT:   Started with servicing (60s timeout)
    MMC:   sd@11c00000: 0, sd@11c10000: 1
    Loading Environment from MMC... OK
    In:    serial@1004b800
    Out:   serial@1004b800
    Err:   serial@1004b800
    U-boot WDT started!
    Net:
    Error: ethernet@11c20000 address not set.
    No ethernet found.
    
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1 is current device
    17904128 bytes read in 2978 ms (5.7 MiB/s)
    40504 bytes read in 12 ms (3.2 MiB/s)
    Moving Image from 0x48080000 to 0x48200000, end=49380000
    ## Flattened Device Tree blob at 48000000
       Booting using the fdt blob at 0x48000000
       Loading Device Tree to 0000000057ff3000, end 0000000057fffe37 ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]
    [    0.000000] Linux version 5.10.201-cip41-yocto-standard (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 8.3.0, GNU ld (GNU Binutils) 2.31.1) #1 SMP PREEMPT Mon Dec 30 07:31:38 UTC 2024
    [    0.000000] Machine model: Renesas SMARC EVK based on r9a07g054l2
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000058000000, size 256 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma@58000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000068000000, size 128 MiB
    [    0.000000] OF: reserved mem: initialized node linux,multimedia, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 64 MiB
    [    0.000000] OF: reserved mem: initialized node image_buf@0, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000048000000-0x00000000bfffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   empty
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000048000000-0x00000000bfffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000048000000-0x00000000bfffffff]
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [    0.000000] psci: SMC Calling Convention v1.2
    [    0.000000] percpu: Embedded 23 pages/cpu s55384 r8192 d30632 u94208
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 483840
    [    0.000000] Kernel command line: root=/dev/mmcblk1p2 rootwait wdt_overflow=0
    [    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] Memory: 875864K/1966080K available (10880K kernel code, 1036K rwdata, 3356K rodata, 2112K init, 387K bss, 631464K reserved, 458752K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=2.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: 480 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] GICv3: Distributor has no Range Selector support
    [    0.000000] GICv3: 16 PPIs implemented
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000011940000
    [    0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (virt).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
    [    0.000004] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
    [    0.000182] Console: colour dummy device 80x25
    [    0.000578] printk: console [tty0] enabled
    [    0.000620] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
    [    0.000644] pid_max: default: 32768 minimum: 301
    [    0.000783] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.000807] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.002449] rcu: Hierarchical SRCU implementation.
    [    0.003215] Detected Renesas RZ/V2L r9a07g054 Rev 1
    [    0.003527] EFI services will not be available.
    [    0.003816] smp: Bringing up secondary CPUs ...
    [    0.004388] Detected VIPT I-cache on CPU1
    [    0.004431] GICv3: CPU1: found redistributor 100 region 0:0x0000000011960000
    [    0.004484] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]
    [    0.004608] smp: Brought up 1 node, 2 CPUs
    [    0.004660] SMP: Total of 2 processors activated.
    [    0.004672] CPU features: detected: Privileged Access Never
    [    0.004682] CPU features: detected: LSE atomic instructions
    [    0.004693] CPU features: detected: User Access Override
    [    0.004704] CPU features: detected: 32-bit EL0 Support
    [    0.004715] CPU features: detected: Common not Private translations
    [    0.004727] CPU features: detected: Data cache clean to the PoU not required for I/D coherence
    [    0.004741] CPU features: detected: CRC32 instructions
    [    0.004750] CPU features: detected: Speculative Store Bypassing Safe (SSBS)
    [    0.004763] CPU features: detected: 32-bit EL1 Support
    [    0.020349] CPU: All CPU(s) started at EL1
    [    0.020430] alternatives: patching kernel code
    [    0.022841] devtmpfs: initialized
    [    0.029151] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.029204] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
    [    0.040056] pinctrl core: initialized pinctrl subsystem
    [    0.040965] DMI not present or invalid.
    [    0.041459] NET: Registered protocol family 16
    [    0.042951] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [    0.043115] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.043273] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.043407] audit: initializing netlink subsys (disabled)
    [    0.043711] audit: type=2000 audit(0.040:1): state=initialized audit_enabled=0 res=1
    [    0.044259] thermal_sys: Registered thermal governor 'step_wise'
    [    0.044636] cpuidle: using governor menu
    [    0.044791] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.044878] ASID allocator initialised with 65536 entries
    [    0.071415] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.071452] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.071466] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.071479] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.073114] cryptd: max_cpu_qlen set to 1000
    [    0.078302] iommu: Default domain type: Translated
    [    0.079256] vgaarb: loaded
    [    0.079549] SCSI subsystem initialized
    [    0.079987] usbcore: registered new interface driver usbfs
    [    0.080043] usbcore: registered new interface driver hub
    [    0.080083] usbcore: registered new device driver usb
    [    0.080950] mc: Linux media interface: v0.10
    [    0.080986] videodev: Linux video capture interface: v2.00
    [    0.081060] pps_core: LinuxPPS API ver. 1 registered
    [    0.081072] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
    [    0.081098] PTP clock support registered
    [    0.081133] EDAC MC: Ver: 3.0.0
    [    0.082541] Advanced Linux Sound Architecture Driver Initialized.
    [    0.083376] clocksource: Switched to clocksource arch_sys_counter
    [    0.083610] VFS: Disk quotas dquot_6.6.0
    [    0.083681] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.089881] NET: Registered protocol family 2
    [    0.090147] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.091229] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
    [    0.091342] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.091503] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
    [    0.091793] TCP: Hash tables configured (established 16384 bind 16384)
    [    0.091969] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.092014] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.092207] NET: Registered protocol family 1
    [    0.092788] RPC: Registered named UNIX socket transport module.
    [    0.092817] RPC: Registered udp transport module.
    [    0.092828] RPC: Registered tcp transport module.
    [    0.092838] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.092859] PCI: CLS 0 bytes, default 64
    [    0.093536] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available
    [    0.094002] kvm [1]: HYP mode not available
    [    0.098120] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [    0.104191] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.104995] NFS: Registering the id_resolver key type
    [    0.105071] Key type id_resolver registered
    [    0.105083] Key type id_legacy registered
    [    0.105175] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.105191] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.105229] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    [    0.105917] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
    [    0.105948] io scheduler mq-deadline registered
    [    0.105960] io scheduler kyber registered
    [    0.151160] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [    0.152435] SuperH (H)SCI(F) driver initialized
    [    0.162360] loop: module loaded
    [    0.165359] tun: Universal TUN/TAP device driver, 1.6
    [    0.165629] CAN device driver interface
    [    0.166179] e1000e: Intel(R) PRO/1000 Network Driver
    [    0.166196] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    [    0.166829] VFIO - User Level meta-driver version: 0.3
    [    0.167133] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    0.167155] ehci-pci: EHCI PCI platform driver
    [    0.167222] ehci-platform: EHCI generic platform driver
    [    0.167996] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
    [    0.168054] ohci-pci: OHCI PCI platform driver
    [    0.168138] ohci-platform: OHCI generic platform driver
    [    0.169371] usbcore: registered new interface driver usb-storage
    [    0.169905] renesas_usbhs 11c60000.usb: host probed
    [    0.169927] renesas_usbhs 11c60000.usb: no transceiver found
    [    0.170071] renesas_usbhs 11c60000.usb: gadget probed
    [    0.170180] renesas_usbhs 11c60000.usb: platform init failed.
    [    0.170323] renesas_usbhs 11c60000.usb: probe failed (-517)
    [    0.171296] usbcore: registered new interface driver usbtouchscreen
    [    0.171435] i2c /dev entries driver
    [    0.176410] rzg2l-csi2 10830400.csi2: 2 lanes found
    [    0.180679] EDAC rzg2l-edac: IO mapped reg addr: 0x11410000
    [    0.180992] EDAC MC0: Giving out device to module rzg2l-edac controller renesas,r9a07g054-edac: DEV 11410000.edac (INTERRUPT)
    [    0.183701] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.183747] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.184386] clocksource: timer@12801400: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604467 ns
    [    0.184424] sched_clock: 32 bits at 100MHz, resolution 10ns, wraps every 21474836475ns
    [    0.184449] /soc/timer@12801400: used for clocksource
    [    0.184875] /soc/timer@12801800: used for clock events
    [    0.185803] usbcore: registered new interface driver usbhid
    [    0.185827] usbhid: USB HID core driver
    [    0.189263] NET: Registered protocol family 10
    [    0.190239] Segment Routing with IPv6
    [    0.190321] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    0.190826] NET: Registered protocol family 17
    [    0.190855] can: controller area network core
    [    0.190927] NET: Registered protocol family 29
    [    0.190942] can: raw protocol
    [    0.190957] can: broadcast manager protocol
    [    0.190975] can: netlink gateway - max_hops=1
    [    0.191153] Key type dns_resolver registered
    [    0.191663] registered taskstats version 1
    [    0.199868] thermal emergency: set temperature to 111 celsius
    [    0.199988] thermal emergency: shutdown target cpus 1
    [    0.200002] thermal emergency: freq scaled target cpus 0
    [    0.202116] gpio-449 (sd0_dev_sel): hogged as output/high
    [    0.202176] gpio-458 (can0_stb): hogged as output/low
    [    0.202203] gpio-459 (can1_stb): hogged as output/low
    [    0.202975] pinctrl-rzg2l 11030000.pinctrl: pinctrl-rzg2l support registered
    [    0.207520] gpt-rzg2l 10048400.gpt: RZ/G2L GPT Driver probed
    [    0.208230] 1004b800.serial: ttySC0 at MMIO 0x1004b800 (irq = 39, base_baud = 0) is a scif
    [    1.309706] printk: console [ttySC0] enabled
    [    1.316825] renesas_spi 1004b000.spi: DMA available
    [    1.322180] renesas_spi 1004b000.spi: probed
    [    1.327635] rcar_canfd 10050000.can: can_clk rate is 50000000
    [    1.333964] rcar_canfd 10050000.can: device registered (channel 0)
    [    1.340211] rcar_canfd 10050000.can: can_clk rate is 50000000
    [    1.346469] rcar_canfd 10050000.can: device registered (channel 1)
    [    1.352664] rcar_canfd 10050000.can: global operational state (clk 0, fdmode 1)
    [    1.360937] ravb 11c20000.ethernet: no valid MAC address supplied, using a random one
    [    1.371146] ravb 11c20000.ethernet eth0: Base address at 0x11c20000, 06:47:a8:0b:73:70, IRQ 140.
    [    1.381045] ravb 11c30000.ethernet: no valid MAC address supplied, using a random one
    [    1.391240] ravb 11c30000.ethernet eth1: Base address at 0x11c30000, 32:ff:14:3e:df:21, IRQ 143.
    [    1.427444] ehci-platform 11c50100.usb: EHCI Host Controller
    [    1.433170] ehci-platform 11c50100.usb: new USB bus registered, assigned bus number 1
    [    1.441141] ehci-platform 11c50100.usb: irq 148, io mem 0x11c50100
    [    1.459384] ehci-platform 11c50100.usb: USB 2.0 started, EHCI 1.10
    [    1.466227] hub 1-0:1.0: USB hub found
    [    1.470019] hub 1-0:1.0: 1 port detected
    [    1.474970] ehci-platform 11c70100.usb: EHCI Host Controller
    [    1.480681] ehci-platform 11c70100.usb: new USB bus registered, assigned bus number 2
    [    1.488592] ehci-platform 11c70100.usb: irq 149, io mem 0x11c70100
    [    1.507388] ehci-platform 11c70100.usb: USB 2.0 started, EHCI 1.10
    [    1.514216] hub 2-0:1.0: USB hub found
    [    1.518009] hub 2-0:1.0: 1 port detected
    [    1.522858] ohci-platform 11c50000.usb: Generic Platform OHCI controller
    [    1.529629] ohci-platform 11c50000.usb: new USB bus registered, assigned bus number 3
    [    1.537590] ohci-platform 11c50000.usb: irq 146, io mem 0x11c50000
    [    1.634028] hub 3-0:1.0: USB hub found
    [    1.637824] hub 3-0:1.0: 1 port detected
    [    1.642688] ohci-platform 11c70000.usb: Generic Platform OHCI controller
    [    1.649434] ohci-platform 11c70000.usb: new USB bus registered, assigned bus number 4
    [    1.657397] ohci-platform 11c70000.usb: irq 147, io mem 0x11c70000
    [    1.754029] hub 4-0:1.0: USB hub found
    [    1.757830] hub 4-0:1.0: 1 port detected
    [    1.762675] renesas_usbhs 11c60000.usb: host probed
    [    1.767619] renesas_usbhs 11c60000.usb: no transceiver found
    [    1.773386] renesas_usbhs 11c60000.usb: gadget probed
    [    1.778712] renesas_usbhs 11c60000.usb: probed
    [    1.912532] ov5645 0-003c: OV5645 detected at address 0x3c
    [    1.919792] ov5645 0-003c: Consider updating driver ov5645 to match on endpoints
    [    1.927686] rzg2l-cru 10830000.video: Device registered as video0
    [    1.934091] i2c-riic 10058000.i2c: registered with 100000Hz bus speed
    [    1.951033] i2c-riic 10058400.i2c: registered with 100000Hz bus speed
    [    1.961657] rtc-isl1208 3-006f: rtc power failure detected, please set clock.
    [    1.970614] rtc-isl1208 3-006f: registered as rtc0
    [    1.975799] rtc-isl1208 3-006f: setting system clock to 2000-01-01T00:00:00 UTC (946684800)
    [    1.990169] i2c-riic 10058c00.i2c: registered with 400000Hz bus speed
    [    2.000674] spi-nor spi1.0: mt25qu512a (65536 Kbytes)
    [    2.006493] 3 fixed-partitions partitions found on MTD device spi1.0
    [    2.012868] Creating 3 MTD partitions on "spi1.0":
    [    2.017655] 0x000000000000-0x00000001c000 : "bl2"
    [    2.023664] 0x00000001d000-0x000002000000 : "fip"
    [    2.029564] 0x000002000000-0x000004000000 : "user"
    [    2.038883] rz-ssi-pcm-audio 10049c00.ssi: DMA enabled
    [    2.045270] rz-ssi-pcm-audio 1004a000.ssi: DMA enabled
    [    2.048258] renesas_sdhi_internal_dmac 11c10000.mmc: mmc1 base at 0x0000000011c10000, max clock rate 100 MHz
    [    2.055473] renesas_sdhi_internal_dmac 11c00000.mmc: mmc0 base at 0x0000000011c00000, max clock rate 100 MHz
    [    2.071406] [drm] Initialized rcar-du 1.0.0 20130110 for 10890000.display on minor 0
    [    2.079196] [drm] Device 10890000.display probed
    [    2.155181] Console: switching to colour frame buffer device 170x48
    [    2.177734] rcar-du 10890000.display: [drm] fb0: rcar-dudrmfb frame buffer device
    [    2.211266] mmc0: new HS200 MMC card at address 0001
    [    2.217007] mmcblk0: mmc0:0001 G1M15M 59.3 GiB
    [    2.221772] mmcblk0boot0: mmc0:0001 G1M15M partition 1 31.5 MiB
    [    2.227934] mmcblk0boot1: mmc0:0001 G1M15M partition 2 31.5 MiB
    [    2.234175] mmcblk0rpmb: mmc0:0001 G1M15M partition 3 4.00 MiB, chardev (242:0)
    [    2.243043]  mmcblk0: p1
    [    2.292962] ALSA device list:
    [    2.296076]   #0: rz-ssi-dai-wm8978-hifi
    [    2.300070]   #1: sound_card
    [    2.303842] Waiting for root device /dev/mmcblk1p2...
    [    2.502937] mmc1: new ultra high speed SDR104 SDHC card at address 0001
    [    2.510334] mmcblk1: mmc1:0001 USD00 14.7 GiB
    [    2.517111]  mmcblk1: p1 p2
    [    2.556374] EXT4-fs (mmcblk1p2): INFO: recovery required on readonly filesystem
    [    2.563788] EXT4-fs (mmcblk1p2): write access will be enabled during recovery
    [    2.598363] EXT4-fs (mmcblk1p2): recovery complete
    [    2.608785] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
    [    2.618902] VFS: Mounted root (ext4 filesystem) readonly on device 179:26.
    [    2.634507] devtmpfs: mounted
    [    2.641645] Freeing unused kernel memory: 2112K
    [    2.648267] Run /sbin/init as init process
    [    3.117650] systemd[1]: System time before build time, advancing clock.
    [    3.168342] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    3.194598] systemd[1]: Detected architecture arm64.
    
    Welcome to Poky (Yocto Project Reference Distro) 3.1.31 (dunfell)!
    
    [    3.225122] systemd[1]: Set hostname to <smarc-rzv2l>.
    [    3.769274] random: systemd: uninitialized urandom read (16 bytes read)
    [    3.778329] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
    [    3.792857] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
    [    3.806600] systemd[1]: Created slice system-getty.slice.
    [  OK  ] Created slice system-getty.slice.
    [    3.831621] random: systemd: uninitialized urandom read (16 bytes read)
    [    3.842007] systemd[1]: Created slice system-serial\x2dgetty.slice.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    3.867628] random: systemd: uninitialized urandom read (16 bytes read)
    [    3.878030] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    3.904032] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password …ts to Console Directory Watch.
    [    3.931969] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password R…uests to Wall Directory Watch.
    [    3.959815] systemd[1]: Reached target Host and Network Name Lookups.
    [  OK  ] Reached target Host and Network Name Lookups.
    [    3.983719] systemd[1]: Reached target Paths.
    [  OK  ] Reached target Paths.
    [    4.003710] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    4.027717] systemd[1]: Reached target Slices.
    [  OK  ] Reached target Slices.
    [    4.047730] systemd[1]: Reached target Swap.
    [  OK  ] Reached target Swap.
    [    4.089789] systemd[1]: Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [    4.115717] systemd[1]: Reached target RPC Port Mapper.
    [  OK  ] Reached target RPC Port Mapper.
    [    4.141775] systemd[1]: Listening on Syslog Socket.
    [  OK  ] Listening on Syslog Socket.
    [    4.164081] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    4.192578] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    4.216221] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    4.240356] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    4.264524] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    4.288398] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    4.312119] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    4.340629] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    4.368295] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    4.396397] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    4.425425] systemd[1]: Mounting Temporary Directory (/tmp)...
             Mounting Temporary Directory (/tmp)...
    [    4.454988] systemd[1]: Starting Create list of static device nodes for the current kernel...
             Starting Create list of st…odes for the current kernel...
    [    4.491463] systemd[1]: Starting Start psplash boot splash screen...
             Starting Start psplash boot splash screen...
    [    4.521930] systemd[1]: Starting RPC Bind...
             Starting RPC Bind...
    [    4.549023] systemd[1]: Starting File System Check on Root Device...
             Starting File System Check on Root Device...
    [    4.582929] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.708932] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.721010] systemd[1]: Starting udev Coldplug all Devices...
             Starting udev Coldplug all Devices...
    [    4.737295] systemd[1]: Started Start psplash boot splash screen.
    [  OK  ] Star[    4.744539] systemd[1]: Mounted Huge Pages File System.
    ted Start psplash boot splash s[    4.753084] systemd[1]: Mounted POSIX Message Queue File System.
    creen.
    [  OK  ] Mounted Huge Pages File[    4.764653] systemd[1]: Mounted Kernel Debug File System.
     System.
    [  OK  ] Mounted POSIX[    4.775352] systemd[1]: Mounted Temporary Directory (/tmp).
     Message Queue File System.
    [  OK  ] Mounted     4.786121] systemd[1]: Started Create list of static device nodes for the current kernel.
    ;1;39mKernel Debug File System.
    [  O[    4.797275] random: systemd: uninitialized urandom read (16 bytes read)
    K  ] Mounted Temporary Directory (/tmp).
    [  OK  ] Started  systemd[1]: Started Start psplash-systemd progress communication helper.
    [0;1;39mCreate list of sta… nodes for the current kernel.
    [  OK  ] Started Start psplash-syst…progress communication helper.
    [    4.840032] random: systemd-journal: uninitialized urandom read (16 bytes read)
    [    4.908797] systemd[1]: Started RPC Bind.
    [  OK  ] Started RPC Bind.
    [    4.929782] random: systemd-journal: uninitialized urandom read (16 bytes read)
    [    4.935636] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [    4.980028] mali_kbase: loading out-of-tree module taints kernel.
    [    4.993162] mali 11840000.gpu: Kernel DDK version r47p0-01eac0
    [    5.000136] mali 11840000.gpu: GPU metrics tracepoint support enabled
    [    5.009747] mali 11840000.gpu: Register LUT 00070000 initialized for GPU arch 0x00070009
    [    5.018489] mali 11840000.gpu: GPU identified as 0x3 arch 7.0.9 r0p0 status 0
    [    5.026095] mali 11840000.gpu: No priority control manager is configured
    [    5.033117] mali 11840000.gpu: Large page allocation set to false after hardware feature check
    [    5.042135] mali 11840000.gpu: No memory group manager is configured
    [    5.052490] mali 11840000.gpu: Probed as mali0
    [    5.134405] rgnmm_drv mmngr: assigned reserved memory node linux,multimedia
    [  OK  ] Started File System Check on Root Device.
             Starting Remount Root and Kernel File Systems...
    [  OK  ] Started Load Kernel Modules.
             Mounting Kernel Configuration File System...
             Starting Apply Kernel Variables...[    5.381871] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
    
    [  OK  ] Started Remount Root and Kernel File Systems.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started Apply Kernel Variables.
             Starting Flush Journal to Persistent Storage...
             Starting Create Static Device Nodes in /dev...
    [    5.528093] systemd-journald[169]: Received client request to flush runtime journal.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /var/volatile...
             Starting udev Kernel Device Manager...
    [  OK  ] Started udev Coldplug all Devices.
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Create Volatile Files and Directories.
    [    5.872120] random: systemd: uninitialized urandom read (16 bytes read)
             Starting     5.910164] random: systemd-journal: uninitialized urandom read (16 bytes read)
    39mNetwork Time Synchronization...
    [    5.932145] random: systemd: uninitialized urandom read (16 bytes read)
             Starting Update UTMP about System Boot/Shutdown...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started udev Kernel Device Manager.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target System Time Set.
    [  OK  ] Reached target System Time Synchronized.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
    [  OK  ] Started Kernel Logging Service.
    [  OK  ] Started System Logging Service.
    [  OK  ] Started D-Bus System Message Bus.
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
             Starting Telephony service...
             Starting Login Service...
    [  OK  ] Started VIN initializing setting.
    [    6.679462] random: crng init done
    [    6.682883] random: 92 urandom warning(s) missed due to ratelimiting
    [  OK  ] Started IPv6 Packet Filtering Framework.
    [  OK  ] Started IPv4 Packet Filtering Framework.
    [  OK  ] Reached target Network (Pre).
             Starting Connection service...
             Starting Network Service...
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started Telephony service.
    [  OK  ] Started Login Service.
    [  OK  ] Started Network Service.
    [  OK  ] Started Connection service.
    [  OK  ] Reached target Network.
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Permit User Sessions...
             Starting Target Communication Framework agent...
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Created slice system-weston.slice.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttySC0.
    [  OK  ] Reached target Login Prompts.
    [    8.032034] Microchip KSZ9131 Gigabit PHY 11c20000.ethernet-ffffffff:07: attached PHY driver [Microchip KSZ9131 Gigabit PHY] (mii_bus:phy_addr=11c20000.ethernet-ffffffff:07, irq=169)
    [  OK  ] Started Target Communication Framework agent.
    [    8.184935] Microchip KSZ9131 Gigabit PHY 11c30000.ethernet-ffffffff:07: attached PHY driver [Microchip KSZ9131 Gigabit PHY] (mii_bus:phy_addr=11c30000.ethernet-ffffffff:07, irq=170)
    [  OK  ] Reached target Multi-User System.
    [  OK  ] Reached target Hardware activated USB gadget.
             Starting Hostname Service...
             Starting Update UTMP about System Runlevel Changes...
             Starting watchdog daemon...
    [  OK  ] Started Weston Wayland Compositor.
             Starting WPA supplicant...
    [  OK  ] Started watchdog daemon.
    [  OK  ] Started Update UTMP about System Runlevel Changes.
             Starting Save/Restore Sound Card State...
    [  OK  ] Started WPA supplicant.
    [  OK  ] Started Save/Restore Sound Card State.
    [  OK  ] Created slice User Slice of UID 0.
    [  OK  ] Reached target Sound Card.
             Starting User Runtime Directory /run/user/0...
    [  OK  ] Started Hostname Service.
    [  OK  ] Started User Runtime Directory /run/user/0.
             Starting User Manager for UID 0...
    [    9.381387] audit: type=1006 audit(1736499193.604:2): pid=266 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
    [  OK  ] Started User Manager for UID 0.
    [  OK  ] Started Session c1 of user root.
    
    Poky (Yocto Project Reference Distro) 3.1.31 smarc-rzv2l ttySC0
    
    BSP: RZV2L/RZV2L-SMARC-EVK/3.0.6-update2
    LSI: RZV2L
    Version: 3.0.6-update2
    

  • Hi,
    Can you please try to make a clean build and try again?
    Kind Regards.

  • Hello  

    I attempted a clean build following the instructions in this manual, and it worked perfectly. Please take a look at this and include the graphics layer while building the image.

    r01us0617ej0103-rz-v(Linux Start-up Guide RZV2L).pdf

    Kind Regards,

    GN_Renesas

  • Can you send me your image to boot? I cleaned and rebuilt but it did not work. Or my hardware is issue.

  • How can I set button to boot with your image? It run NOTICE: BL2: v2.9(release):cc18695-dirty
    NOTICE: BL2: Built : 04:12:39, Dec 14 2023 and not boot.

  • NOTICE: BL2: v2.9(release):v2.5/rzg2l-1.00-3892-gcc1869562-dirty
    NOTICE: BL2: Built : 04:12:39, Dec 14 2023
    NOTICE: BL2: Booting BL31
    NOTICE: BL31: v2.9(release):v2.5/rzg2l-1.00-3892-gcc1869562-dirty
    NOTICE: BL31: Built : 04:12:39, Dec 14 2023


    U-Boot 2021.10 (Apr 19 2024 - 01:37:50 +0000)

    CPU: Renesas Electronics CPU rev 1.0
    Model: smarc-rzv2l
    DRAM: 1.9 GiB
    WDT: watchdog@0000000012800800
    WDT: Started with servicing (60s timeout)
    MMC: sd@11c00000: 0, sd@11c10000: 1
    Loading Environment from MMC... OK
    In: serial@1004b800
    Out: serial@1004b800
    Err: serial@1004b800
    U-boot WDT started!
    Net:
    Error: ethernet@11c20000 address not set.
    No ethernet found.

    Hit any key to stop autoboot: 0
    switch to partitions #0, OK
    mmc1 is current device
    Failed to load 'Image-smarc-rzv2l.bin'
    Failed to load 'Image-r9a07g054l2-smarc.dtb'
    Bad Linux ARM64 Image magic!
    => printenv
    baudrate=115200
    bootargs=root=/dev/mmcblk1p2 rootwait
    bootcmd=mmc dev 1;fatload mmc 1:1 0x48080000 Image-smarc-rzv2l.bin; fatload mmc 1:1 0x48000000 Image-r9a07g054l2-smarc.dtb; booti 0x48080000 - 0x48000000
    bootcmd_check=if mmc dev 1; then run sd1load; else run emmcload; fi
    bootdelay=2
    bootimage=unzip 0x4A080000 0x48080000; booti 0x48080000 - 0x48000000
    bootm_size=0x10000000
    emmcload=ext4load mmc 0:2 0x48080000 boot/Image;ext4load mmc 0:2 0x48000000 boot/r9a07g054l2-smarc.dtb;run prodemmcbootargs
    fdtcontroladdr=bbf22e20
    loadaddr=0x58000000
    platform=cpu
    prodemmcbootargs=setenv bootargs rw rootwait earlycon root=/dev/mmcblk0p2
    prodsdbootargs=setenv bootargs rw rootwait earlycon root=/dev/mmcblk1p2
    sd1load=ext4load mmc 1:2 0x48080000 boot/Image;ext4load mmc 1:2 0x48000000 boot/r9a07g054l2-smarc.dtb;run prodsdbootargs
    stderr=serial@1004b800
    stdin=serial@1004b800
    stdout=serial@1004b800
    usb_pgood_delay=2000
    ver=U-Boot 2021.10 (Apr 19 2024 - 01:37:50 +0000)
    wdt_status=1
    wdt_timeout=60000

    Environment size: 1005/65532 bytes
    =>

  • Hello  

    Please refer to my build file. It appears that your SD card files may be corrupted, which is causing this error. Kindly check the manual for instructions on flashing the SD card. Additionally, ensure that you are uploading the correct DDR files as per the board specifications.

    https://community.renesas.com/cfs-file/__key/communityserver-discussions-components-files/180/smarc_2D00_rzv2l.7z

    Kind Regards,

    GN_Renesas