I see in this link that RZ/V2H supports the interpreter mode https://github.com/renesas-rz/rzv_drp-ai_tvm/blob/56b3dd425ba694dbbdd7766fa1295671f1ffccf0/tutorials/tutorial_RZV2H.md#c-interpreter-mode . It means that we can run inference compiled model on PC on the custom dataset to check accuracy. I understood that this guide is for RZ/V2H and RZ/V2H support INT8 model.
My question is that: Is there the interpreter mode for RZ/V2L? I understood that RZ/V2L supports only FP16 model and I do not see any guide for the interpreter mode with RZ/V2L.
Furthermore, I think that to evaluate actual accuracy of model on the board, we need to load the custom dataset on the board and run inference.
Thank you.