Assistance required for PMIC RAA215300A2GNP#HA0 in board bring up

We are currently in the board bring-up stage for our design, where we have used the RAA215300A2GNP#HA0 PMIC to provide power for the RZ/G2L processor. However, we are facing an issue where the PMIC is not providing any voltage output.

Current Setup and Observations:

  • Power Input: 5V supplied from an RPS (regulated power supply).
  • Power-On Pin: Set to default low, with a push button used to pull it high for 3 seconds.
  • CEN Pin: Pulled high using a 10kΩ resistor to the input voltage.
  • No output voltage observed from the PMIC.

Request for Assistance:

  • Could you please provide guidance on troubleshooting this issue?
  • Are there any additional power-on sequence requirements that we may have overlooked?
  • Any specific test points or debugging steps we should follow to identify the root cause?
Parents Reply Children
No Data