USB Isochronous request with r_usbh0 basic driver

Hi,
I am implementing the USB video class for host on a RZ/A2M MCU, starting from the MSC host sample code.
I have finished the device configuration part, and I must now implement the isochronous request to retrieve video data.

I would like to use endpoints with multiple transactions per microframe, but I am not sure that the r_usbh0 basic driver handles it.
I noticed that the driver function R_USBH0_HstdSetPipe sets the maximum packet size without fully parsing the wMaxPacketSize field of the endpoint descriptor.
Indeed, the 5 highest bits do not describe the packet size but the number of transactions per microframe.
If I set the right MPS in the st_usbh0_pipe_t structure, which can reach up to 3072 bytes, will the USB driver handle it ?

I am also wondering how asynchronous requests work with this driver. It is not described in the driver documentation and the sample codes do not use them. The official USB 2.0 and UVC documentations did not help me either.
When I use a buffer length of 3060 bytes in the request structure st_usbh0_utr_t, I get two different results from the EHCI : sometimes USBH0_DATA_ERR, and nothing was written in the buffer, and sometimes USBH0_DATA_READING, which indicates a successful request I believe, but only the 12 header bytes are written to zeroes.
I do not know if the problem comes from the camera that does not accept my request, or a wrong use of the USB driver.
I noticed that asking for more than 3072 bytes makes the response callback never trigger.

I suppose that I cannot just queue a big empty buffer, large enough to hold an entire video frame ? I presume the buffer is limited to the maximum theoretical packet size, 3072 bytes ?
Do I need to fill the buffer ? I noticed my PC does it. Here is a truncated isochronous request my PC sent :

Frame 537: 1575 bytes on wire (12600 bits), 1575 bytes captured (12600 bits) on interface \\.\USBPcap2, id 0
USB URB
    [Source: host]
    [Destination: 2.7.1]
    USBPcap pseudoheader length: 1575
    IRP ID: 0xffffd4825b3c78a0
    IRP USBD_STATUS: USBD_STATUS_SUCCESS (0x00000000)
    URB Function: URB_FUNCTION_ISOCH_TRANSFER (0x000a)
    IRP information: 0x00, Direction: FDO -> PDO
    URB bus id: 2
    Device address: 7
    Endpoint: 0x81, Direction: IN
    URB transfer type: URB_ISOCHRONOUS (0x00)
    Packet Data Length: 0
    [Response in: 553]
    Isochronous transfer start frame: 0
    Isochronous transfer number of packets: 128
    Isochronous transfer error count: 0
USB isochronous packet
    ISO Data offset: 0x00000000
    ISO Data length: 0x00000000 (irrelevant)
    ISO USBD status: USBD_STATUS_SUCCESS (0x00000000) (irrelevant)
USB isochronous packet
    ISO Data offset: 0x00000bf4
    ISO Data length: 0x00000000 (irrelevant)
    ISO USBD status: USBD_STATUS_SUCCESS (0x00000000) (irrelevant)
...
USB isochronous packet
    ISO Data offset: 0x0005ee0c
    ISO Data length: 0x00000000 (irrelevant)
    ISO USBD status: USBD_STATUS_SUCCESS (0x00000000) (irrelevant)


Regards,

AlexR


Parents
  • Hi,
    It seems my first response did not get posted.
    I forgot to mention that I am using FreeRTOS, this is why I started from the MSC sample code. I could not find in the Azure example the use of the r_usbh0 functions I am interested in.
    I managed to make successful isochronous request, but only by waiting for one to finish before sending the next.
    I am using usbh0_hstd_transfer_start() to make those requests. I looked at the underlying HCD and EHCI code and it seems that it should support queueing transactions.
    However when I try to queue multiple requests, i.e. calling usbh0_hstd_transfer_start() multiple times successively using different st_usbh0_utr_t message structures, only one request gets a callback anwser. I noticed the same iTD gets reused for every request.
    What is the proper way to queue requests ?

    I modified these user-defined constants, are there any other that I need to change ?
    #define USBH0_EHCI_PFL_SIZE (1024u)
    #define USBH0_EHCI_NUM_QTD (9180u)
    #define USBH0_EHCI_NUM_ITD (32u)
    #define USBH0_EHCI_NUM_SITD (2u)
    #define USBH0_EHCI_ITD_DATA_SIZE (1024u)

    Is the EHCI driver capable of handling multiple transactions per microframe ? As described in the first post, how must I set the mps field of the st_usbh0_pipe_t structure ?

    Regards,

    AlexR

  • Hii  

    For isochronous transfers, it’s important to allocate a new iTD (Isochronous Transfer Descriptor) for each transfer. Reusing the same iTD across transfers can lead to data loss or unexpected errors, since EHCI expects fresh descriptors for every microframe transaction.

    Also, reusing iTDs without ensuring the buffer is flushed and ready can lead to data integrity issues. The USB hardware manual actually covers this—please refer to section 33.9.9.5 (Transmit buffer flush for isochronous transfer). That might give you a better understanding of what’s expected before submitting new transfer descriptors.

    To help further, could you please share the code ? where you're configuring the endpoint and setting up the transfer? I'd like to review how the buffer and iTDs are being managed, and see if any driver-level tweaks might be needed. This will help us understand how the request is being made and whether anything needs to be modified in the driver logic.

    Looking forward to your response.

    GN_Renesas

  • Hi,

    Thanks for the response.
    Apparently my answer did not go through again, maybe because of the code insert I used.
    Here is my answer with the code pasted as text then.

    Here is the function I call to set the pipe. It is very similar to R_USBH0_HstdSetPipe.
    I found in the RZ/A2M group documentation that high-bandwidth isochronous requests are not supported, so the maximum packet size is up to 1024.

    /***********************************************************************************************************************
    Function Name : uvc_set_pipe
    Description : Set up the pipe
    Argument : uint8_t *p_descriptor : Endpoint descriptor address
    : uint8_t ifnum : Interface number
    : uint16_t pipe_id : Pipe ID global variable, to fill
    Return value : usbh0_er_t : Error value
    ***********************************************************************************************************************/
    usbh0_er_t uvc_set_pipe(uint8_t *p_descriptor, uint8_t ifnum, uint16_t *pipe_id) // Based off R_USBH0_HstdSetPipe.
    {
    st_usbh0_pipe_t *p_pipe = &g_usbh0_hstd_pipe[1];
    uint16_t temp_pipe_id = 1;

    /* Search Empty Pipe */
    while (0 != p_pipe->epnum)
    {
    p_pipe++;
    temp_pipe_id++;
    if (temp_pipe_id >= USBH0_MAXPIPE)
    {
    USBH0_PRINTF0("PIPE_FULL ERROR\n");
    return USBH0_ERROR;
    }
    }

    /* Get value from Endpoint Descriptor */
    p_pipe->epnum = (p_descriptor[USBH0_EP_B_EPADDRESS] & USBH0_EP_NUMMASK);
    p_pipe->direction = (p_descriptor[USBH0_EP_B_EPADDRESS] & USBH0_EP_DIRMASK);
    p_pipe->type = (p_descriptor[USBH0_EP_B_ATTRIBUTES] & USBH0_EP_TRNSMASK);
    p_pipe->mps = ((uint16_t)(p_descriptor[USBH0_EP_W_MPS_H] << 8)
    | (uint16_t)(p_descriptor[USBH0_EP_W_MPS_L])); // max 1024 supported

    /* Get value from Attach Info */
    p_pipe->devaddr = g_uvc_dev_info.addr;
    p_pipe->ifnum = ifnum;
    *pipe_id = temp_pipe_id;

    return USBH0_OK;
    } /* End of function uvc_set_pipe() */

    /***********************************************************************************************************************/


    Here is the function where I start the transfer. I call it several times to queue multiple transfers with different buffers. The buffers are circular to allow storing requests which await parsing while sending the next.

    /******************************************************************************
    Function Name : usbh0_huvc_get_data
    Description : Get video data
    Argument : uint16_t buff_id : Output buffer ID
    Return value : usbh0_er_t : Error Code
    ******************************************************************************/
    usbh0_er_t usbh0_huvc_get_data(uint16_t buff_id)
    {
    uint16_t circ_buff_id = 0xFFFF;
    for(int i = 0; i < UVC_CIRC_BUFF_SIZE; i++)
    {
    if(UVC_WRITE==g_uvc_data_buff_state[buff_id][i])
    {
    circ_buff_id = i;
    break;
    }
    }

    if(0xFFFF==circ_buff_id) //circular buffer full
    {
    printf("Circular buffer of buff %d full\n", buff_id);
    return;
    }

    uint8_t *buff = g_uvc_data_buffer[buff_id][circ_buff_id];
    uint16_t msg_info = USBH0_MSG_HUVC_DATA_RQST + buff_id*100 + circ_buff_id;
    g_uvc_data_buff_state[buff_id][circ_buff_id] = UVC_WAIT;

    memset(buff, 0, UVC_DATA_BUFFER_SIZE*sizeof(uint8_t));

    /* transfer request packet */
    g_usbh0_uvc_transfer[buff_id][circ_buff_id].keyword = g_uvc_data_pipe;
    g_usbh0_uvc_transfer[buff_id][circ_buff_id].p_tranadr = buff;
    g_usbh0_uvc_transfer[buff_id][circ_buff_id].tranlen = UVC_DATA_BUFFER_SIZE-1;
    g_usbh0_uvc_transfer[buff_id][circ_buff_id].complete = &usbh0_uvc_rqst_callback;
    g_usbh0_uvc_transfer[buff_id][circ_buff_id].msginfo = msg_info;

    /* err = R_USBH0_HstdTransferStart(&g_usbh0_uvc_transfer); */
    usbh0_er_t err = usbh0_hstd_transfer_start(&g_usbh0_uvc_transfer[buff_id][circ_buff_id]);
    return err;
    } /* eof usbh0_huvc_get_data() */

    /******************************************************************************/



    Only one transfer gets a call back answer. I think the problem comes from the driver function usbh0_hstd_ehci_search_itd(), called inside usbh0_hstd_ehci_make_isochronous_request().
    I noticed this search function returns the same iTD when I make several simultaneous requests, even when I ask for 20 requests, although the iTD can obviously not store that many requests.

    I crudely fixed it by skipping usbh0_hstd_ehci_search_itd() and always initializing a new iTD in usbh0_hstd_ehci_make_isochronous_request().
    I had to clear these iTDs in usbh0_hstd_ehci_transfer_end_itd(), which I implemented by looking at how usbh0_hstd_ehci_clear_device_itd did it.
    These changes allow me to make multiple requests which do get callback answers.


    I ask for 8 times the maximum packet size of the endpoint at each request, so that each iTD will consist of 8 transactions. Is it the right size to ask ?

    The output buffer I receive look strange : I get zeroes, then a normal UVC packet (header + payload, so one USB transaction), then zeroes again. The offsets at which the packet start always change. I sometimes get another UVC packet in the buffer as well, but non zero data does not exceed 2000 bytes. Sometimes I get payload data without any header, as if I received half a packet.
    I do not get more than 12 packets with the same UVC Frame ID before it changes, which is very weird.

    All this makes me think I am missing some packets by not sending requests at a high enough fequency. I tried to limit the latency between a request finishing and the new one starting, but I faced another problem :
    I am using the same code architecture as the MSC sample : a main task and a driver task that just handles request response, woken using the mailbox. However the mailbox seems to take a long time to wake up after a mail is sent. After a mail is sent, the main loop can run several dozen of times before the driver task wakes up. I tried setting the task priority higher, to no avail. Is there a FreeRTOS parameter I can to change to speed up this ?

    Regards,

    AlexR

  • Hii  ,

    can you try 

    Reduce each tranlen to 1024 bytes, queue many single‑transaction iTDs.

    Insert the buffer‑flush sequence per section 33.9.9.5.

    Switch your mailbox wakeup to direct‑to‑task notifications.

    Please try these adjustments and share any updated code snippets or logs. I’m confident this will stabilize your stream and eliminate the zero‑padding artifacts.

    Best Regards,

    GN_Renesas

  • Hi,

    Thanks for the response.
    If I use tranlen 1024, most packets are 12 or 944 bytes long, which is expected behaviour. However, some packets are bigger, around 2500 bytes. I even received packets with lengths up to 25000 bytes, and by looking at the iTDs, I noticed that the transactions were indeed reaching lengths above 4000 bytes, which should be impossible even with 3 transaction per microframe. It looks like different packets get aggregated together upon arrival.

    I am not sure I understand how to implement the buffer flush. Do I just need to set IFIS to 1 and IITV to 0 in the PIPEPERI register, once ?
    And in order to do this, I would have to follow the sequence described in : 33.9.3.3 Pipe control register switching procedure, then just set PID to BUF again ?

    Regards,

    AlexR

Reply
  • Hi,

    Thanks for the response.
    If I use tranlen 1024, most packets are 12 or 944 bytes long, which is expected behaviour. However, some packets are bigger, around 2500 bytes. I even received packets with lengths up to 25000 bytes, and by looking at the iTDs, I noticed that the transactions were indeed reaching lengths above 4000 bytes, which should be impossible even with 3 transaction per microframe. It looks like different packets get aggregated together upon arrival.

    I am not sure I understand how to implement the buffer flush. Do I just need to set IFIS to 1 and IITV to 0 in the PIPEPERI register, once ?
    And in order to do this, I would have to follow the sequence described in : 33.9.3.3 Pipe control register switching procedure, then just set PID to BUF again ?

    Regards,

    AlexR

Children
No Data