we are trying to get GTIOC2B to be the PWM backlight provider. it is connected via P2_1. i am getting nothing out of the pin
i am using linux 5.10, cip41
here is my device tree set up. what am i doing wrong?
gpt2_pins: gpt2 { pinmux = <RZG2L_PORT_PINMUX(2, 1, 3)>; /* GTIOC2B */ };
&gpt2 { pinctrl-0 = <&gpt2_pins>; pinctrl-names = "default"; channel = "channel_B"; poeg = <&poega &poegb &poegc &poegd>;
status = "okay";};
lcd_bl: backlight { compatible = "pwm-backlight"; pwms = <&gpt2 0 1200>; brightness-levels = <0 50 70 90 110 130 150 170 190 210 255>; default-brightness-level = <10>; power-supply = <®_3p3v>; };
defconfig settings i assume apply:
CONFIG_PWM=yCONFIG_PWM_RCAR=yCONFIG_PWM_RZV2M=yCONFIG_PWM_RENESAS_TPU=yCONFIG_GPT_RZG2L=yCONFIG_POEG_RZG2L=y
i should also state the gpt driver seems to be loading:
[ 0.245935] gpt-rzg2l 10048200.gpt: Can use GTETRGA as POEG, reset_counter[ 0.245965] gpt-rzg2l 10048200.gpt: Can use GTETRGB as POEG, reset_counter[ 0.245986] gpt-rzg2l 10048200.gpt: Can use GTETRGC as POEG, reset_counter[ 0.246006] gpt-rzg2l 10048200.gpt: Can use GTETRGD as POEG, reset_counter[ 0.246572] gpt-rzg2l 10048200.gpt: RZ/G2L GPT Driver probed
Hi Mike,There is a similar ticket on our private ticketing system. We can continue our conversation, if you want to avoid duplicated tickets.Thank you.Kind Regards.