Demo: Crank Software GUI on RZ/A1 RSK (XIP Linux)

A demonstration of using the Crank Software's Storyboard software on an XIP Linux system. No external SDRAM is used in this demo. If you have the Storyboard software installed, you can run your own application from an SD card.
 
Additionally, the demo can be configured to boot from reset in 2.1 seconds.