AppNote: RZ/A1 Linux with Redpine RS9113 Module

This document describes the setup and usage of the Redpine Signals RS9113 Evaluation Board running under Linux on
a RZ/A1H RSK board. The scope of the document is to describe all the build steps as well as the order of the scripts and
command lines in order to a working wireless and BLE interrupt up and running. This document does not go into the
details of using wireless and BLE as that information is generic can be researched regardless of the system you are
running on.


The outlined operations are for:

  • WiFi Access Point with upstream internet connection through Ethernet
  • WiFi client connecting to a router and access the internet
  • Bluetooth Low Energy Client that can be access by a phone or tablet
  • Bluetooth Low Energy Host that can access a BLE device