Guiliani GSE migration from version 2.3 to v2.4

HI 

Here i am using GSE 2.3v for my GUI development . Now i have to migrate to 2.4v, i opened the old gpr file in 2.4v . But i cant even run in GSE environment. Is there any steps which i should follow to work the gpr file of 2.3v in 2.4v.

  • Hello,

    in general projects made with version 2.3 will open without any errors in 2.4.

    when using custom extensions the GSE needs to be rebuilt to incorporate the additional files. opening the project using these otherwise unknown extensions will cause loading errors.

    please be more specific on the errors you encounter when opening the project in 2.4 (e.g. error-messages from GSE)

    Best Regards,

    Guiliani Support

  • Hi

    Yeah oi am facing some extension issues like incompatibel header files like CGUIDatapool.h also am attaching the screenshot of errors

  • Hello,

    it seems that something went wrong when updating from 2.3 to 2.4.

    Normally an update of a Guiliani-SDK is done by extracting the package into a new folder and syncronizing all relevant user-files (usually located under Source and Include-folder in the StreamRuntime) into the StreamRuntime-folder of the new SDK.

    By doing this, it is assuered that the correct Guiliani and eGaC-folders (e.g include-files and libraries) are used and no problems with incompatible header-files or libraries will arise.

    The CustomStandardFactory.cpp indicates that it was generated with a GSE 2.4 whereas your SDK-files (especially the header-files) are not matching.

    Please repeat the update-procedure as described above.

    Best Regards,

    Guiliani Support

  • Hi,

    Now we removed the errors and 2.4 integration has been done but simulation is limited to only main screen, other screens and its dialogues are not able to simulate in run time also need to know the library file which we should add in 2.4 version

  • Hello,

    in Version 2.4 of GSE a new feature called "Export Configuration" has been implemented. This gives you the possibility to define different settings for different configurations (resolution, export-formats, etc.).

    Also the starting-dialog can be different for a configuration. To change the starting dialog of your application, you can use the button (shaped like a circle) in the toolbox below the dialogs-list. This will also change the starting-dialog for the current configuration. when using "run simulation" this dialog will  be displayed when the application starts.

    For more information on "export configurations" and how they can help you when having multiple configurations, see chapter 3.2.6.3  and chapter 4 in the GSE User Manual.

    Best Regards,

    Guiliani Suppot

  • Hi

    Some of the folder from gse2.4 i have added listed below

    1.eGaC

    2.GSE

    3.Streamruntime

    4.Guiliani

    after adding this files i received an error of undefined refrence to _dso_handle attaching image along with this

    Other than this anything required to add for migration from 2.3v to 2.4v

  • Hi

    Also while i was using GSE2.3v the GUI is running exactly 1hour.20 min only , we checked the free heap size it is 2552936 bytes(using the function(xPortGetFreeHeapSize();) there is no change in heapsize.Still we faced the hanging issue after 1hr20min.

    Thats why mainly we decided to migrate GSE from 2.3 to 2.4, could you please suggest a solution

    We used guiliani paid licence and entered in both GSE and E2 studio, will it be a problem of licence? or other memory deadlock? 

  • I'm not sure if the macros pre-installed on GSE still work, but you can get macros from the website WoWLazyMacros.com. When you do, be sure to use the spec suggestions the macro has. As far as the macros not firing, you have to either manually spam the button you put the macro on or have AHK or a gaming keyboard like Razer, Logitech, or Corsair. I use GSE myself and rarely do I have this problem. Also be sure that you clear any keybinds for any modifiers used in the macros(i.e. shift, ctrl, or alt). My All Savers Connect