Hi all,
I am using Guiliani v2.3 and I have a question.
Image files are used a lot in my project.When I checked with the tool, it seems that the size of the resource binary is increased because the image is stored as raw format data. Is it right?Is there a way to save as a compressed image to reduce the size of the Resource binary?Could you tell me how to reduce the resource binary?
Hello YJ Kim,
please refer to the GSE Manual Chapter 2.3.8 Export Formats.
Of course you can store the images in a compressed format by selecting "native". But be aware that this will use up a reasonable amount of RAM, since the images need to be uncompressed somewhere for blitting.
When using RAW or RLE the images can be blitted directly from the Flash-Memory which greatly saves RAM.
Best Regards
Guiliani Support