Remove default fonts and images

Hi all,

I have a question regarding the settings of TES (GSE:Guiliani Streaming Editor).


I'm trying to exclude default fonts and images to save space.
Since it cannot be deleted directly, is it okay to exclude it by turning off the check box for "Export Guiliani standard resources" when outputting the resource file?
Also, are there any other settings or methods that can reduce capacity?

Best Regards

Parents
  • Hello Mochi,

    Yes, unchecking the box will do just that. Please make sure to remove all references to the standard resources, as otherwise you will get a loading error during runtime.

    The following methods can be used:

    - use smaller or fewer images/resources

    - remove all unused resources. Within GSE select the menu item "Resources" -> "Manage" -> "Find Unsued Resource-IDs".
    But make sure to not delete any resources, used by your application code, as the GSE can't determine which resources are used there.

    Best Regards
    Guiliani Support

Reply
  • Hello Mochi,

    Yes, unchecking the box will do just that. Please make sure to remove all references to the standard resources, as otherwise you will get a loading error during runtime.

    The following methods can be used:

    - use smaller or fewer images/resources

    - remove all unused resources. Within GSE select the menu item "Resources" -> "Manage" -> "Find Unsued Resource-IDs".
    But make sure to not delete any resources, used by your application code, as the GSE can't determine which resources are used there.

    Best Regards
    Guiliani Support

Children