This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ZMOD4410 programming

Hello, I want to use ZMOD4410 for my project, but I am confused with the programming method of the sensor. The datasheet did not mention any specific register for gas measurements. Is it possible to program  ZMOD4410 without using RENESAS API or Library? I am using NXP kinetics MCU with NXP MCUxpresso IDE. 

If I can work without using RENESAS API or Library, How can I do it? please provide me specific register for each measurement.

Or if I need to use RENESAS API or Library how I will get it. I am requesting sufficient resources to use the ZMOD4410 gas sensor.

THANK YOU.

With Regards

Raduan




[locked by: Sai (SWF) at 6:31 (GMT 0) on 10 Jun 2022]
Parents Reply
  • Hello Thank you for your reply, but I need to work on NXP Kinetics MCU (MKL27Z128LH4) with NXP MUCxpresso IDE.

    As it is not included so it means I can not work with this sensor. 

    ZMOD4410 is not possible to work with NXP Kinetics MCU (MKL27Z128LH4) with NXP MUCxpresso IDE???

Children