This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ZMOD4410 programming

Hello, I want to use ZMOD4410 for my project, but I am confused with the programming method of the sensor. The datasheet did not mention any specific register for gas measurements. Is it possible to program  ZMOD4410 without using RENESAS API or Library? I am using NXP kinetics MCU with NXP MCUxpresso IDE. 

If I can work without using RENESAS API or Library, How can I do it? please provide me specific register for each measurement.

Or if I need to use RENESAS API or Library how I will get it. I am requesting sufficient resources to use the ZMOD4410 gas sensor.

THANK YOU.

With Regards

Raduan




[locked by: Sai (SWF) at 6:31 (GMT 0) on 10 Jun 2022]
Parents Reply
  • please note that we will only support our firmware on REN MCU as it has been specifically designed to work on a target MCU and tried/tested to work out of the box with our software tools (FSP). We can only support 3rd party MCU for specific customer opportunities. Thanks JE_REN

Children
No Data