ZMOD4XXX REDUCE TIME OF STABILIZATION

Hy, I wanna reduce the time of stabilization of sensor ZMOD4510, I just need to waith 1 hour to receive the first data.

This is the part of my code that go in 1 hour loop "Sensor in stabilisation", there is a way to reduce this time ?

//calculating result
                 APP_PRINT("calculating result\r\n");
                 rm_zmod4xxx_oaq_2nd_data_t data;
                 fStatus = RM_ZMOD4XXX_Oaq2ndGenDataCalculate(&g_zmod4410_ctrl, &rawData, &data);

                 if (fStatus == FSP_ERR_SENSOR_IN_STABILIZATION) {
                       SEGGER_RTT_printf(0, "Sensor in stabilisation.\r\n");
                       continue;
                 }

                 if (fStatus) {
                     SEGGER_RTT_printf(0, "\r\nRM_ZMOD4XXX_Oaq2ndGenDataCalculate failed. Event code: %d.", fStatus);
                     //isInitialized = 0;
                     continue;
                 }
I'm using the zmod4510 without IRQ on RA2L1 and I'm reading AQI vqalue.

Thank you.