Hi.
I'm testing to use ZMOD4410 on Allwinner's H3 chip and I will make this library for python 3.10 using C extention.
The os is Ubunut-based Armbian, and the kernel version is 5.15.79-sunxi.
The sensor conection was successful using the Raspberry Pi's library(maybe..).
However, it does not progress in the cleaning phase.
It show just "Starting cleaning procedure. This might take up to 1 min..." and blocking forever.
If delete the cleaning step from the source code, it will output "Error : Sensor probably damaged. Algorithm results may be incorrect".
Is there any solution? I just need tVOC and eCO2 it self... with out any algorithm.
Fig. Enter the cleaning_run function.
Fig. Without cleaning_run function.
I solved this problem.
My problem is I2C's timing. The hint is "i2cReadI2CBlockData, i2cWriteI2CBlockData" in the pigpio.
It work as well !!!