Multiple FS2012 flow sensors on the same I2C bus?

Hi!

We are in the development phase of a project were we would like to use multiple (4pcs) of the FS2012 flow sensors. We would prefer to have them all on the same I2C bus but is that even possible?

As far as we can see there is no way of changing the default I2C address of the sensors (x07).