IPS2200 not working

I am having issue with the IPS2200 board. I have my circuit board made and trying to test the encoder with no success. I know I have to spec CT1 and CT2 capacitors using the formula provided. The formula needs to have a value for L but I am not sure how to get the value?

I used the ICD tool from Renesas to create the coil and nowhere it says the value of coil inductance. 

When I power up the board and spin the target board, there is no Sin or Cosine waves.

See below for board drawing and pdf schematic.

  

[No Variations].PDF

Thanks

Armando

Parents Reply
  • Hi Raja,

    This encoder will be used to provide feedback for a stepper motor which is has a gear ration of 80:1.

    I have followed all the proper instructions to design the board but I believe I am missing something. When I power the board up there is no output. The suggested circuit from Renesas uses Ct1 and Ct2. How do I know what the value of my coil is in order to properly calculate the values of Ct1 and Ct2?

    Also, is the chip pre-programmed? Or do we have to program the chip before we use it?

    Can we have a Zoom or Teams meeting to chat about our project?

Children