IPS2200 not working

I am having issue with the IPS2200 board. I have my circuit board made and trying to test the encoder with no success. I know I have to spec CT1 and CT2 capacitors using the formula provided. The formula needs to have a value for L but I am not sure how to get the value?

I used the ICD tool from Renesas to create the coil and nowhere it says the value of coil inductance. 

When I power up the board and spin the target board, there is no Sin or Cosine waves.

See below for board drawing and pdf schematic.

  

[No Variations].PDF

Thanks

Armando

Parents Reply Children
No Data