ZMOD4510

Hello


I'm having problems compiling the 2nd gen gas detection algorithm libraries. When I try to build the program, I keep getting this same error:

"C:\Program Files\Microchip\xc8\v2.36\pic\sources\c99\common\roundf.c:12:: error: (1098) conflicting declarations for variable "_roundf" (/builds/industrial/zmod4xxx/zmod4xxx_generic_example/libraries/oaq_2nd_gen/src/oaq_2nd_gen.c:261)
(908) exit status = 1"

I already tried a few possilble solutions, but to no avail. Since I can´t change the library source code, I was wondering if you guys could help.

I'm using MPLAB v6.05, with xc8 v2.40 and a PIC18F27K42 MCU.
Any help would be greatly appreciated.

Best regards,
Carlos Silva

Parents Reply
  • You have been added to the moderated user list because you have breeched our community policy with repeated commercial solicitation in response to threads.

    All future posts from this user will be queued for review prior to posting to the forum.  Continued infraction will result in your removal from the community.

    REC Community Manager

Children
No Data