IPS2200 I2C communication issues. No ACK after address byte when reading.

Hello,

I am testing the IPS2200 for absolute position sensing applications. I made a prototype board and the sensor seem to work fine. I can get good sin/cos analog signals at the output while rotating a metal target. 

Now I am trying to communicate with this sensor over I2C bus using a PIC microcontroller. The problem is, that I can write data, but I can't read it. The sensor never sends an ACK signal after it's address byte when reading, but sends it when writing. Is it possible, that I first need to write some initialization data before reading the device? 

Here are the data packets recorded with digital analyzer.

READING - I don't get ACK, although the address seems to be correct.

WRITING - seems to work correctly, I get ACK after the address byte. 

Here are some more details about my setup.

I use 4.7k pullup resistor on both SCL and SDA lines, the CSn_IRQN pin is pulled up as well. The oscilloscope shows clear digital signals, with steep edges and no significant noise. I tried 2.2k resistors as well, but without any difference. I tried lowering I2C bus speed from 100kHz to 50kHz and then 20kHz as well. Tried to change the IC (two times).

To make sure, that there are no issues with the microcontroller, I connected a completely different i2c device to the same setup using the same code, just changed the i2c address. It is responding properly to both read and write commands, so I assume that it the problem is on the sensor side.  

What might be a possible cause for this?