Different values with FS3000 airflow sensor

I am building out an airflow testing rig and I’m using 16 airflow sensors. I realized that there is a difference in values for the different sensor when measuring the same air speed. I don’t think it’s dirt because all the sensors are new and I just assembled them. I measured the voltage across being supplied to the sensor and they are different, could this cause the difference in values. 
Also is the Vreg supposed to be connected to my 3.3v supply? It is not shown on the data sheet but I’m wondering if that’s part of the issue.

Also does shorting the board damage it?