Hello,
We are considering using the ZSC31050 for temperature compensation of sensors.
Regarding a mass calibration setup, would the evaluation kit (ZSC31050KIT) be enough for simultaneous calibration of multiple sensors using an additional multiplexer ?For example, we would connect multiple ZSC31050 using the SPI line and only switch the CS for adressing each of them individually.Is the provided software capable of registering calibration data of multiple sensors at a given temperature or do we need to calibrate each ZSC31050 at a time ?
Thank you for your time,
Best regards,
Hello Akoz,
my first answer may have been misleading, so here again are the options you have with the communication board (CB) and evaluation SW:
Examples:
Sending the command to the CB "SW_002CAFE", is translated into an SPI write sequence from CB to DUT, writing two bytes: 0xCA and 0xFE
Sending the command to the CB "SR_005", is translated into an SPI read sequence that reads 5 bytes from the DUT
Kornelius
Hello Kornelius,Thank you for your detailled answer, everything looks clear to me now.
Best regards,Akoz