Modify ZSSC3281 memory individually

Is there a way to change Indvidual register through the memory tab in the ZSSC328x Application v1.5.0?

If not, can it be done by the console?

  • Hello Elik,

    Thanks for your request and for reaching out Renesas Engineering Community.

    In case you are using the evaluation kit with the graphical software tool  you are able to view and edit the registers contents. 

    Please check section 10.2 of the evaluation kit manual attached here:

    www.renesas.com/.../zssc3281-evaluation-kit-manual

    Also I saw that you have created a duplicate request in  our internal ticket system and that one of our engineers has already reached out to you.

    Thank you.

    Best Regards,

    IK

  • Hi IK,

    Thank you for the answer.

    Let me clarify.

    1. I'm referring to ZSSC3281.
    2. The ZSSC328x Application does not allow to change registers, just to view the registers.
    3. I also look to use the console to view each register, and to modify each individual register.
    4. The console commands allow to view and change by I2C address (in my case) with number of bytes, but I could not find an example of script of console command to modify register by register address.
    5. Also, no procedure what needed to do to connect and prepare the ZSSC3281 for modifying the register. There is a spreadsheet with the command's syntax, but it does not use the register address just number of bytes to read.

    Any additional script, procedure, examples will be appreciated.

    Elik

  • Hi IK,

    Yes, you can view the registers, but not changing it.

    I tried it.

    According to the support it's not intended for editing unlike the ZSSC3241 application.

    Thank you.

    Regards

    Elik