IPS2200 Unable to communicate issues

Hello

I'm testing IPS2200 for absolute position sensing applications. I made a prototype board and the sensor seems to be working fine. I can get a good sin/cos analog signal at the output when rotating the metal target.

Right now, I'm trying to use a cortex microcontorller to communicate with this sensor over the I2C bus. The problem is, I can write data, but when reading the registers, the data is always changing. During the communication process, the oscilloscope grabs the I2C waveform, the communication is normal, and there is also a normal ACK, but the correct data is not obtained.

Hardware:

The CS pin of the sensor is pulled down to the ground, and the I2C pin is pulled up by 4.7K to the power supply. 3.3V for power supply.

Is there a problem with the reading and writing timing of the chip manual? What might be a possible cause for this?

Looking forward to a reply.

Parents Reply Children
No Data