Association between 13 RMOX raw values and heating temperature

Hi all,

I am using the 13 RMOX raw values taken from ZMOD4410 sensor to develop a custom algorithm. So, I would like to know the association between the 13 raw RMOX values and the associated heating temperature. 

Where can I found this information?

Best Regards,

David

Parents
  • Hello David,

    Thanks for your request, I assume you are referring to the heater temperature that is measured on each stage of an active measurement depending the RMOX value measured on each stage? As shown in the programming manual:

    Is that right? Could you please confirm. Also please specify to us which operating mode are you using  and which library?

    Thank you.

    Best Regards,

    IK_Renesas 

Reply
  • Hello David,

    Thanks for your request, I assume you are referring to the heater temperature that is measured on each stage of an active measurement depending the RMOX value measured on each stage? As shown in the programming manual:

    Is that right? Could you please confirm. Also please specify to us which operating mode are you using  and which library?

    Thank you.

    Best Regards,

    IK_Renesas 

Children