Connect script issues with ZSSC3281 kit

I wrote I connect script that does exactly what the script in log file created and initialization of the ZSSC3281.

The difference is the that the ZSSC3281 kit turn all the 4 LEDs on the ZSSCSRBV3 board (5V,12V,KS5V and KS12v) and my script turn on only 3 LEDs, and not the KS12V LED.

That is missing in the script? 

What the KS5V and KS12V LEDs  role in the board?

Elik

  • Hello Elik,

    Apologies for my delayed response!

    Please let me inform you that KS12V and KS5V are switchable power sources on the EV kit.

    Could you please provide us your connect script to be able to do a further analysis on your issue?

    Thanks.

    Best Regards,

    IK_Renesas

  • Hi,

    I attach the script which is basically the log from the initial connection.

    This is the original script, but since I use TeraTerm software to connect, since the ZSSC3281 application 

    force you to connect ahead I add also the TeraTerm script as well.

    Thank you.

    Regards

    Elik.

                                                                 

           Original script                        TeraTerm script (ttl extension)

    T0000000
    V
    V_HW
    T0000000
    V
    V_HW
    V
    V_HW
    T11100
    T_200
    PS_E71
    PS_E60
    T00000
    TWAIT100
    PS_A61
    PS_A51
    TWAIT20
    PS_E70
    IS_10
    IR_3C001
    IR_3C001
    IR_3C001
    IR_3C001
    IR_3C001
    IW_3C003820010
    IR_3C065
    IW_3C003821010
    IR_3C065
    IW_3C003822010
    IR_3C065
    IW_3C003823010
    IR_3C065
    IW_3C003824010
    IR_3C065
    IW_3C003825010
    IR_3C065
    IW_3C003826010
    IR_3C065
    IW_3C003827010
    IR_3C065
    IW_3C003828010
    IR_3C065
    IW_3C003829010
    IR_3C065
    IW_3C00382A010
    IR_3C065
    IW_3C00382B010
    IR_3C065
    IW_3C00382C010
    IR_3C065
    IW_3C00382D010
    IR_3C065
    IW_3C00382E010
    IR_3C065
    IW_3C00382F010
    IR_3C065
    IR_3C001
    IW_3C0018E
    IR_3C009
    IW_3C003840901
    IR_3C005
    IW_3C00189
    IR_3C004

    sendln 'T0000000'
    sendln 'V'
    sendln 'V_HW'
    sendln 'T0000000'
    sendln 'V'
    sendln 'V_HW'
    sendln 'V'
    sendln 'V_HW'
    sendln 'T11100'
    sendln 'T_200'
    sendln 'PS_E71'
    sendln 'PS_E60'
    sendln 'T00000'
    sendln 'TWAIT100'
    sendln 'PS_A61'
    sendln 'PS_A51'
    sendln 'TWAIT20'
    sendln 'PS_E70'
    sendln 'IS_10'
    sendln 'IR_3C001'
    sendln 'IR_3C001'
    sendln 'IR_3C001'
    sendln 'IR_3C001'
    sendln 'IR_3C001'
    sendln 'IW_3C003820010'
    sendln 'IR_3C065'
    sendln 'IW_3C003821010'
    sendln 'IR_3C065'
    sendln 'IW_3C003822010'
    sendln 'IR_3C065'
    sendln 'IW_3C003823010'
    sendln 'IR_3C065'
    sendln 'IW_3C003824010'
    sendln 'IR_3C065'
    sendln 'IW_3C003825010'
    sendln 'IR_3C065'
    sendln 'IW_3C003826010'
    sendln 'IR_3C065'
    sendln 'IW_3C003827010'
    sendln 'IR_3C065'
    sendln 'IW_3C003828010'
    sendln 'IR_3C065'
    sendln 'IW_3C003829010'
    sendln 'IR_3C065'
    sendln 'IW_3C00382A010'
    sendln 'IR_3C065'
    sendln 'IW_3C00382B010'
    sendln 'IR_3C065'
    sendln 'IW_3C00382C010'
    sendln 'IR_3C065'
    sendln 'IW_3C00382D010'
    sendln 'IR_3C065'
    sendln 'IW_3C00382E010'
    sendln 'IR_3C065'
    sendln 'IW_3C00382F010'
    sendln 'IR_3C065'
    sendln 'IR_3C001'
    sendln 'IW_3C0018E'
    sendln 'IR_3C009'
    sendln 'IW_3C003840901'
    sendln 'IR_3C005'
    sendln 'IW_3C00189'
    sendln 'IR_3C004'

  • Thanks Elik, let us check in more detail and come back to you.

    Best Regards,

    IK

  • Dear Elik,

    As you already know, I have forwarded your request to our Application Engineers for the SSCs products.

    And one of them has reached out to you by e-mail. Let me also attach here his response in case you missed the mail you received.

    I saw that your not waiting of the response of the communication Board (CRLF).
    Working Example:

    V

    <ACK>V4.21 ? ZMD AG 2020 - CB || SVN: 13769

    V_HW

    <ACK>SSC CB V4.1 : SSC EB ---- - not connected

    Your Example:
    Your Answer of the first V_HW is splitted and not after your command.


    V
    V4.21 © ZMD AG 2020 - CB || SVN: 13769
    V_HW
    T0000000
    V
    V_HW
    T0000000
    V
    V_HW
    V
    V_HW
    T11100
    T_200
    PS_E71
    SSC CB V4.1 : SSCPS_E60
    T00000
    TWAIT100
    PS_A61
    PS_A51
    TWAIT20
    PS_E70
    IS_10
    EB ---- - not connected

    KS5V = 5V switch
    KS12V = 12V switch
    To enable power supply to the IC

    You will find a excel document with more information’s in the zip

    https://www.renesas.com/us/en/document/swo/ssc-cb-firmware-v421-bootloader-use-communication-board-v41-only

     

    Hope it helps.

    Best Regards,

    Irini