Does Renesas offer a ZMOD4410 register manual?

I‘m using ZMOD4410 and use algorithm iaq_2nd_gen. And when I place the sensor with a fixed concentration of alcohol gas, the TVOC value returned by the sensor is fluctuating.

The following picture is drawn by tvoc*1000.

So I'm asking if there is a register manual for the ZMOD4410 so that we can parse the tvoc values and see for ourselves.