If you’re caught up watching House of Cards and the last episodes of Breaking Bad, consider watching some educational videos on work time to which your boss won’t object.
If any media outlet ever deserved to be called an “educational channel” it’s YouTube. With over 60 hours of new videos being uploaded every minute, there’s a wealth of educational material—much of it very professional (well, some of it anyway)—that’s just a mouse click away.
The official Renesas YouTube channel includes over 500 videos covering the full range of Renesas products in addition to those from Renesas’ Alliance partners. The videos run the gamut from high-level introductions (Get Started with RX) to the very specific (RX Sytem Exceptions & Interrupts). Each video is only a few minutes long, making it easy for you to quickly get the picture by watching the picture.
Check out Renesas Presents on YouTube before going straight to the datasheet. The videos are entertaining, will save you time, and may answer questions that you didn’t think to ask.