All but the most deeply embedded applications generally require an LCD screen to indicate status, report errors, or indicate the response to a command. Renesas RL78/L12 MCUs include an on-chip LCD driver/controller, making them a natural for consumer and industrial devices that require a fast, low-power MCU with a visual interface.
RL78/L12 MCUs run at up to 24 MHz, consuming just 75 μA/MHz in active mode; 0.64 μA…