Simplicity and complexity may be logical opposites, but customers expect the most complex, feature-rich applications to be simple and intuitive to use. Slick user interfaces are the norm in consumer devices, but commercial and industrial control systems are starting to catch up. With the Internet of Things (IoT) promising to be the Next Big Thing (NBT), design engineers need some way to overlay their complex designs with an intuitive user interface. Renesas and BugLabs have just made that a lot easier.
BugLabs provides two services to enable easy M2M communications. Dweet provides, in their words, “ridiculously simple data sharing for the internet of things. Fast, free, and easy to use, it’s like Twitter for social machines.” Dweet.io is a publisher and subscriber service to which devices connect to share data. The first graphic shows dweet.io capturing the data in real time from an Internet-connected Renesas RL78/G14 RDK. While nicely structured, this isn’t a format that’s useful for a control engineer.
Freeboard.io is another BugLabs offering, this one providing a dashboard of customizable widgets that enable you to easily visualize and control a remote device. The new BugLabs demo comes with a pre-build dashboard that connects seamlessly to an RL78/G14 RDK—once you’ve provisioned it and gotten it online.
Up and Running
To run the demo:
For a quick visual on how that works check out the brief (2:10) video below:
BugLabs promises “ridiculously simple dashboards for your devices.” In terms of the effort required to craft a slick interface to a powerful control board that isn’t far off the mark.